Beli wood pellet di monotaro.id

Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
  1. ACZET MB Series Moisture Balance
    Mulai

    Rp29.999.900

    ACZET MB Series Moisture Balance
    Deskripsi:
    The uncompromising & sophisticated halogen Moisture Analyzer with innumerable features & extensive data storage ability With New Aczet Moisture Analyzer you can achieve higher productivity without compromising on quality in your daily business challenges, since it is DIVERSE and can be programmed according to the individual needs of the person. No matter if user is from quality assurance, manufacturing or R&D. Built-in application program other than basic weighing ease your routine lab work like. Accurate & Reproducible Reliability : Reliable result depend on correct methodology. Select the intelligent function, key in the reference value and maximum time. The MB swiftly calculates appropriate switch-off criteria automatically to match the reference value to the last decimal place. You can save this parameter as method. Intelligent efficiently develops your method and saves your time in any area where different products are analyzed for their moisture content. You could never match your reference value with such accuracy. Ultra Fast and uniform heating Uniquely designed circular halogen Lamp and reflectors ensures utmost rapid heating, shorten the measurement time. Well engineered heating chamber ensure uniform heating to achieve exact result with exceptional reproducibility. Brilliant Monotech sensor with analytical precision The outstanding measurement performance of MB series is based on Aczet brilliant analytical weighing Technology MONOTECH, The forth decimal place is not displayed but is measured and used in calculation of highly precise results, gives highest measurement security. Compliance & Data Storage: Statistics This can display and print statistics for the last 9999 measurements based on each Method or Batch making this ideal intelligent instrument for R&D and Production both. Memory of each Moisture Determination This being the most versatile feature of Aczet MB series, it stores last 1000 moisture determination, so you can almost recall your work even after months, this make it UNIQUE and DEPENDABLE, no other instrument can offer this. Password protection Password protection prevents the unauthorized access to the stored data & alterations of the parameters thus ensuring its security ISO/GLP compliance print out It helps identify how, when & who performed the moisture determination. Highly flexible user configurable print format with 4 user id makes it customized yet traceable document in compliance to SOP's and GLP regulation making MB series most acceptable in each industry. Every successful calibration is been tracked and record with incremental numbers also last successful calibration report stored in memory makes it even more flexible and convenient. Diversity: DATA STORAGE This unique feature offers the flexibility to choose the data storage mode as per user application. Method Wise storage allows the user to store 25 moisture determination results in each method, user can store such 40 methods. Method wise storage is suitable for application in R&D or Quality Assurance where there are more number of different product (samples) to be analyzed. Batch wise storage allows user to create 100 batches & store maximum 1000 data with no restriction on the data storage per batch. Batch wise storage is suitable for application in production where there are more numbers of samples to be analyzed for the same product. Connectivity Do you have to write down the measurement of several dozen samples each day? Not any more. Thanks to the standard USB and RS232 interfaces, you can now conveniently transfer your data to your PC and continue working on it there, or print it out directly on Aczet print Graph Thanks to graphical display, user can view auto updating graph of the drying process with the change in the moisture level. Features like Weight in assist and Standby temperature helps user to improve reproducibility by taking same amount sample weight and similar climatic state for each moisture determination. Multiple Units of measurement results %M, %D, %R (ratio), Gm/Lt, %M Atro, %D Atro make it most convenient for each user. Various heating profile like Standard, Gentle, Rapid, Step & High temperature heating make's it possible to analyze any product sample. Various switch off criteria from Auto, Manual, Timed, User Defined G/T, User Defined %U/T, Intelligent makes it possible to achieve utmost accurate result. Sample Identification is traceable Graphical display with alpha numeric keypad and ps2 keyboard made user interface very easy for defining user specific text for each sample. Accessory -CPR 02 or Statistic printer -Calibration Weights -Aluminum Dish -Temperature Kit
    atribut:
    • Units of Measurement: % M, %D, %R (ratio), Gm/Lt, %M Atro, %D Atro
  2. TESTO Material Moisture Meter
    Mulai

    Rp5.299.900

    TESTO Material Moisture Meter
    atribut:
    • AS ONE Part Number: 1-6453-01
    • TGK Part Number: 540-68-08-01
    • Measurement Accuracy: (Material moisture) +/- 1% (with respect to measured electric conductivity)
    • Battery: 2xAAA alkaline batteries
    • Measurement Range: (Material moisture) 0-54.8 mass%
    • Resolution: (Material moisture) 0.1%
    • Accessories: Shipping inspection, strap, belt holder, protective cap, dry cell
    • Battery Life (hour): 200 (when backlight is off)
    • External Dimensions (mm): 119x46x25 (excluding protective cap device)
    • TRUSCO Number: 333-7481
    • Weight (g): 45 (excluding battery)
  3. AND Moisture Analyzer
    Mulai

    Rp37.999.900

    AND Moisture Analyzer
    Deskripsi:
    - 400W straight halogen lamp heating system with SRA filter and SHS weighing technology. - Measurement unit: Wet base/Dry base/Dry content/Ratio/Weight. - Sample pan size : Diameter 85mm.
    atribut:
    • Pan Size Diameter (mm): 85
  4. OHAUS MB Series Moisture Analyzers
    Mulai

    Rp43.999.900

    OHAUS MB Series Moisture Analyzers
    Deskripsi:
    Moisture affects everything we use on a daily basis. Therefore, in many cases it is important to be able to accurately determine the moisture content of samples. Equipped to handle routine and sophisticated measurements, our flagship moisture analyzer MB120 makes the whole process faster, easier, and more efficient. The MB120 allows you to analyze more samples, access saved data, and spend less time prepping and more time putting your results to work.
    atribut:
    • Moisture Content (%): 0.01
    • Heater Type: Halogen Lamp
  5. monotaro Digital Moisture Analyzer
    Mulai

    Rp2.399.900

    monotaro Digital Moisture Analyzer
    Deskripsi:
    A compact, lightweight size, convenient style for carrying mobile phones. Data hold function with fixed measurement value. With maximum value/minimum value/average value display function.With auto power off function to prevent battery drain due to forgetting (cancellation possible).Convenient backlight function when working in the dark. To check moisture of timber, cement and other building materials.Dokumentasi Produk:WARRANTY MonotaRO Private Brand
    atribut:
    • Measurement Pricision: ± 1%
    • Operating Temperature and Humidity Range: 0 to + 50 ° C, 70% RH or less (with no condensation)
    • Sampling: 1 time / s
    • Storage Temperature/Humidity Range: -20 to + 60 ° C, 80% RH or less (with no condensation)
    • Accessories: Instruction manual, strap, protective cover
    • Measuring Range: 8.8 to 54.8% (beech, spruce, larch, birch, cherry, walnut),. 7.0 - 47.9% (oak, pine, maple, ash tree, rice bran, melan tea),. 0.9 to 22.1% (cement, concrete, plaster),. 0.0 to 11.0% (gypsum),. 0.7 to 8.6% (cement mortar),. 0.6 to 9.9% (lime mortar),. 0.1 to 16.5% (brick)
    • Measurement Item: Moisture percentage
    • Batteries: Two AAA (1.5 V) batteries
    • Resolution Capability: 0.10%
    • Weight (g): Approximately 119 (with protective cover installed, batteries included)
    • Battery Life (continuous use): About 150 (when using alkaline dry batteries)
    • Dimensions (mm): 50.9x132.9x24.7
  6. Landtek Grain Moisture Meter
    Mulai

    Rp2.799.900

    Landtek Grain Moisture Meter
    Deskripsi:
    Landtek MC-7825G Grain Moisture Meter Adalah Alat Pengukur kadar air dari pabrikan Landtek ini mengukur kadar air 36 jenis biji bijian dan hasil bumi.
    atribut:
    • Resolution: 0.1
  7. Kett Grain & Seed Moisture Meter
    Mulai

    Rp23.999.900

    Kett Grain & Seed Moisture Meter
    atribut:
    • Measuring Principle: Capacitance (Di-Electric)
    • Power: 4AA Batteries
    • Sample Volum: Approximately 240ml
  8. AND Moisture Analyzer- Accessories
    Rating:
    100% of 100
    (2)
    Mulai

    Rp319.900

    AND Moisture Analyzer- Accessories
    Deskripsi:
    Moisture Analyzer-Accessories:AX-MX-31 : Sample Pan (100pcs)AX-MX-32-1 : Filtration Glass Fiber Sheet (100 sheets)AX-MX-32-2 : Glass Fiber Sheet (100 sheets)AX-MX-33 : Sodium Tartrate Dihydrate (30gx12pcs)AX-MX-34 : Halogen LampAX-MX-43 : Temperature Calibrator for MX
  9. INGCO Wood Moisture Meter
    Mulai

    Rp619.900

    INGCO Wood Moisture Meter
    Deskripsi:
    INGCO Wood Moisture Meter // Alat Ukur Kadar Air Kelembaban Kayu Semen Gipsum Bata Hebel
    atribut:
    • Moisture Measurement Range (%): 2-70
    • Moisture Measurement Accuracy (%): ±2
    • Temperature Range (°C): 0 to 40
    • Environment Temperature (°C): 0 to 40
    • Response Time (s): <1
  10. TESTO Material Moisture Meter (With Temperature And Humidity Meter)
    Mulai

    Rp6.099.900

    TESTO Material Moisture Meter (With Temperature And Humidity Meter)
    atribut:
    • TGK Part Number: 540-68-08-02
    • Measurement Range: (Material moisture) 0-54.8 mass%, (humidity) 5-95% RH, (gas temperature) -10-50 degrees Celsius
    • Resolution: (Material moisture) 0.1%, (humidity) 0.1% RH, (gas temperature) 0.1 degrees Celsius
    • Operating Temperature (°C): -10 to 50
    • Accessories: Shipping inspection, strap, belt holder, protective cap, dry cell
    • Accuracy: (Material moisture) +/- 1% (based on measured electric conductivity), (Humidity) +/- 2.5% RH, (Gas temperature) +/- 0.5 degrees Celsius
    • Battery: 2xAAA alkaline batteries
    • Battery Life (hour): 130 (when backlight is off)
    • External Dimensions (mm): 119x46x25 (excluding protective cap device)
    • TRUSCO Number: 333-7499
    • Weight (g): 45 (excluding battery)
  11. TESTO Moisture Meter
    Mulai

    Rp3.499.900

    TESTO Moisture Meter
    Deskripsi:
    The testo 616 professional moisture meter provides you with a precise and non-destructive means of measuring the moisture content of wood and building materials and of monitoring the drying process after water damage. Simply select the characteristic curve and place the meter’s measuring claw against the surface of the material you would like to measure. The meter shows you the moisture content as a weight percentage compared to the dry weight. Press the relevant key to save the reading to your meter.Although the measuring claw only comes into contact with the surface, wall or flooring that is being measured, it is able to determine the moisture content of the wood or other material down to a depth of 5 cm.Ideal areas of use for the testo 616 moisture meterThe testo 616 moisture meter is a professional measuring device that can be used in areas as diverse as water damage restoration or carpentry or joinery.Moisture damage detection: the non-destructive method for finding moisture in walls and floorsMonitoring drying processes: from carrying out moisture inspections to meeting building schedules to controlled drying after water damage - the non-destructive method for determining the moisture content in wood and building materialsMoisture in wood: for checking the moisture content of wood that has been stored prior to processingtesto 616 moisture meter with 10 characteristic curvesSoft woodHard woodPressboardAnhydrite screedCement screedLime sand brickGas concreteConcreteHigh insulation bricksBrickwork Product Includes: testo 616 moisture meter for wood and building materials, calibration protocol, batteries.Determining moisture in wood Moisture content is a decisive factor in the further processing and use of timber products. If wood is installed with the wrong moisture content this may result in mechanical deformations (contracting and swelling) at the site where the material is subsequently used, and therefore damage to pieces of furniture or entire supporting structures in buildings. Therefore, before being made into furniture or supporting material by a joiner/carpenter, the suitability of the wood has to be assessed by measuring the moisture content. The testo 616 enables the quick and non-destructive examination of the material moisture characteristics in timber. Characteristic curves are available for measuring wood moisture in soft and hard woods, and chipboard. These characteristic curves were developed in cooperation with the LPI institute.The measurement results are calculated up to a depth of 5 cm and can be recorded at the touch of a button. The readings are displayed in percent by weight in comparison to the dry mass of the material. Monitoring drying processes Whether freshly laid screed, or monitored drying of moisture damage, timely determination of the required moisture level will save time and therefore money. Screeds are laid in the in interior works stage, generally after plastering. The flooring and painting and decorating then follow. The drying behaviour is therefore a significant factor in the works schedule, primarily because the laying of flooring depends on this.The moisture measurement establishes readiness for flooring; liability for the flooring is thus transferred to the respective trade installing the flooring. An important part of this work is therefore documentation and assurance in the testing for readiness for flooring. What is the extent of moisture damage? This question has to be answered in order to decide which instruments are to be used to speed up the drying process.The testo 616 can be used to quickly and non-destructively examine the material moisture in building materials. It also makes work easier when drying processes for floors, walls and surfaces have to be observed. Diagnosing building moisture Moisture may penetrate walls, floors and ceilings due to pipes bursting or water ingress. Some of this moisture damage may not be detected immediately. Rising or ingressing water, faulty rain and waste water drains, or even blocked drains and inadequate seepage capacity may be the cause. Depending on where it is getting out or in, the moisture can spread in different ways; enormous damage may be done if discovered too late. Therefore, measurement of the material moisture in the affected places is necessary to be able to identify the source of the damage. The testo 616 can be used to quickly and non-destructively examine the material moisture in building materials. The measuring clamp is laid on the surface; the value can be read immediately. The measurement results are calculated up to a depth of 5 cm and can be recorded at the touch of a button. The readings are displayed in percent by weight in comparison to the dry mass of the material. For easy, quick handling, characteristics are already stored in testo 616 for the following construction materials: anhydrite screed, cement screed, lime sand brick, aerated concrete, concrete, vertically perforated brick and solid brick; these aid detection of wet places in the construction materials.
  12. Extech Moisture Meter
    Mulai

    Rp1.599.900

    Extech Moisture Meter
    Deskripsi:
    MO260 is a Combination Pin/Pinless Moisture Meter which measures Relative Moisture in wood and other building materials using pinless technology plus % of Moisture in sheetrock and other materials using the direct pin method. Measurements are displayed on a digital LCD with backlighting and a tri-color LED bargraph. Pinless non-invasive measurement depth to 0.75 Inch (22mm) below the surface. Complete with 9V battery, replacement pins, protective cap, and pouch case.
  13. OHAUS Moisture Analyzer
    Mulai

    Rp28.999.900

    OHAUS Moisture Analyzer
    Deskripsi:
    The MB23 provides precise moisture content determination at an unbeatable value. With a large backlit LCD display, standard RS232 port, 110g capacity with a readability of 0.01g/0.1% and an non-glass infrared heating element, the MB23 offers moisture analysis for any budget.ApplicationsPercent Moisture Determination, Percent Solid Determination, WeighingDisplayBacklit liquid crystal display (LCD)OperationPower cord (included)CommunicationRS232 (included)ConstructionInfrared heat source, ABS housing, metal pan support, metal pan handler, in-use coverDesign Features3 shut off criteria (manual, timed or auto), 1 standard heating profile, 50° to 160° C heating range (5° C increments)
  14. Lutron Moisture Meter
    Mulai

    Rp3.199.900

    Lutron Moisture Meter
    Deskripsi:
    - Designed to check the moisture level of wood, concrete, and other non-wood material- 6 % to 40 % moisture range on wood.- 0 to 100% relative moisture value for Concrete and other non-wood material.- Red LED bar graph indicator and LCD digital display.- All in one, meter build in the test pins- Optional separate probe, available for remote measurement- Microprocessor circuit assures maximum possible accuracy, provides special functions and features- Records Maximum & Minimum reading with recall.- Data hold function to freeze the desired value on display- Heavy duty & compact housing case, designed for easy carry out & operation- Built-in low battery indicator
    atribut:
    • LCD Size (mm): 51x37
    • Digit Size (mm): 16
    • Material Range: Material 1 : 0 to 100% relative moisture value for Concrete. and other non-wood material. Material 2 : 6 % to 40 % moisture range on wood.
    • Resolution (%): 0.1
    • Probe: 2 pins moisture electrode.
    • Data Hold: By push button on front panel.
    • Memory Recall: Records Maximum & Minimum reading value
    • Operating Temperature (°C): 0 to 50
    • Humidity (%RH): 80
    • Power Current (mA): Approx. DC 16
    • Dimensions (mm): 216.5x68.5x29.7
    • Sampling Time (s): Approx. 0.8
  15. OHAUS Moisture Meter
    Mulai

    Rp27.999.900

  16. KRISBOW Alat Ukur Kelembaban Kayu Portabel
    Mulai

    Rp529.900

    KRISBOW Alat Ukur Kelembaban Kayu Portabel
    atribut:
    • Accuracy (%): Wood : ±2, Material : ±0.2
    • Ambient Relative Humidity: 0-85% RH
    • Ambient Temperature (°C): Measuring Range: 0 to 50 (32 to 122°F), Accuracy: ±1/±1.8
    • Auto Power OFF: After Approx. 3 minutes
    • Battery: 4 A-LR44, replaceable
    • Dimension (HxWxD) (mm): 96x40x20
    • Electrode Length (mm): 8.5
    • Humidity Content: Wood, Building Material
    • Measuring Principle: Electrical resistance
    • Measuring Range (%): Wood : 6-44, Builing Material : 0.2-2.0
    • Moisture Content: Degree Celcius And Fahrenheit
    • Sensor Type: Electrode Pins
    • Type: Portable
    • Weight (kg): 0.083
  17. KRISBOW Alat Ukur Kelembaban Kayu Profesional
    Mulai

    Rp4.299.900

    KRISBOW Alat Ukur Kelembaban Kayu Profesional
    atribut:
    • Auto Power OFF: After approx. 3 mins
    • Auto LCD backlight OFF: After approx. 10 sec
    • Accuracy (%): Wood : 0-30%/±1, 30-60%/±2, 60-75%/±4, Others Materials : /±0.5%
    • Ambient Relative Humidity: Measuring Range: 0 to 100%, Accuracy: 0-20% & 80-100%/±5°C, 20-80%/±3.5°C
    • Ambient Temperature (°C): Measuring Range: -40 to 70 (-40 to 158°F), Accuracy: -40 to -10 & +40 to +70/±2°C, -10 to +40/±1°C
    • Battery: 3 x Cr 2032
    • Dimension (HxWxD) (mm): 160x60x28
    • Electrode Length (mm): 8
    • Measuring Range (%): Wood : 1-75, Builing Material : 0.1-2.4
    • Weight (kg): 0.203
  18. AND Moisture Meter
    Mulai

    Rp47.999.900

  19. CHINA Digital Paper Moisture Meter
    Mulai

    Rp1.299.900

    CHINA Digital Paper Moisture Meter
    Deskripsi:
    Digital paper Moisture Meter can work on 3 types paper (carton, copperplate paper and writing paper) through the spring contact precise measuring.
    atribut:
    • Display: Large LCD Display
    • Range (%): 0-40
    • Resolution: 0.01
    • Accuracy (%): ±1
    • Operating Temperature (°C): 15-30, 30-70%RH
    • Battery Consumption (mA): Approx. 7.5
    • Power: 9V Battery
Daftar Harga wood pellet Terbaru March 2026
ACZET MB Series Moisture BalanceRp29.999.900
TESTO Material Moisture MeterRp5.299.900
AND Moisture AnalyzerRp37.999.900
OHAUS MB Series Moisture AnalyzersRp43.999.900
monotaro Digital Moisture AnalyzerRp2.399.900
Landtek Grain Moisture MeterRp2.799.900
Kett Grain & Seed Moisture MeterRp23.999.900
AND Moisture Analyzer- AccessoriesRp319.900
AS ONE Halogen Moisture MeterRp22.999.900
INGCO Wood Moisture MeterRp619.900

Data diperbarui pada 06/03/2026 (Harga belum termasuk PPN)