Beli Data Logger Temperature Humidity di monotaro.id

Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
  1. Elitech Temperature Data Logger
    Mulai

    Rp519.900

    Elitech Temperature Data Logger
    Deskripsi:
    Elitech RC-5 USB Temperature Data Logger terutama digunakan untuk pencatatan suhu selama penyimpanan dan transportasi laut / udara / jalan raya bahan makanan, obat-obatan, bahan kimia dan produk lainnya, terutama banyak digunakan di semua jenis pergudangan, logistik dan rantai dingin, seperti wadah berpendingin, berpendingin truk paket berpendingin, penyimpanan dingin, laboratorium, dll. atau dalam bisnis rantai pasokan global berskala besar.Pencatat Data Suhu mini ini memiliki rentang pengukuran yang luas -30 ° C ~ + 70 ° C, akurasi tinggi, interval pencatatan yang dapat disesuaikan & masa pakai baterai yang lama untuk perekaman, pemantauan, dan analisis data suhu yang nyaman dan andal.Memiliki memori data permanen besar 32000 poin dan dilengkapi dengan perangkat lunak manajemen data untuk mengunduh data dengan mudah ke komputer melalui antarmuka USB. Dengan software ini, Anda dapat menganalisis data dalam bentuk tabel dan grafik dan mengekspornya dalam format gambar. Data dapat dipertanyakan, disimpan, dicetak dan diekspor dalam format Word / Excel / TXT / PDF.
    atribut:
    • Temperature Resolution (°C/°F): 0.1
  2. TESTO Temperature and Humidity Data Logger
    Mulai

    Rp9.999.900

    TESTO Temperature and Humidity Data Logger
    Deskripsi:
    Are the prescribed humidity and temperature values in warehouses and buildings being adhered to? Is mould in the apartment the result of insufficient ventilation, or caused by building damage? With the data logger for temperature and humidity testo 176 H1, you can find out.Up to two temperature and/or temperature/humidity probes can be connected to the 4-channel data logger testo 176 H1 and positioned in the room according to the individual requirements. A wide selection of probes is available to you for this purpose.The lock included in delivery protects your temperature and humidity loggers from unauthorized access.Security and convenience at all levelsThe testo 176 H1 data logger for temperature and humidity guarantees high data security and reliable measurement results on the basis of modern measurement technology.In addition to the current temperature and humidity values, the data logger testo 176 H1 also shows the dewpoint in the display (when a temperature/humidity probe is connected). You can read programmed limit values, min. and max. values, limit value violations as well as the remaining battery life easily from the large display. It is therefore not necessary to read out the temperature and humidity logger to a PC in order to gain a quick overview.Thanks to the large memory for 2 million measurement values, and the battery lifetime of up to 8 years, you can read out the data much less often, even at a shorter measurement intervals. The standard battery (AA) can be easily exchanged at any time by the user.Programming and evaluation of the data logger for temperature and humidityFor the programming and readout of the data logger for temperature and humidity, as well as for the analysis of the measurement data on a PC, three software versions are available.ComSoft Basic software - available for free download - allows the fast programming of the data logger as well as easy data analysisComSoft Professional software - optionally available - offers you different possibilities for the detailed analysis of temperature and humidity valuesComSoft CFR 21 Part 11 software - optionally available - optimum for the special requirements of the pharmaceutical sector according to CFR 21 Part 11Caution: To program the temperature and humidity data logger, you require a USB cable which is not included in delivery. Transfer of the saved measurement data from the data logger to a PC takes place by USB cable or SD card - you can order both as optional accessories together with your testo 176 H1.Application areas for the temperature and humidity data loggerMonitoring and documentation of building climateMonitoring and documentation of storage temperature and humidityMould in an apartment: With the temperature and humidity data logger you can find out whether moisture and mould on ceilings and walls are the consequence of building damage or a sign of incorrect ventilation behaviour. Product Includes: 4-channel data logger for temperature and humidity testo 176 H1 with external probe connections (NTC/capacitive humidity sensor), including wall bracket, battery and calibration protocol.Mould in an apartment Damp ceilings and walls may be a result of structural damage. In most cases, however, it is a sign of improper ventilation. Once the mould appears inside a house, the tenant assumes that moisture has come in from outside. Numerous disputes have erupted because of the issue of who is liable for the mould damage. It is very difficult to determine who or what has caused mould: the inhabitants or defective building construction? The temperature and humidity data logger testo 176 H1 is ideal for measuring humidity in ceilings and walls. For the measurement,you connect both optional probes – temperature/humidity probe and wall surface temperature probe – to the humidity logger testo 176 H1, and save the measurement data over a longer period.You need the temperature/humidity probe in order to monitor the dewpoint of the indoor air. The wall surface temperature probe attached to the wall measures the surface temperature of the wall. The dewpoint distance determined from the dewpoint of the indoor air and the wall surface temperature provides information on whether the mould in the apartment is caused by insufficient ventilation or by structural damage. Please note that the optional software ComSoft Professional is necessary for the calculation of the dewpoint distance. Monitoring and documentation of building climate Temperature and relative humidity are crucial factors when it comes to assessing air quality and comfort levels in indoor areas, e.g. in workplaces. Both values can be monitored and documented over the long term using data loggers.They are also very well suited for checking ventilation systems or for assessing any building moisture which occurs.The use of special software means measurement configurations can be carried out individually and recorded measurement data can be both analysed and archived. Monitoring and documentation of storage temperature and humidity Correct compliance with storage temperature and humidity is an important prerequisite for the quality assurance of many products, e.g. in the area of food and pharmaceutical products.As a general rule, data loggers are used to do this. They automatically check and document the profile of the ambient conditions and thus make a crucial contribution to verifiable preservation of product quality.Viewing breaches of limit values directly on the display means you can respond quickly to temperature and humidity deviations. In addition, with the help of the configuration and read-out software, customer-specific measurement configurations can be carried out and recorded measurement data can be both analysed and archived.
    atribut:
    • Interface: mini usb, SD card slot
    • Product Color : Black
    • Product/Housing Material: Plastic
    • Standards: EU-guideline 2014/30/EU; 2011/65/EU
  3. Comark Temperature & Humidity Data Logger
    Mulai

    Rp19.999.900

    Comark Temperature & Humidity Data Logger
    Deskripsi:
    Comark Data LoggerThe Comark compact and lightwEight 2-channel temperature and humidity data logger. Internal sensor measurement temperature ranges between -20°C and 60°C, humidity 0 to 97% RH non-condensing.ApplicationsFoodPharmaceutical industryChemical industryCertificationsIP67 ratedEN60529IEC529
    atribut:
    • Alarm: Yes
    • Battery Life (Year): 5
    • Battery Type: AA
    • Best Humidity Measurement Accuracy: ±3 %
    • Best Temperature Measurement Accuracy (°C): ±0.5
    • Data Logger Type: Temperature & Humidity
    • Display Type: LCD
    • Humidity Measurement Resolution (%RH): 0.1
    • IP Rating: IP67
    • Interface Type: Infrared
    • Maximum Humidity Measurement (%RH): 97
    • Maximum Operating Temperature (°C): 70
    • Maximum Temperature Measurement (°C): +60
    • Measurement Parameters: Humidity, Temperature
    • Minimum Operating Temperature (°C): -40
    • Number of Input Channels: 2
    • Power Source: Battery
    • Sensor Type: Thermistor
    • Temperature Measurement Resolution (°): 0.1
  4. TESTO Absolute Pressure, Temperature and Humidity Data Logger
    Mulai

    Rp24.999.900

    TESTO Absolute Pressure, Temperature and Humidity Data Logger
    Deskripsi:
    When ambient conditions, for example in a laboratory, need to be documented securely and highly accurately, choose the data logger testo 176 P1. It has an integrated sensor which measures absolute pressure precisely in the range from 600 mbar up to 1100 mbar.Up to two temperature/humidity probes can be additionally connected to the 5-channel data logger testo 176 P1. A wide selection of probes is available to you for this purpose.The lock included in delivery protects your loggers from unauthorized access.Security and convenience at all levelsThe testo 176 P1 data logger for absolute pressure, temperature and humidity guarantees high data security and reliable measurement results on the basis of modern measurement technology.When temperature/humidity probes are connected, the data logger also shows the dewpoint in the display, in addition to the current measurement values. You can read programmed limit values, min. and max. values, limit value violations as well as the remaining battery life easily from the large display. It is therefore not necessary to read out the data logger to a PC in order to gain a quick overview.Thanks to the large memory for 2 million measurement values, and the battery lifetime of up to 8 years, you can read out the data much less often, even at a shorter measurement intervals. The standard battery (AA) can be easily exchanged at any time by the user.Programming and evaluation of the data loggerFor the purposes of programming and readout of your data logger, as well as the evaluation of the measurement data on a PC, you can choose between three software versions:ComSoft Basic software - available for free download - for the fast programming of the data logger as well as easy data analysisComSoft Professional software - optionally available - offers you different possibilities for the detailed analysis of absolute pressure, temperature and humidity valuesComSoft CFR 21 Part 11 software - optionally available - optimum for the special requirements of the pharmaceutical sector according to CFR 11 Part 11To program the data logger, you require a USB cable which is not included in delivery. Transfer of the saved measurement data from the data logger to a PC can also take place by USB cable or by an SD card. You can order both as optional accessories. Product Includes: testo 176 P1, 5-channel data logger with internal pressure sensor (absolute pressure) and external probe connections (NTC/ capacitive humidity sensor). Including wall bracket, battery and calibration protocol.Monitoring and documentation of laboratory conditions The ambient conditions for research projects must frequently be documented in laboratories to check external influencing factors. In addition to recording temperature and humidity, this also includes checking the absolute pressure. There are major requirements in terms of reliability, along with tamper-proofing and data security of the recording instrument, as incorrect documentation could invalidate the whole research result. There are only a few instruments which can log all three measurement parameters at the same time and also offer the required amount of data security.
    atribut:
    • Measuring Rate: 1 s to 24 h; 2 s to 24 h (online Measurement)
    • Memory: 2,000,000 Measuring values
    • Operating Temperature: -20 to +70 °C
    • Protection Class: IP54
    • Battery Life: 8 years at 15 min. Meas. Rate, +25 °C
    • Battery Type: 1xLithium (TL-5903)
    • Channels: 4 external; 1 internal
    • Connectable Probes: 2xNTC Temperature Probe or 2xHumidity Probe
    • Dimensions (mm): 103x63x33
    • Interface: mini usb, SD card slot
    • Product Color : Black
    • Product/Housing Material: Plastic
    • Standards: EU-guideline 2014/30/EU; 2011/65/EU
    • Storage Temperature: -40 to +85 °C
    • Weight (g): 218
  5. Besantek Wireless Temperature and Humidity Data Logger
    Mulai

    Rp47.999.900

    Besantek Wireless Temperature and Humidity Data Logger
    Deskripsi:
    The BESANTEK BST-DL115 Wireless Temperature and Humidity Data Logger with External Probe can be widely applied to laboratory settings, medical applications, the food and pharmaceutical industries, industrial applications, environmental protection areas, and agricultural research fields. The logger features an adaptive and highly sensitive sensor with fast response and high accuracy. It uses Zigbee 2.4GHz wireless technology and has a transmission range (line of sight) of up to 100 meters. The logger's memory can be automatically downloaded to a PC, allowing for real time monitoring on a computer.In the Box1 - Data Logger1 - PC Software1 - Adaptor1 - Screw4 - AA Batteries1 - Manual
    atribut:
    • Humidity Accuracy (RH): ±3%
    • Humidity Range (RH): 0 - 100%
    • Humidity Resolution (RH): 0.001
    • Log Interval: 2 Seconds - 24 Hours
    • Recording Capacity: Maximum 8192
    • Sensor Type (m): External Temperature and Humidity Sensor With 3 Cable
    • Temperature Accuracy (°C): ±0.5
    • Temperature Range (°C): -40 to 85
    • Temperature Resolution (°C): 0.1
  6. TESTO Air Humidity and Temperature Data Logger
    Mulai

    Rp7.599.900

    TESTO Air Humidity and Temperature Data Logger
    Deskripsi:
    With the temperature and humidity data loggers testo 184 H1, you monitor the transport of sensitive goods such as pharmaceuticals, foods or electronics or art, over an unlimited period.At their destination, a glance at the display or the LEDs tells you whether the configured limit values have been adhered to. In order to obtain detailed information, it is sufficient to connect the logger to a PC - a PDF report is immediately generated with all relevant data. In order for you to be able to work even more efficiently and conveniently with the data loggers, all required files and information are stored directly and securely in the testo 184 H1: Configuration file, instruction manual and PDF report of your recorded data.The measurement value store of the temperature data logger testo 184 H1 has a capacity of 64000 measurement values. The measurement rate is freely selectable from 1 min to 24 h. The battery has a life of 500 days. The temperature data logger testo 184 H1 is supplied by a standard battery which can be exchanged by the user.testo 184 H1 is compliant with GxP, 21 CFR Part 11 and HACCP. Testo is an ISO 9001-certified company, and ensures the adherence to the norms through internal audits as well as accredited external audits. All advantages at a glance:1. Clear alarm indicationA glance at the display or the LEDs is enough to know whether limit values have been violated during transport.2. Easiest operationtesto 184 H1 is intuitively operated, and can be used without special training or previous knowledge: The "Start" button begins data recording. "Stop" ends it.3. Easiest configurationIn each testo 184 H1, a configuration file is stored, with which the configuration of the testo 184 H1 is childsplay - no download, no installation, no user interface and no additional costs.4. Convenient readoutA PDF report with the transport data is created immediately on connection of the testo 184 H1 data logger to the USB interface of a computer. This is suitable for long-term archiving according to PDF/A standard.5. Mobile readout/printout on siteData transfer from the data logger to a compatible Testo fast printer (option) also functions wirelessly via NFC.6. IT-safeThe testo 184 H1 data loggers work securely without software installation or download, so that IT problems are triggered neither by the firewall nor the virus scanner. Product Includes: Temperature and humidity data logger testo 184 H1 and battery.Monitoring and documentation of temperature, humidity and shock in food logistics Handling foods involves danger to human health at all levels. In order to be able to eliminate them as far as possible, food companies must comply with an HACCP concept which guarantees food safety along the entire production chain – "from farm to fork". The adherence to product-specific limit values and the uninterrupted monitoring of the cold chain are crucial. In many cases, the monitoring of humidity and shock, in addition to temperature, are relevant for the maintenance of food quality.With the testo 184, quality managers in food logistics have six HACCP International-certified data loggers available to them, which monitor and document all critical parameters during the transport of foods. The data loggers testo 184 T1,T2, T3 and T4 have been additionally tested and certified according to EN 12830 by the TÜV Süd, and are therefore ideally suitable for the transport of refrigerated and deep-frozen foods. Monitoring and documentation of temperature and humidity during the transport of flowers Researchers discovered long ago that the temperature during the transport of cut flowers and green plants has a crucial influence on their quality. Since flowers are traded globally, and as it is not uncommon for flowers from Kenya, Tanzania or Ecuador to be sold in the USA, Germany or Russia, the monitoring of transport conditions during their often days-long journeys is essential.Flowers must be transported neither too warm not too cold. The former results in the loss of blossoms and leaves, the latter involves cold damage, which negatively influences not only the appearance but also the longevity of the plants. Sufficient air humidity is furthermore also of significance for the quality of the flowers.With the data loggers testo 184, measuring instruments are now available to you with which you can monitor and document temperature and humidity in the logistics of cut flowers and green plants quickly, easily and reliably. Monitoring and documentation of temperature, humidity and shock in logistic services of all kinds Providers of logistic service often take on the responsibility for expensive and sensitive products from the fields of pharmaceuticals, food, electronics or art. The wrong conditions during transport can lead to considerable losses of quality, right up to the complete devaluation of the monitored products.With the help of the testo 184 data logger, the prescribed temperature and humidity limit values as well as the shock tolerance levels can be monitored during transport, and thanks to the automatic report creation, very easily analyzed and documented. This allows all doubts regarding the correct transport conditions to be eliminated.Shock-sensitive products such as electronics, delicate machinery or certain bio-pharmaceuticals can be additionally monitored for the violation of previously defined shock limits with the help of the testo 184 G1. Monitoring and documentation of temperature, humidity and shock in pharmaceutical logistics Most pharmaceuticals must be continuously transported and stored at defined upper and lower temperature and humidity limit values, along the entire supply chain. A violation of these predefined upper and lower limit values can lead to irreversible alterations of the active ingredients or the composition of the medicaments. However, not only medicaments and their active ingredients are endangered. Minus temperatures or extreme temperature fluctuations can also cause damage to containers or medical instruments. The consequence is the threat of spoilage of the entire goods, financial losses and damage to reputation.In GxP-compliant quality management, the control of the entire cold chain, from production to delivery, is therefore a prerequisite, in order not only to ensure product quality, but also to prevent financial losses and damage to your reputation in the pharmaceutical industry.With the testo 184 data loggers, your products can be protected from unnoticed gaps in the cold chain, and the entire distribution path monitored and documented simply, securely and compliantly with all common standards, guidelines and regulations.
    atribut:
    • Memory: 64,000 Measuring values
    • Operating Temperature (°C): -20 to +70
    • Operating Time: Unlimited
    • Protection Class: IP30
    • Alarm Function: via LED and Display
    • Battery Life: 500 days (at +25 °C and 15 mins Measurement Rate).
    • Battery Type: Lithium battery CR2450, 3V, exchangeable
    • Certificate Type: Certified by HACCP International
    • Channels: 2 internal
    • Dimensions (mm): 97x40x12
    • Display Lighting: no
    • Display Size: one-line
    • Display Type: segment LCD
    • Interface: USB; NFC
    • Product Color : White
    • Product/Housing Material: ABS
    • Standards: CE 2014/30/EU; CFR 21 Part 11 (in use with testo ComSoft CFR-Software)
    • Storage Temperature: -55 to +70 °C
    • System Requirements: Adobe Acrobat Reader
    • Weight (g): 44
  7. TESTO Vibration, Humidity and Temperature Data Logger for Transport Monitoring
    Mulai

    Rp11.999.900

    TESTO Vibration, Humidity and Temperature Data Logger for Transport Monitoring
    Deskripsi:
    With the data loggers testo 184 G1 for shock, humidity and temperature, you can now monitor the transport of sensitive products such as electronics , art, pharmaceuticals or foods over an unlimited operating time. More info on applications (link to tab Applications)At their destination, a glance at the display or the LEDs tells you whether the configured limit values have been adhered to. In order to obtain detailed information, it is sufficient to connect the logger to a PC - a PDF report is immediately generated with all relevant data. In order for you to be able to work even more efficiently and conveniently with the data loggers, all required files and information are stored directly and securely in the testo 184 G1: Configuration file, instruction manual and PDF report of your recorded data.The measurement value store of the data logger testo 184 G1 for shock has a capacity of 1000 measurement values, for humidity and temperature 64000 measurement values. The measurement rate is freely selectable from 1 min to 24 h. The battery has a life of 120 days. The temperature data logger testo 184 G1 is supplied by a standard battery which can be exchanged by the user.testo 184 G1 is compliant with GxP, 21 CFR Part 11 and HACCP. Testo AG is an ISO 9001:2008-certified company, and ensures the adherence to the norms through internal audits as well as accredited external audits.All advantages at a glance:1. Clear alarm indicationA glance at the display or the LEDs is enough to know whether limit values have been violated during transport.2. Easiest operationtesto 184 G1 is intuitively operated, and can be used without special training or previous knowledge: The "Start" button begins data recording. "Stop" ends it.3. Easiest configurationIn each testo 184 G1, a configuration file is stored, with which the configuration of the testo 184 G1 is childsplay - no download, no installation, no user interface and no additional costs.4. Convenient readoutA PDF report with the transport data is created immediately on connection of the testo 184 G1 data logger to the USB interface of a computer. This is suitable for long-term archiving according to PDF/A standard.5. Mobile readout/printout on siteData transfer from the data logger to a compatible Testo fast printer (option) also functions wirelessly via NFC.6. IT-safeThe testo 184 G1 data loggers work securely without software installation or download, so that IT problems are triggered neither by the firewall nor the virus scanner.  Product Includes: Data logger for shock, humidity and temperature testo 184 G1 for transport monitoring, battery and wall bracket.Monitoring and documentation of temperature, humidity and shock in food logistics Handling foods involves danger to human health at all levels. In order to be able to eliminate them as far as possible, food companies must comply with an HACCP concept which guarantees food safety along the entire production chain – "from farm to fork". The adherence to product-specific limit values and the uninterrupted monitoring of the cold chain are crucial. In many cases, the monitoring of humidity and shock, in addition to temperature, are relevant for the maintenance of food quality.With the testo 184, quality managers in food logistics have six HACCP International-certified data loggers available to them, which monitor and document all critical parameters during the transport of foods. The data loggers testo 184 T1,T2, T3 and T4 have been additionally tested and certified according to EN 12830 by the TÜV Süd, and are therefore ideally suitable for the transport of refrigerated and deep-frozen foods. Monitoring and documentation of temperature, humidity and shock in logistic services of all kinds Providers of logistic service often take on the responsibility for expensive and sensitive products from the fields of pharmaceuticals, food, electronics or art. The wrong conditions during transport can lead to considerable losses of quality, right up to the complete devaluation of the monitored products.With the help of the testo 184 data logger, the prescribed temperature and humidity limit values as well as the shock tolerance levels can be monitored during transport, and thanks to the automatic report creation, very easily analyzed and documented. This allows all doubts regarding the correct transport conditions to be eliminated.Shock-sensitive products such as electronics, delicate machinery or certain bio-pharmaceuticals can be additionally monitored for the violation of previously defined shock limits with the help of the testo 184 G1. Monitoring and documentation of temperature, humidity and shock in pharmaceutical logistics Most pharmaceuticals must be continuously transported and stored at defined upper and lower temperature and humidity limit values, along the entire supply chain. A violation of these predefined upper and lower limit values can lead to irreversible alterations of the active ingredients or the composition of the medicaments. However, not only medicaments and their active ingredients are endangered. Minus temperatures or extreme temperature fluctuations can also cause damage to containers or medical instruments. The consequence is the threat of spoilage of the entire goods, financial losses and damage to reputation.In GxP-compliant quality management, the control of the entire cold chain, from production to delivery, is therefore a prerequisite, in order not only to ensure product quality, but also to prevent financial losses and damage to your reputation in the pharmaceutical industry.With the testo 184 data loggers, your products can be protected from unnoticed gaps in the cold chain, and the entire distribution path monitored and documented simply, securely and compliantly with all common standards, guidelines and regulations.
    atribut:
    • Memory: 64,000 Measurement values (Temperature and Humidity); 1,000 Measurement values (shock)
    • Operating Temperature (°C): -20 to +70
    • Operating Time: Unlimited
    • Protection Class: IP30
    • Alarm Function: via LED and Display
    • Battery Life: 120 days (at +25 °C and 15 min. Meas. cycle)
    • Battery Type: Lithium battery CR2450, 3V, exchangeable
    • Channels: 5 internal
    • Dimensions (mm): 97x40x12
    • Display Lighting: no
    • Display Size: one-line
    • Display Type: segment LCD
    • Interface: USB; NFC
    • Product Color : White
    • Product/Housing Material: ABS
    • Standards: CE 2014/30/EU; DIN EN 61326-1:2013; DIN EN 50581:2013; CFR 21 Part 11 (in use with testo ComSoft CFR-Software); HACCP International
    • Storage Temperature: -55 to +70 °C
    • System Requirements: Adobe Acrobat Reader
    • Weight (g): 44
  8. TESTO Mini Data Logger
    Mulai

    Rp6.099.900

    TESTO Mini Data Logger
    Deskripsi:
    Does your work involve the warehousing or storage of climate-sensitive items (food, drugs, archive media, museum exhibits, metal parts susceptible to rust film, etc.)? Or would you like to keep a check on the building climate, for example monitoring how your tenants use ventilation? Then continuous recording of temperature and humidity readings can be very useful for you. The testo 174H mini data logger for temperature and humidity provides you with competent support for this kind of measurement task. It may be small, but it achieves great (measurement) results.This is what the mini data logger for temperature and humidity offersThe current measuring values and any possible violations of limit values can be read on the mini data logger’s display. Its measurement data memory can reliably record up to 16¿000 measuring values. Saved measurement data will not be lost even when the battery is empty or being replaced.The testo 174H mini data logger has internal sensors which measure temperature and humidity. The humidity sensor is a capacitive Testo humidity sensor with long-term stability which has an accuracy of up to ±3 % RH when measuring humidity. With an accuracy of ±0.5 °C, the internal NTC temperature sensor is particularly high-precision and covers a measuring range from -20 to +70 °C.Particularly practical: the mini data logger runs on standard batteries (2x CR 2032) which you can replace yourself at any time.Programming and analysis with the data logger for temperature and humiditySoftware is used to programme and read your mini data logger as well as to analyze measurement data on the PC. You have a choice of three software versions: ComSoft Basic software - available as a free download - for fast programming of the mini data logger and easy analysis of measurement data ComSoft Professional software - can also be ordered as an option - offers a variety of possibilities for detailed analysis of temperature and humidity readings ComSoft CFR 21 Part 11 software - can also be ordered as an option - the best solution for special requirements according to CFR 21 Part 11 in the pharmaceutical sectorAdvantage of the set: the mini data logger is ready to use straight awayA USB interface is needed to programme and read your mini data logger for temperature and humidity. If you decide on this set, it includes a USB interface which means a speedy start for your measuring tasks.Attention: Please download the newest software version before using the USB interface for the first time. The software can be found in the download area. Product Includes: testo 174H mini data logger set for temperature and humidity, including USB interface for programming and reading the mini data logger, wall bracket, batteries (2 x CR 2032 lithium) and calibration protocol.Monitoring and documentation of building climate Temperature and relative humidity are crucial factors when it comes to assessing air quality and comfort levels in indoor areas, e.g. in workplaces. Both values can be monitored and documented over the long term using data loggers.They are also very well suited for checking ventilation systems or for assessing any building moisture which occurs.The use of special software means measurement configurations can be carried out individually and recorded measurement data can be both analysed and archived. Monitoring and documentation of storage temperature and humidity Correct compliance with storage temperature and humidity is an important prerequisite for the quality assurance of many products, e.g. in the area of food and pharmaceutical products.As a general rule, data loggers are used to do this. They automatically check and document the profile of the ambient conditions and thus make a crucial contribution to verifiable preservation of product quality.Viewing breaches of limit values directly on the display means you can respond quickly to temperature and humidity deviations. In addition, with the help of the configuration and read-out software, customer-specific measurement configurations can be carried out and recorded measurement data can be both analysed and archived. Monitoring and documentation of transport temperature and humidity For all goods which react sensitively to temperature and humidity fluctuations or have to be stored within a predefined range, uninterrupted measurement data recording and documentation play a major role.Incorrect conditions during transport can lead to major losses of quality, including the total loss of value of the products that require monitoring.Using a data logger, shipments can be checked for compliance with the specified temperature and humidity ranges and the data can then be read, analysed and archived by means of special software.
    atribut:
    • Measuring Rate: 1 min - 24 h
    • Memory: 16,000 Measuring values
    • Battery Type: 2x3V button cell (CR 2032)
    • Dimensions (mm): 60x38x18.5
    • Product/Housing Material: Plastic
    • Storage Temperature: -40 to +70 °C
  9. Amprobe Temperature and Relative Humidity Data Logger
    Mulai

    Rp8.299.900

    Amprobe Temperature and Relative Humidity Data Logger
    Deskripsi:
    Amprobe’s Model TR200-A takes both temperature and relative humidity readings in one compact size unit. Use the included Amprobe software for recording measurements to your personal computer. Set up these parameters for recording: sample interval timing, start/stop, date and time, hi/lo alarm threshold, unit selection, and number of memory points.
  10. Lascar Temperature Humidity Meter Data Logging
    Mulai

    Rp9.899.900

    Lascar Temperature Humidity Meter Data Logging
    Deskripsi:
    Temperature data loggers connect to temperature sensors or sense ambient temperatures and log measurements at set intervals. They can take multiple readings in different locations rapidly without manual data logging.
    atribut:
    • AC Current Accuracy: Not Applicable
    • AC Voltage Accuracy: Not Applicable
    • Accuracy (°C): +/-0.2
    • Accuracy (°F): +/-0.36
    • Battery Size: AAA
    • Current Channels: Not Applicable
    • DC Current Accuracy: Not Applicable
    • DC Voltage Accuracy: Not Applicable
    • Includes: Bracket
    • Interface: USB
    • Item: Temperature Humidity Data Logger
    • Maximum DC Voltage Measured: Not Applicable
    • Maximum Dew Point Measured: Not Applicable
    • Maximum Operating Temperature (°F): 131
    • Maximum Relative Humidity Measured (%): 100
    • Maximum Temperature Measured (°F): 131
    • Minimum DC Voltage Measured (V): Not Applicable
    • Minimum Dew Point Measured: Not Applicable
    • Minimum Operating Temperature (°F): -0.4
    • Minimum Relative Humidity Measured (%): Zero
    • Minimum Temperature Measured (°F): -0.4
    • Number of Voltage Channels: Not Applicable
    • Parameters Measured: Temperature Degrees C, Temperature Degrees F
    • UNSPSC: 41111906
  11. Kusam Meco Wall Mounting High-Precision Temperature & Humidity Data Logger
    Mulai

    Rp4.199.900

    Kusam Meco Wall Mounting High-Precision Temperature & Humidity Data Logger
    Deskripsi:
    Temperature and Humidity Data LoggersModel KM 9122 KM 9122 Temperature and Humidity Data Logger has internal high-precision sensors for temperature or temperature and humidity measurements. There is no need to install any software to automatically generate a PDF report. The device stores maximum 16000 measuring data automatically with selectable sampling intervals from 1s to 24h. It is also equipped with intelligent data analysis and management software for data download, graph checking and analysis, etc. This meter is designed with LCD, LED indicators & buttons. Real-time readings & alarm information can be displayed on LCD. The two LEDs flash in Red, Green & Yellow colors to indicate the status of working & alarming. It’s easy to operate with the two buttons to check data, start logging & clear data, etcMAX/MIN Function
    atribut:
    • Data Port: USB
    • Dimensions (HxWxT) (mm): Approx. 92x35x20
    • Display: LCD
    • Humidity Accuracy (%): ±2.2 RH
    • Humidity Range (%RH): 0-100
    • Humidity Resolution (%RH): 0.1
    • Power Supply: 1 x CR2450 3V Battery
    • Records: 16000 data
    • Sampling Rate: 1 second to 24 hours selectable
    • Software: included. Compatible with Windows Vista, Windows 2000/2003, Windows 7,8,10 systems
    • Temperature Accuracy (°C): ± 0.5
    • Temperature Range (°C): -30 to 70
    • Temperature Range (°F): -22 to 158
    • Temperature Resolution (°C): 0.1
    • Temperature Resolution (°F): 0.2
    • Waterproof Level: Ip65
  12. Extech Nonelectrical Properties Data Logger
    Mulai

    Rp2.299.900

  13. SUPCO Nonelectrical Properties Data Logger
    Mulai

    Rp899.900

  14. Tenmars Temperature Data Logger
    Mulai

    Rp5.599.900

    Tenmars Temperature Data Logger
    Deskripsi:
    - USB Datalogger- IP 54 Water Proof
  15. Oxford Precision Mini Humidity and Temperature Tester
    Mulai

    Rp889.900

    Oxford Precision Mini Humidity and Temperature Tester
    Deskripsi:
    UT330 series meters measure temperature and humidity with low power consumption and high precision. Measurement data to be saved and exported to PC software for further analysis. These meters can be used in factories, laboratories, research institutes, food, health, environmental protection, and other fields.
    atribut:
    • Resolution (°C): 0.1
    • Resolution (°F): 0.2
    • Accuracy (°C): ±1.0
    • Accuracy (°F): ±2.0
    • Dimensions (mm): 155x50x28
    • Battery (V): 4.5
    • Temperature Range (°C): -10 to 60
    • Temperature Range (°F): 14 to 140
  16. RS PRO Temperature & Humidity Data Logger
    Mulai

    Rp3.499.900

    RS PRO Temperature & Humidity Data Logger
    atribut:
    • Alarm: Yes
    • Best Humidity Measurement Accuracy: ±3.5 %RH
    • Data Logger Type: Temperature & Humidity
    • Maximum Humidity Measurement (%RH): 100
    • Number of Input Channels: 1
    • Power Source: Battery
  17. AS ONE Temperature and Humidity Data Logger
    Mulai

    Rp7.099.900

    AS ONE Temperature and Humidity Data Logger
    atribut:
    • Size (mm): 100.7x21.0x10.4
    • Maximum Record Capacity (points): 15000
  18. Extech Humidity/Temperature
    Mulai

    Rp4.299.900

    Extech Humidity/Temperature
    Deskripsi:
    HUMIDITY/TEMPERATUR USB DATALOGGER RHT10 adalah alat yang digunakan untuk mengukur jumlah air dan kelembaban dalam sebua h objek tertentu, selain kelembaban alat ini dapat digunakan untuk mengu kur aliran udara dan tingkat suhu suatu zat. Alat ini biasa digunakan untuk menentukan standar tertentu pada suatu perusahaan. Kelebihan lain alat ini adalah pengukuran yang dilakukan sangat presi si. Humidity me ter ini mempunyai humidity 0-100 % RH. Humidity meter sering digunakan di industri, pabrik, laboratorium, sekolah atau perkantoran.
  19. TESTO Temperature Data Logger for Transport Monitoring
    Mulai

    Rp2.099.900

    TESTO Temperature Data Logger for Transport Monitoring
    Deskripsi:
    Under normal conditions, the sublimation of dry ice takes place at -78.48 °C. With the temperature data loggers testo 184 t4, you can monitor the transport of pharmaceuticals with dry ice over an unlimited period of time and up to -80 °C. More info on applications (link to tab Applications)At their destination, a glance at the LEDs tells you whether the configured limit values have been adhered to. In order to obtain detailed information, it is sufficient to connect the logger to a PC - a PDF report is immediately generated with all relevant data. In order for you to be able to work even more efficiently and conveniently with the data loggers, all required files and information are stored directly and securely in the testo 184 T4: Configuration file, acceptance test certificate 3.1 according to DIN ISO 10204, instruction manual and PDF report of your recorded data.The measurement value store of the temperature data logger testo 184 T4 has a capacity of 40000 measurement values. The measurement rate is freely selectable from 1 min to 24 h. The battery has a life of 100 days (at -80 °C and 15 mins measurement rate). The temperature data logger testo 184 T4 is supplied by a standard battery which can be exchanged by the user.testo 184 T4 is compliant with GxP, 21 CFR Part 11, HACCP and EN 12830. Testo is an ISO 9001-certified company, and ensures the adherence to the norms through internal audits as well as accredited external audits.All advantages at a glance:1. Clear alarm indicationA glance at the the LEDs is enough to know whether limit values have been violated during transport. 2. Easiest operationtesto 184 T4 is intuitively operated, and can be used without special training or previous knowledge: The "Start" button begins data recording. "Stop" ends it. 3. Easiest configurationIn each testo 184 T4, a configuration file is stored, with which the configuration of the testo 184 T4 is childsplay - no download, no installation, no user interface and no additional costs. 4. Convenient readoutA PDF report with the transport data is created immediately on connection of the testo 184 T4 data logger to the USB interface of a computer. This is suitable for long-term archiving according to PDF/A standard. 5. Mobile readout/printout on siteData transfer from the data logger to a compatible Testo fast printer (option) also functions wirelessly via NFC. 6. IT-safeThe testo 184 T4 data loggers work securely without software installation or download, so that IT problems are triggered neither by the firewall nor the virus scanner. Product Includes: Temperature data logger testo 184 T4, including acceptance test certificate 3.1 according to DIN ISO 10204 (stored in testo 184 T4 ), battery and 1 piece double-sided adhesive tape for easy attachment of the data logger.Monitoring and documentation of temperature, humidity and shock in food logistics Handling foods involves danger to human health at all levels. In order to be able to eliminate them as far as possible, food companies must comply with an HACCP concept which guarantees food safety along the entire production chain – "from farm to fork". The adherence to product-specific limit values and the uninterrupted monitoring of the cold chain are crucial. In many cases, the monitoring of humidity and shock, in addition to temperature, are relevant for the maintenance of food quality.With the testo 184, quality managers in food logistics have six HACCP International-certified data loggers available to them, which monitor and document all critical parameters during the transport of foods. The data loggers testo 184 T1,T2, T3 and T4 have been additionally tested and certified according to EN 12830 by the TÜV Süd, and are therefore ideally suitable for the transport of refrigerated and deep-frozen foods. Monitoring and documentation of temperature, humidity and shock in logistic services of all kinds Providers of logistic service often take on the responsibility for expensive and sensitive products from the fields of pharmaceuticals, food, electronics or art. The wrong conditions during transport can lead to considerable losses of quality, right up to the complete devaluation of the monitored products.With the help of the testo 184 data logger, the prescribed temperature and humidity limit values as well as the shock tolerance levels can be monitored during transport, and thanks to the automatic report creation, very easily analyzed and documented. This allows all doubts regarding the correct transport conditions to be eliminated.Shock-sensitive products such as electronics, delicate machinery or certain bio-pharmaceuticals can be additionally monitored for the violation of previously defined shock limits with the help of the testo 184 G1. Monitoring and documentation of temperature, humidity and shock in pharmaceutical logistics Most pharmaceuticals must be continuously transported and stored at defined upper and lower temperature and humidity limit values, along the entire supply chain. A violation of these predefined upper and lower limit values can lead to irreversible alterations of the active ingredients or the composition of the medicaments. However, not only medicaments and their active ingredients are endangered. Minus temperatures or extreme temperature fluctuations can also cause damage to containers or medical instruments. The consequence is the threat of spoilage of the entire goods, financial losses and damage to reputation.In GxP-compliant quality management, the control of the entire cold chain, from production to delivery, is therefore a prerequisite, in order not only to ensure product quality, but also to prevent financial losses and damage to your reputation in the pharmaceutical industry.With the testo 184 data loggers, your products can be protected from unnoticed gaps in the cold chain, and the entire distribution path monitored and documented simply, securely and compliantly with all common standards, guidelines and regulations.
    atribut:
    • Protection Class: IP67
    • Certificate Type: Certified by HACCP International
    • Channels: 1 internal
    • Interface: USB; NFC
    • Product Color : White
    • Product/Housing Material: ABS
    • System Requirements: Adobe Acrobat Reader
Daftar Harga Data Logger Temperature Humidity Terbaru November 2026
Elitech Temperature Data LoggerRp519.900
TESTO Temperature and Humidity Data LoggerRp9.999.900
Comark Temperature & Humidity Data LoggerRp19.999.900
TESTO Absolute Pressure, Temperature and Humidity Data LoggerRp24.999.900
Besantek Wireless Temperature and Humidity Data LoggerRp47.999.900
TESTO Air Humidity and Temperature Data LoggerRp7.599.900
TESTO Vibration, Humidity and Temperature Data Logger for Transport MonitoringRp11.999.900
TESTO Mini Data LoggerRp6.099.900
Amprobe Temperature and Relative Humidity Data LoggerRp8.299.900
Lascar Temperature Humidity Meter Data LoggingRp9.899.900

Data diperbarui pada 12/11/2026 (Harga belum termasuk PPN)