Beli bt40 di monotaro.id

Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
  1. Terragene Bionova Biological Indicator Spore Strip
    Mulai

    Rp4.799.900

    Terragene Bionova Biological Indicator Spore Strip
    Deskripsi:
    BT40/6 / Spore Strips Biological Indicator for Ethylene Oxide and Dry Heat sterilization processes. Bacillus atrophaeus (ATCC 9372) 10^6 spores per strip.The envelope containing Bionova® BT40 Spore Strip is specifically designed for the monitoring of Ethylene Oxide (EO) sterilization processes or for Dry Heat sterilization processes.Spore strips should be incubated in Bionova® MC1030-2, Bionova® MC1020-2 Growth Medium tube or in appropriate growth medium for Bacillus atrophaeus ATCC 9372 growth. If the sterilization process was not successful, Bionova® MC1030-2 or Bionova® MC1020-2 growth medium will turn to yellow after incubation at 37±2 ºC, thus indicating the existence of living Bacillus atrophaeus spores on the strip.If the sterilization process was successful, MC1030-2 or MC1020-2 Indicating Medium will remain its original color. A final readout should therefore be performed after 48 hours of growth medium incubation at 37±2 ºC.Instructions for use1. Identify Bionova® BT40 envelope by writing on its back the sterilizer number (in case of having more than one), load number and processing date.2. Pack it in appropriate package along with material to be sterilized, according to recommended sterilization practices. Place the envelope in those areas you a priori consider more inaccessible for sterilizing agent. A typical problematic area is the load center.3. Sterilize as usual.4. After the sterilization process has finished, you can:A. Remove the Bionova® BT40 envelope from the package for processing and incubation.B. For Ethylene Oxide sterilization, you can aerate the package containing the biological indicator with the rest of the load or remove the biological indicator from the sterilization package for incubation in MC1030-2, MC1020-2 culture medium or any other appropriate growth medium prior to material aeration.5. Tear up the envelope at one end very carefully under sterility conditions (eg. laminar flow cabinet) and transfer spore strip with a sterile clamp to MC1030-2, MC1020-2 Growth Medium tube, or to any other appropriate growth medium.IMPORTANT! Use latex gloves and chin strap when transferring spore strips from the envelope to growth medium tube. WARNING! Avoid spore strip contact with any kind of surface including the outer part of growth medium tube and of Bionova® BT40 envelope.IMPORTANT: Use a non-sterilized spore strip as a positive control at least once per day, when a sterilization cycle is run. Both, processed spore strip and the strip used as positive control must belong to the same batch. Positive control guarantees that the incubation was carried out under appropriate conditions.6. Incubate processed spore strips along with the strip used as positive control during a maximum of 48 hours at 37±2 ºC. It is advisable to make observations every 10 hours. Color change of MC1030-2 or MC1020-2 Growth medium to yellow means a failure on sterilization process.If after 48 hours no colour change is visible on MC1030-2 or MC1020-2 Growth Medium, the result is negative (i.e. the sterilization process was successful). MC1030-2 or MC1020-2 Indicating Medium used for incubating the spores strips which have not been sterilized (positive control) should turn to yellow in order for the results to be valid.
  2. VIPER Polisher High Speed (Mesin Poles Lantai)
    Mulai

    Rp36.999.900

    VIPER Polisher High Speed (Mesin Poles Lantai)
    atribut:
    • Speed (rpm): 1500
    • Pad Size (mm): 510
    • Voltage (V): 220
    • Dimensions (mm): 820x570x1260
    • Power Consumption (W): 1100
  3. Terragene Bionova Biological Indicator
    Mulai

    Rp709.900

    Terragene Bionova Biological Indicator
    Deskripsi:
    BT20 / Self-contained Biological Indicator for Steam sterilization processes. Geobacillus stearothermophilus (ATCC 7953) 10^5 or 10^6 spores per vial. Readout: 24 hours.Monitoring vacuum-assisted and gravity air-displacement Steam Sterilization processes at 121-135 °C.Instructions for use1. Identify the Bionova® BT20 Indicator by writing the sterilizer number (in case of having more than one), load number and processing date on the indicator label.2. Pack the biological indicator along with materials to be sterilized in an appropriate package according to recommended sterilization practices. Place this package in those areas which a priori you consider most inaccessible for the sterilizing agent (Steam). Generally, the center of the load and areas near the door are problematic.3. Sterilize as usual.4. After the sterilization process has finished, open the sterilizer door, wait for 5 minutes and remove the biological indicator from the package. CAUTION: Wear safety glasses and gloves when removing the Bionova® BT20 Biological Indicator from the sterilized package. WARNING: Do not crush or handle the biological indicator excessively, since this might cause the glass ampoule to burst.5. Allow the biological indicator to cool down to room temperature.6. Check the chemical indicator on the label of the biological indicator. A color change to brown confirms that the biological indicator has been exposed to steam. IMPORTANT: this color change does not indicate that the process was sufficient to achieve sterility. If the chemical indicator is unchanged, check the sterilization process.7. Crush the ampoule contained in the biological indicator with an individual ampoule crusher or with the ampoule crusher placed within the top of the incubator´s incubation area. Then shake the tube down vigorously, with movements similar to those performed to lower the temperature of a mercury thermometer, until the medium reaches the base of the tube and soaks the spore carrier entirely. Finally, place the biological indicator in the incubator.IMPORTANT: Use a non-sterilized biological indicator as a positive control at least once per day, when a sterilization cycle is run. The positive control ensures that appropriate incubation conditions were met. Both the positive control indicator and the processed indicator should belong to the same batch.8. Incubate the processed biological indicator and the indicator used as a positive control for a maximum of 24 hours between 55-62 ºC. Readout should be carried out at convenient intervals of 10 hours. Color change of the growth indicator medium from purple to yellow means that a sterilization process failure has occurred.If at 24 hours there is no color change in the processed indicators, a final negative result is obtained (the sterilization process was effective). The positive control indicator should show a purple to yellow color change for the results to be valid. NOTE: To extend the incubation time beyond 24 hours, we recommend using a humidified environment to prevent complete evaporation of the culture medium contained within the indicator.
  4. YG1 ER Collet Chuck
    Mulai

    Rp1.299.900

  5. Terragene Sterilized Indicator ISO 11140 -1 compliant
    Mulai

    Rp389.900

    Terragene Sterilized Indicator ISO 11140 -1 compliant
    atribut:
    • Expiration Date: 5 years after manufacturing.
    • Storage Method: 10 to 30° C/Humidity RH 30 to 80% (Places away from direct sunlight.)
    • Type: ISO 11140 -1 Type 4
  6. Terragene Tape Indicator Chemical (Isolasi Indikator)
    Mulai

    Rp389.900

    Terragene Tape Indicator Chemical (Isolasi Indikator)
    Deskripsi:
    CT22 / Indicator Tape for Steam sterilization processes.Cintape® CT22 Process Indicators (Type 1 according ISO 11140-1:2014 standard) aresingle-use chemical indicators that consist of a roll of self-adhesive paper tape printed with indicator ink.These indicators have been designed to monitor Steam sterilization processes, ensuring an adequate exposure to the sterilizing agent during the sterilization process and allowing to distinguish between processed and unprocessed items.The adhesive component of the tape allows the adhesion to different types of packaging and wraps, such as cloth, paper and plastic being easy to remove and leaving no residues. Innovative highly sensitive yellow ink was developed to turn to dark brown / black when the indicator is exposed to Steam. Endpoint condition: 121 ºC, 10 minutes; 134 ºC, 2 minutes.Instructions for Use1. Place within a sterilizer a wrapped package closed with Cintape® CT22 Process Indicator tape that will be sterilized by Steam.2. Perform the sterilization cycle.3. After the sterilization process has finished, remove the package from the sterilizer and analyze the indicator results. The indicator must turn to the reference color for considering that it was exposed to Steam. For reference color, please refer to Result Reference Guide.
    atribut:
    • Indicator Type: Type 1 Chemical Indicator
    • Regulations: ISO 11140-1
  7. Vertex Collet Holders with BT Taper Shank
    Mulai

    Rp1.999.900

    Vertex Collet Holders with BT Taper Shank
    Deskripsi:
    Accuracy Runout 0.005 mm Taper Shank At-3 R.P.M. 7000
    atribut:
    • Measurement Type: Metric
    • Taper: BT-40
    • Draw Bar Threads Metric: M16x2.0P, M22x1.5P
  8. Sandvik MAS-BT 403 to ER Collet Chuck (Chuck Kolet)
    Mulai

    Rp2.799.900

    Sandvik MAS-BT 403 to ER Collet Chuck (Chuck Kolet)
    atribut:
    • Coolant Pressure (CP) (bar): 80
  9. NIKKEN Milling Chuck (Chuck Pahat Frais)
    Mulai

    Rp4.899.900

    NIKKEN Milling Chuck (Chuck Pahat Frais)
    atribut:
    • Applicable Collet: CCK20, CCNK20, KM20, NK20
    • Shank: BT40
    • Taper No.: 40
    • Chuck Inner Diameter D (phi mm): 20
    • Dimension C₁ (mm): 52
    • Dimension L (mm): 120
    • Dimension L1 (inch): 80
    • Mass (kg): 2.2
  10. Vertex Intergrated Type Keyless Drill Chuck
    Mulai

    Rp1.899.900

    Vertex Intergrated Type Keyless Drill Chuck
    Deskripsi:
    The main-shafts is of integrated type, which is much more superior than the traditional design.The major features are as follows:Extremely rigid construction.The accumulative tolerances can be reduced to a minimum, since the traditional mechanism requiring an AROBOR to connect the Drill Chucks which will generate the accumulative tolerances.The Integrated type Keyless Drill Chuck is designed to solve this problem totally.Prevent the Drill Chucks from falling out.Extremely safe in operation.
    atribut:
    • Chuck Type: Integrated Type
    • Key Size: keyless
  11. monotaro.id Sepatu Safety Antistatik Slip Papua PU (Sepatu Proyek)
    Mulai

    Rp349.900

    monotaro.id Sepatu Safety Antistatik Slip Papua PU (Sepatu Proyek)
    atribut:
    • Color: White
    • Upper: Synthetic Leather
    • Outsole: Single Density PU
    • Slip Sole: Anti Static
    • Logo Tag: Direct TPR Injection
    • Model : Low Cut Slip-On Shoes
    • SNI License: Yes
    • SNI Number: SNI Number: JPA 009 016.5
    • Series: Papua
    • Toe Cap: Steel
  12. YG1 Straight Shank Gold-P Drill Regular D1GP191 Series (Mata Bor Lurus)
    Mulai

    Rp13.900

    YG1 Straight Shank Gold-P Drill Regular D1GP191 Series (Mata Bor Lurus)
    Deskripsi:
    Flute Geometry : Right Hand HelixPoint Angle : 135° under 1.6mm : Normal Point 1.6mm & Over : Split PointSurface Treatment : TiN-tip coatingApplication : Drilling in Stainless Steels, Material of difficult machinability such as titanium Alloy and Inconel
    atribut:
    • Point Angle (°): 118
  13. Mesa Labs Biological Indicator (Mesa Labs)
    Mulai

    Rp6.999.900

    Mesa Labs Biological Indicator (Mesa Labs)
    Deskripsi:
    The glassine paper used for the primary packaging has approximately 200 meshes per 1mm2, which allows gas to flow in and out easily, but it also prevents bacteria from entering from the outside and spores from scattering from the inside.Conforms to US Pharmacopeia 23 (FDA 510K), USP standards, AAMI standards, GMP standards, European EN standards, ISO standards, etc.
  14. Vertex Clamping Kit
    Mulai

    Rp2.799.900

    Vertex Clamping Kit
    Deskripsi:
    52-Pc Steel Clamping Kit.
Daftar Harga bt40 Terbaru October 2026
YG1 ER Collet Chuck JIS B6339/MAS 403 BT (Chuck Kolet)Rp1.299.900
YG1 ER Collet Chuck BT SeriesRp2.099.900
Terragene Bionova Biological Indicator Spore StripRp4.799.900
VIPER Polisher High Speed (Mesin Poles Lantai)Rp36.999.900
NIKKEN Multi-Lock Milling Chuck (Holder Pahat Frais)Rp5.399.900
Terragene Bionova Biological IndicatorRp709.900
YG1 Face Mill Arbor CBT (Arbor Pisau Frais)Rp2.599.900
YG1 ER Collet ChuckRp1.299.900
Terragene Sterilized Indicator ISO 11140 -1 compliantRp389.900
Terragene Tape Indicator Chemical (Isolasi Indikator)Rp389.900

Data diperbarui pada 09/10/2026 (Harga belum termasuk PPN)