Beli round belt di monotaro.id
Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
- BANDO Bang Cord Round Belt # 480 (Orange)Deskripsi:It is a standard product of round belt (Orange).Because it can be joined simply and strongly by thermal fusion, a belt of the required length can be obtained when necessary.Multi-axis transmission, 3D transmission possible.
- EAGLE BELTING Round BeltDeskripsi:Hollow-core smooth round belts can be joined at their ends with barb-style connectors to create a closed-loop belt without welding. The belt's smooth surface is suitable for conveying applications that require washdown, and they are often used in food processing applications.
- BANDO Bancoran Round BeltDeskripsi:Bando memiliki range produk Bancoran Round Belt yang lengkap dengan panjang 100-460mm digunakan untuk kebutuhan transmisi industri otomotif, mesin industri dan pabrik lainnyaatribut:
- Type: Round belt
- Material: Polyurethane
- BANDO Ban Code Endless # 480 Phi 10Deskripsi:It is a standard product of round belt (Orange). Since it fuses and it processes endless, it can be used as it is. Multi-axis transmission, 3D transmission possible. Because it can be joined simply and firmly by heating, you can freely select the required belt length without sticking to the standard. Since there is no directionality in the cross section, three-dimensional complex transmission such as multi-axis transmission and direction change by idler pulley is possible. It can be attached without disassembling the machine, and less management such as tightening adjustment. Bancoran (polyurethane) excellent in wear resistance and tear resistance is used, and it has excellent mechanical properties.
- BANDO Ban Code Endless # 480 Phi 5Deskripsi:It is a standard product of round belt (Orange). Since it fuses and it processes endless, it can be used as it is. Multi-axis transmission, 3D transmission possible. Because it can be joined simply and firmly by heating, you can freely select the required belt length without sticking to the standard. Since there is no directionality in the cross section, three-dimensional complex transmission such as multi-axis transmission and direction change by idler pulley is possible. It can be attached without disassembling the machine, and less management such as tightening adjustment. Bancoran (polyurethane) excellent in wear resistance and tear resistance is used, and it has excellent mechanical properties.
- BANDO Ban Code Endless # 480 Phi 6Deskripsi:It is a standard product of round belt (Orange). Since it fuses and it processes endless, it can be used as it is. Multi-axis transmission, 3D transmission possible. Because it can be joined simply and firmly by heating, you can freely select the required belt length without sticking to the standard. Since there is no directionality in the cross section, three-dimensional complex transmission such as multi-axis transmission and direction change by idler pulley is possible. It can be attached without disassembling the machine, and less management such as tightening adjustment. Bancoran (polyurethane) excellent in wear resistance and tear resistance is used, and it has excellent mechanical properties.
- Mitsuboshi Star RopeDeskripsi:Belt is thin, since it has excellent flexibility, small pulley diameter can be used, can be a compact design.. The weight is reduced by as thin as possible the belt. The influence of the centrifugal force can correspond to less high-speed rotation. (Belt is the best: You can use up to 60m / sec). By the manufacturing method it is possible to suppress the growth of the belt extremely (Pat.), There is almost no need to re-tension the belt.. Since the transmission capacity of the belt is large, you can narrow design of the belt width. In addition, in order to use the flat pulley, there is no need for processing of extra pulley.. Since the thickness of the belt is uniform, vibration is small, it can smooth operation.. Because it is a synthetic rubber of special compounding, heat resistance, excellent oil resistance, to prevent the generation of static electricity.atribut:
- Maximum Speed: less than 10m/s
- BANDO Ban Code Endless # 480 Phi 8Deskripsi:It is a standard product of round belt (Orange). Since it fuses and it processes endless, it can be used as it is. Multi-axis transmission, 3D transmission possible. Because it can be joined simply and firmly by heating, you can freely select the required belt length without sticking to the standard. Since there is no directionality in the cross section, three-dimensional complex transmission such as multi-axis transmission and direction change by idler pulley is possible. It can be attached without disassembling the machine, and less management such as tightening adjustment. Bancoran (polyurethane) excellent in wear resistance and tear resistance is used, and it has excellent mechanical properties.
- BANDO Ban Code Endless # 480 Phi 3Deskripsi:It is a standard product of round belt (Orange). Since it fuses and it processes endless, it can be used as it is. Multi-axis transmission, 3D transmission possible. Because it can be joined simply and firmly by heating, you can freely select the required belt length without sticking to the standard. Since there is no directionality in the cross section, three-dimensional complex transmission such as multi-axis transmission and direction change by idler pulley is possible. It can be attached without disassembling the machine, and less management such as tightening adjustment. Bancoran (polyurethane) excellent in wear resistance and tear resistance is used, and it has excellent mechanical properties.
- BANDO Ban Code Endless # 480 Phi 12Deskripsi:It is a standard product of round belt (Orange). Since it fuses and it processes endless, it can be used as it is. Multi-axis transmission, 3D transmission possible. Because it can be joined simply and firmly by heating, you can freely select the required belt length without sticking to the standard. Since there is no directionality in the cross section, three-dimensional complex transmission such as multi-axis transmission and direction change by idler pulley is possible. It can be attached without disassembling the machine, and less management such as tightening adjustment. Bancoran (polyurethane) excellent in wear resistance and tear resistance is used, and it has excellent mechanical properties.
- BANDO Bang Cord Round Belt # 489 (White)Deskripsi:Because it can be joined simply and strongly by thermal fusion, a belt of the required length can be obtained when necessary.Multi-axis transmission, 3D transmission possible.
- BANDO Vancode Dedicated AdhesiveDeskripsi:Please use the exclusive bonding machine DX - 81 for van code bonding.atribut:
- Temperature: 240 +/- 10° c
- Gates Unitta Asia Urethane cordatribut:
- Color: Orange
- BANDO Ban Code Endless # 480 Phi 1.5Deskripsi:It is a standard product of round belt (Orange). Since it fuses and it processes endless, it can be used as it is. Multi-axis transmission, 3D transmission possible. Because it can be joined simply and firmly by heating, you can freely select the required belt length without sticking to the standard. Since there is no directionality in the cross section, three-dimensional complex transmission such as multi-axis transmission and direction change by idler pulley is possible. It can be attached without disassembling the machine, and less management such as tightening adjustment. Bancoran (polyurethane) excellent in wear resistance and tear resistance is used, and it has excellent mechanical properties.
- Camelion Rechargable Battery Ni-MH (Baterai)atribut:
- Voltage (V): 1.2
- BANDO Bancoran V-BeltDeskripsi:Bando memiliki range produk Bancoran V-Belt yang lengkap dengan panjang 250-800mm digunakan untuk kebutuhan transmisi industri otomotif, mesin industri dan pabrik lainnyaatribut:
- Material: Polyurethane
- Type: V belt
- Belt Height: 4mm
- Belt width: 6mm
- BANDO Rib Ace Belt Type 4PKDeskripsi:Produk Rib Ace Belt Type 4PK dari Bando ini memiliki range panjang dari 1000-1980mm cocok digunakan pada mesin-mesin transmisi mobil, bus, truk dan otomotif lainnyaatribut:
- Material: Rubber
- Angle (°): 40°
- Center Distance (mm): 3.56
- Number of Ribs: 4
- Thickness (mm): 4.8
Daftar Harga round belt Terbaru March 2026
| BANDO Bang Cord Round Belt # 480 (Orange) | Rp119.900 |
| EAGLE BELTING Round Belt | Rp389.900 |
| BANDO Bancoran Round Belt | Rp68.900 |
| BANDO Ban Code Endless # 480 Phi 10 | Rp589.900 |
| BANDO Ban Code Endless # 480 Phi 5 | Rp179.900 |
| BANDO Ban Code Endless # 480 Phi 6 | Rp289.900 |
| BANDO Bancollan Round Belt | Rp44.900 |
| Mitsuboshi Star Rope | Rp28.900 |
| BANDO Ban Code Endless # 480 Phi 8 | Rp419.900 |
| BANDO Ban Code Endless # 480 Phi 3 | Rp129.900 |
Data diperbarui pada 07/03/2026 (Harga belum termasuk PPN)



















































































































































/P102362460-1.jpg)










/P102362503-1.jpg)




/ngP103204844-9.jpg)
/Epson%20Pita%20Tinta%20Printer/P101502861-11.jpg)