Beli Timbangan Protein di monotaro.id

Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
  1. Termic Timbangan Digital
    Mulai

    Rp85.900

    Termic Timbangan Digital
    atribut:
    • Max. Capacity Weight (kg): 180
    • Power Battery: 2xAAA
    • Display: LCD
  2. Master Flex Silicone Tube (Selang Silikon)
    Mulai

    Rp1.199.900

    Master Flex Silicone Tube (Selang Silikon)
    Deskripsi:
    Excellent biocompatibility that meets multiple classifications.Genuine Masterflex tubing undergoes robust testing to provide optimal performance / pump life hours with peristaltic pump equipment Precision extruded to tight tolerances for high repeatability, accuracy and reproducibility Global market leader in range of formulations for most extensive chemical compatibility Single-use custom lengths and configurations available to minimize downtime Regulatory approvals to match your unique application Always in stock-most formulations and sizes available to ship same day Unique packaging options include packs, cases, and spools for customer-friendly ordering and delivery Slightly greater clarity than peroxide-cured tubing Smooth surfaces; lower protein binding levelsFewer potential leachablesTubing Size: L/S 13Applications: Pharmaceutical, biotech, peristaltic pumping, and food applicationsCharacteristics: Excellent heat resistance, low compression set, odorless, nontoxic, translucentFor use with Masterflex multichannel pump heads.For custom tubing lengths and configurations, please contact us. We can provide the tubing type, length, and quantity you need.
  3. Ultra Milk Susu UHT Full Cream
    Rating:
    99% of 100
    (19)
    Mulai

    Rp5.900

  4. TESTO Ph Meter
    Mulai

    Rp12.999.900

    TESTO Ph Meter
    Deskripsi:
    The cosmetics industry, the food industry, the metal industry: the testo 206-pH2 pH meter can be used virtually anywhere. That’s because it’s ideally suited for measuring the pH value of semi-solid media like, for example:Viscous and protein-containing foodstuffs like jelly, cheese, fruit etc.Liquid and soft or paste-like materials like creams and oilsWater-mixed solid cooling lubricantsClever measurement technology paired with intelligent features: the testo 206-pH2 pH meterThe testo 206-pH2 pH meter is equipped with a pH immersion tip and an integrated temperature sensor which allow you to carry out quick and reliable pH measurements and accurate core temperature measurements simultaneously. Thanks to the full-size gel electrolyte volume and annular clearance, the pH sensor is not only leakproof and maintenance-free, but also extremely durable and insensitive to dirt.   The testo 206-pH2 allows you to perform 1, 2 or 3-point calibrations. The automatic final value recognition function supports you throughout your measurements.Hygienic and ruggedThe testo 206-pH2 pH meter comes with a TopSafe protective case which gives it its IP68 rating: the hygienic, dishwasher safe case protects the meter against dirt, water and impact.Product Includes: testo 206-pH2 pH meter for viscous media, gel storage cap, TopSafe protective case, belt buckle, wall bracket.pH measurement for drinking water analysis There have been statutory European directives from as early as 1980, which have regulated the limit values of specific parameters in drinking water. The Drinking Water Ordinance of 21 May 2001 in Germany decreed that water supply companies are obliged to provide their customers with drinking water which complies with the quality laid down in the Drinking Water Ordinance. The pH value is an important parameter for determining water quality.The water samples taken must be checked for their pH value directly or immediately after sampling. This must not exceed the acidic limit of 6.5 or the alkaline limit of 9.5 and should normally be in the neutral range around 7.The advantages of the testo 206 one-hand pH measuring instrument: Direct measurement on site for fast assessment of the pH value Available in three different models (including a version with plug-in probes for easy remote measurement)Robust, waterproof "TopSafe” protective cover (protection class IP68) Built-in temperature probe for simultaneous measurement of two parametersMaintenance-free gel electrolyte pH measurement for quality assurance in the food sector The pH value of foods has a direct effect on the growth of microorganisms and therefore on food quality and safety. For this reason, many companies use the pH value as a quality characteristic for evaluating their food. For example, the pH value is of great importance in the manufacture of meat, sausage, delicatessen and dairy products.The pH value is an important quality parameter in the food sector. It particularly affects the properties of meat and meat-based products, especially with regard to water binding capacity, taste, colour, tenderness and shelf life. In the bakery sector, the acidity of the sourdough can be determined by means of the pH value. In the case of products such as salad dressings, the pH value helps to ensure consistent quality or consistent acidity of the product.The advantages of the testo 206 one-hand pH measuring instrument: Direct measurement in process / in the food for fast assessment of the pH value Available in three different versions – depending on the medium in which the measurement is being madeRobust, waterproof and dishwasher-safe "TopSafe” protective cover (protection class IP68) Built-in temperature probe for simultaneous measurement of pH and temperature valuesMaintenance-free gel electrolyte1, 2 or 3-point calibration possible pH measment inure the cosmetics industry The pH value is a crucial factor when it comes to assessing the quality of cosmetic products. Cosmetic products which are too acidic or too alkaline can cause skin irritations or rashes. The pH value of the skin is normally between 5 and 6.5 thanks to its natural protective acid mantle. "Skin-neutral” cleansers are actually slightly acidic and can support the skin's protective acid mantle, which is particularly important for people with sensitive skin. On the other hand, alkaline cleansers could encourage the skin's process of replenishing its natural oils.The pH value of cosmetics must therefore be monitored, controlled and, if necessary, adjusted right from the production stage, so that the end product has the required value. The testo 206 one-hand pH measuring instrument helps you to do this through: Direct measurement in process for fast assessment of the pH value Three different versions of the product – depending on the medium in which the measurement is being made (e.g. liquid, paste-like, etc.)Robust, waterproof and dishwasher-safe "TopSafe” protective cover (protection class IP68) to meet strict cleaning requirements in the pharmaceutical sector.Built-in temperature probe for simultaneous measurement of two parametersMaintenance-free gel electrolyte1, 2 or 3-point calibration possible
    atribut:
    • Measuring Rate: 2 Measurements per second
    • Number of Channels: 2-channel
    • Operating Temperature: 0 to +60 °C
    • Protection Class: IP68
    • Authorizations: CE 2014/30/EU
    • Battery Life: 80 h (Auto Off 10 min)
    • Battery Type: 1xCR2032
    • Diameter Probe shaft (mm): 11
    • Dimensions (mm): 197x33x20 110x33x20 (without Probe and TopSafe)
    • Display Size: 2 lines
    • Display Type: LCD (Liquid Crystal Display)
    • Length Probe shaft (mm): 35
    • Product Color : White
    • Product/Housing Material: ABS
    • Storage Temperature: -20 to +70 °C
    • Temperature Compensation: automatic
    • Weight (g): 115 (with TopSafe) 65 (without TopSafe)
  5. TESTO Ph/Temperature Measuring Instrument
    Rating:
    100% of 100
    (1)
    Mulai

    Rp4.799.900

    TESTO Ph/Temperature Measuring Instrument
    Deskripsi:
    The cosmetics industry, the food industry, the metal industry: the testo 206-pH2 pH/temperature measuring instrument can be used virtually anywhere. That’s because it’s ideally suited for measuring the pH value of semi-solid media like, for example: Viscous and protein-containing foodstuffs like jelly, cheese, fruit etc. Liquid and soft or paste-like materials like creams and oils Water-mixed solid cooling lubricantsClever measuring technology: the testo 206-pH2 starter set for pH/temperature measurementThe testo 206-pH2 pH/temperature measuring instrument is equipped with a pH immersion tip and an integrated temperature sensor which allow you to carry out quick and reliable pH measurements and accurate core temperature measurements simultaneously.Thanks to the full-size gel electrolyte volume and annular clearance, the pH sensor is not only leakproof and maintenance-free, but also extremely durable and insensitive to dirt.  Calibration dosing bottles: Our DAkkS-certified calibration solutions are suitable for calibrating the pH probe. The pH probe is calibrated in the integrated dosing aperture of the calibration dosing bottle. This guarantees economical use of the calibration solution.The automatic final value recognition function supports you throughout your measurements.Hygienic and ruggedThe testo 206-pH2 pH/temperature measuring instrument comes with a TopSafe protective case which gives it its IP68 rating: the hygienic, dishwasher safe case protects the instrument against dirt, water and impact.The aluminium case protects your pH/temperature measuring instrument during transport and storage. Product Includes: Starter set testo 206-pH2 pH/temperature measuring instrument, pH2 probe head for semi-solid substances, incl. storage cap with gel, calibration dosing bottles 250 ml pH 4 and 7, TopSafe, belt/wall holder and aluminium case.pH measurement for drinking water analysis There have been statutory European directives from as early as 1980, which have regulated the limit values of specific parameters in drinking water. The Drinking Water Ordinance of 21 May 2001 in Germany decreed that water supply companies are obliged to provide their customers with drinking water which complies with the quality laid down in the Drinking Water Ordinance. The pH value is an important parameter for determining water quality.The water samples taken must be checked for their pH value directly or immediately after sampling. This must not exceed the acidic limit of 6.5 or the alkaline limit of 9.5 and should normally be in the neutral range around 7.The advantages of the testo 206 one-hand pH measuring instrument: Direct measurement on site for fast assessment of the pH value Available in three different models (including a version with plug-in probes for easy remote measurement)Robust, waterproof "TopSafe” protective cover (protection class IP68) Built-in temperature probe for simultaneous measurement of two parametersMaintenance-free gel electrolyte pH measurement for quality assurance in the food sector The pH value of foods has a direct effect on the growth of microorganisms and therefore on food quality and safety. For this reason, many companies use the pH value as a quality characteristic for evaluating their food. For example, the pH value is of great importance in the manufacture of meat, sausage, delicatessen and dairy products.The pH value is an important quality parameter in the food sector. It particularly affects the properties of meat and meat-based products, especially with regard to water binding capacity, taste, colour, tenderness and shelf life. In the bakery sector, the acidity of the sourdough can be determined by means of the pH value. In the case of products such as salad dressings, the pH value helps to ensure consistent quality or consistent acidity of the product.The advantages of the testo 206 one-hand pH measuring instrument: Direct measurement in process / in the food for fast assessment of the pH value Available in three different versions – depending on the medium in which the measurement is being madeRobust, waterproof and dishwasher-safe "TopSafe” protective cover (protection class IP68) Built-in temperature probe for simultaneous measurement of pH and temperature valuesMaintenance-free gel electrolyte1, 2 or 3-point calibration possible pH measment inure the cosmetics industry The pH value is a crucial factor when it comes to assessing the quality of cosmetic products. Cosmetic products which are too acidic or too alkaline can cause skin irritations or rashes. The pH value of the skin is normally between 5 and 6.5 thanks to its natural protective acid mantle. "Skin-neutral” cleansers are actually slightly acidic and can support the skin's protective acid mantle, which is particularly important for people with sensitive skin. On the other hand, alkaline cleansers could encourage the skin's process of replenishing its natural oils.The pH value of cosmetics must therefore be monitored, controlled and, if necessary, adjusted right from the production stage, so that the end product has the required value. The testo 206 one-hand pH measuring instrument helps you to do this through: Direct measurement in process for fast assessment of the pH value Three different versions of the product – depending on the medium in which the measurement is being made (e.g. liquid, paste-like, etc.)Robust, waterproof and dishwasher-safe "TopSafe” protective cover (protection class IP68) to meet strict cleaning requirements in the pharmaceutical sector.Built-in temperature probe for simultaneous measurement of two parametersMaintenance-free gel electrolyte1, 2 or 3-point calibration possible
    atribut:
    • Measuring Rate: 2 Measurements per second
    • Display Size: 2 lines
    • Display Type: LCD (Liquid Crystal Display)
    • Product Color : White
    • Product/Housing Material: ABS
    • Storage Temperature: -20 to +70 °C
  6. Ultra Milk Susu UHT Coklat
    Rating:
    99% of 100
    (27)
    Mulai

    Rp5.900

    Ultra Milk Susu UHT Coklat
    atribut:
    • Flavor: Chocolate
  7. Lipton Teh Celup Sir Thomas
    Rating:
    100% of 100
    (2)
    Mulai

    Rp69.900

    Lipton Teh Celup Sir Thomas
    Deskripsi:
    Aroma bunga yang ditemukan dalam teh aromatik memastikan ketenangkan jiwa anda. Dapat lebih enak jika ditambah dengan sedikit manisnya madu. secara alami bebas kafein Koleksi Teh Istimewa Sir Thomas Lipton menawarkan bahan-bahan terbaik yang dikemas dalam sachet tertutup untuk menjaga kualitas, kesegaran dan memastikan konsistensi aroma. Koleksi ini membantu menciptakan pengalaman teh yang sempurna untuk setiap saat, setiap kesempatan termasuk di ruangan (pojok teh), sarapan, restoran, kafe, bar, lounge, banquet dan tempat-tempat lainnya.Bahan - bahanChamomile (100%)Informasi alergenMungkin mengandung sisa kedelaiPersiapanSeduh tiap kantong teh di cangkir atau teko dengan air mendidih selama 4-5 menit.Hasil25 gelasKeunggulanDikemas dalam amplop higienis berkualitas tinggi untuk menjaga kesegaran rasa dan aroma. Rangkaian Sir Thomas Lipton akan memberikan sebuah pengalaman menikmati teh yang luar biasa.Masa simpan24 bulanPenyimpananSimpan di tempat yang sejuk dan kering1 pc isi 25 tea bags
    atribut:
    • Content: 25's
  8. Merck Millipore QCM Chemotaxis Cell Migration Assay
    Mulai

    Rp11.999.900

    Merck Millipore QCM Chemotaxis Cell Migration Assay
    Deskripsi:
    Also available: Cell Comb Scratch Assay! Get biochemical data from a scratch assay! Click HereIntroductionCell migration is a fundamental function of normal cellular processes, including embryonic development, angiogenesis, wound healing, immune response, and inflammation (Clark et al., 1996; Martin, 1997). In immune responses, monocyte migration is critical for providing immunological defense and eliminating infectious agents. Monocytes (macrophage precursors) circulate the blood until encountering specific chemotactic factors that initiate the migration process. Once engaged, monocytic cells transverse the vascular endothelium in a multistep mechanism by: A) E-selectin mediated monocyte rolling B) cell adhesion C) transmigration into the subendothelium (Ashida et al., 2001). During this migration and entering the tissue, monocytes develop/differentiate into mature macrophages, increasing in size, phagocytic activity, and proteolytic enzyme secretion. Once at the site of infection, mature macrophage respond to infection by phagocytosis, cytokine secretion, respiratory burst, T-cell antigen presentation, and digestive enzyme secretion (Holevinsky & Nelson, 1995). Microporous membrane inserts are widely used for cell migration and invasion assays. The most widely accepted of which is the Boyden Chamber assay. However, current methods of analysis are time-consuming and tedious, involving cotton swabbing of non-migrated cells on the topside of insert, manual staining and counting. Recently a fluorescence blocking membrane insert was introduced to address these issues; however, this approach requires labeling of the cells with Calcein-AM and extensive washing to remove free Calcein before cell migration. The effect of this treatment on cell behavior/migration remains questionable. The Chemicon QCM 96-well 5 μm Migration Assay does not require cell labeling, scraping, washing or counting. The 96-well insert and homogenous fluorescence detection format allows for large-scale screening and quantitative comparison of multiple samples (Gildea et al., 2000). In the Chemicon QCM 5 μm 96-well Migration Assay, migratory cells on the bottom of the insert membrane are dissociated from the membrane when incubated with Cell Detachment Buffer. These cells are subsequently lysed and detected by the patented CyQuant GR dye (Molecular Probes). This green-fluorescent dye exhibits strong fluorescence enhancement when bound to cellular nucleic acids (Jones et al., 2001). Most migration assays utilize an 8 μm pore size, as this is appropriate for most cell types, e.g. epithelial and fibroblast cells. The Chemicon QCM 5 μm 96-well Migration Assay utilizes a 5 μm pore size, which is appropriate for studying monocyte/macrophage migration. The system may be adapted to study different types of cell migration, including haptotaxis, random migration, chemokinesis, and chemotaxis. The Chemicon QCM 5 μm 96-well Migration Assay provides a quick and efficient system for quantitative determination of various factors on cell migration, including screening of pharmacological agents, evaluation of integrins or other adhesion receptors responsible for cell migration, or analysis of gene function in transfected cells. In addition, Chemicon continues to provide numerous migration, invasion, and adhesion products including: QCM 8μm 96-well Chemotaxis Cell Migration Assay (ECM510) QCM 3μm 96-well Chemotaxis Cell Migration Assay (ECM515) QCM 96-well Cell Invasion Assay (ECM555) 24-well Insert Cell Migration and Invasion Assay Systems CytoMatrix Cell Adhesion strips (ECM protein coated) QuantiMatrix ECM protein ELISA kits Application The Chemicon QCM 96-well 5μm Migration Assay is ideal for studying chemotaxis cell migration. The quantitative nature of this assay is especially useful for large scale screening of pharmacological agents. The 5 μm pore size of this assay's Boyden chambers is appropriate for studying monocyte/ macrophage migration. Each kit provides sufficient materials for the evaluation of 96 samples. The Chemicon QCM 5μm 96-well Migration Assay is intended for research use only; not for diagnostic applications.
    atribut:
    • Key Applications: Activity Assay
    • Material Size: 1 plate
    • Quality Level: MQ100
    • Species Reactivity: All
  9. Velp BOD Sensor
    Mulai

    Rp71.999.900

    Velp BOD Sensor
    Deskripsi:
    Safe and Easy to use- Measurement on scales of 90, 250, 600 and 999 ppm BOD- Higher values can be measured by diluting the sample- Fits directly on the bottle containing the sample- Automatically stores 5 BOD values at 24-hour intervals- Enables analysis to continue over the weekend- Results directly readable at any time, even after five days- Direct readout in mg/l (ppm)- Compact stirring stations- Models with stirring stations offer VELP stirring quality- IP 54 protection against particle and liquid ingress- Class 3 IEC 1010 conformity
    atribut:
    • Construction Material: Technopolymer
    • Power (W): 2
    • Total Capacity (ml): 500
    • Scales: 90, 250, 600, 999 ppm BOD. Higher values after dilution
    • BOD Values: directly on the display at any time also after the standard 5 days period
    • Frequency (Hz): 50/60
    • Power Supply (V): 115 or 2230
    • Protection : IP 54
    • Safety Class: 3 IEC 1010
  10. Merck Millipore QCM Chemotaxis Cell Migration Assay 96-well Fluorimetric (Kit Uji Migrasi Sel)
    Mulai

    Rp11.999.900

    Merck Millipore QCM Chemotaxis Cell Migration Assay 96-well Fluorimetric (Kit Uji Migrasi Sel)
    Deskripsi:
    Also available: Cell Comb Scratch Assay! Get biochemical data from a scratch assay! Click HereIntroductionCell migration is a fundamental function of normal cellular processes, including embryonic development, angiogenesis, wound healing, immune response, and inflammation (1-2). One such process, leukocyte extravasation, is crucial for appropriate and effective immune response (3). Neutrophils normally exist in a resting state as they circulate though the body. However, upon interaction with small molecules known as chemoattractants, they rapidly respond with endothelial adhesion followed by emigration from the vasculature and chemotaxis to the site of inflammation (4-5). These chemoattractant receptors activate heterotrimeric GTP-binding proteins (G proteins) that initiate numerous elaborate signal transduction cascades, culminating in neutrophil migration and activation. Once at the site of inflammation, neutrophils respond with phagocytosis, superoxide generation, and the release of degradative enzymes. Microporous membrane inserts are widely used for cell migration and invasion assays. The most widely accepted of which is the Boyden Chamber assay. However, current methods of analysis are time-consuming and tedious, involving cotton swabbing of non-migrated cells on the topside of insert, manual staining and counting. Recently a fluorescence blocking membrane insert was introduced to address these issues; however, this approach requires labeling of the cells with Calcein-AM and extensive washing to remove free Calcein before cell migration. The effect of this treatment on cell behavior/migration remains questionable. The Chemicon QCM 96-well 3 μM Migration Assay does not require cell labeling, scraping, washing or counting. The 96-well insert and homogenous fluorescence detection format allows for large-scale screening and quantitative comparison of multiple samples (6). In the Chemicon QCM 3 μM 96-well Migration Assay, migratory cells on the bottom of the insert membrane are dissociated from the membrane when incubated with Cell Detachment Buffer. These cells are subsequently lysed and detected by the patented CyQuant GR dye (Molecular Probes) (7). This green-fluorescent dye exhibits strong fluorescence enhancement when bound to cellular nucleic acids (8). Most migration assays utilize an 8 μm pore size, as this is appropriate for most cell types, e.g. epithelial and fibroblast cells. The Chemicon QCM 3 μM 96-well Migration Assay utilizes a 3 μm pore size, which is appropriate for leukocyte migration. The system may be adapted to study different types of cell migration, including haptotaxis, random migration, chemokinesis, and chemotaxis. The Chemicon QCM 3 μM 96-well Migration Assay provides a quick and efficient system for quantitative determination of various factors on cell migration, including screening of pharmacological agents, evaluation of integrins or other adhesion receptors responsible for cell migration, or analysis of gene function in transfected cells. In addition, Chemicon also provides QCM 8μM 96-well Chemotaxis Cell Migration (ECM510) and Invasion Assays (ECM555) (8 μm pore), 24-well insert Cell Migration and Invasion Assay Systems, CytoMatrix Cell Adhesion strips coated with ECM proteins, or anti-integrin antibodies, and QuantiMatrix ECM protein ELISA kits. Application: The Chemicon QCM 96-well 3μM Migration Assay is ideal for studying chemotaxis cell migration. The quantitative nature of this assay is especially useful for large scale screening of pharmacological agents. The 3 μm pore size of this assay's Boyden chambers is appropriate for studying leukocyte migration. Each kit provides sufficient materials for the evaluation of 96 samples. The Chemicon QCM 3μM 96-well Migration Assay is intended for research use only; not for diagnostic applications.
    atribut:
    • Detection Method: Fluorescent
    • Key Applications: Activity Assay
    • Material Package: 96 wells
    • Material Size: 1 plate
    • Quality Level: MQ100
    • Species Reactivity: All
  11. Frisian Flag Susu UHT Purefarm Fullcream
    Rating:
    100% of 100
    (1)
    Mulai

    Rp249.900

    Frisian Flag Susu UHT Purefarm Fullcream
    Deskripsi:
    Tiga Alasan Kenapa Kamu Harus Minum Susu Frisian Flag Full Cream:Rasakan kesegaran susu murni dengan rasa full cream yang gurih dan lezat.Mengandung nutrisi baik ya itu sumber 8 Vitamin (Vitamin A, D3, B1, B2, B3, B5, B6, dan B12), dan sumber 3 Mineral (Kalsium, Fosfor dan Iodium).Cocok diminum kapan saja terutama di pagi hari untuk membantu boosting semangat sebelum memulai aktifitas kamu
    atribut:
    • Variant: Fullcream
  12. Velp Flocculators
    Mulai

    Rp37.999.900

    Velp Flocculators
    Deskripsi:
    Precise and Easy to use- Speed can be changed during the run- Illuminated back panel to simplify sample observation- Stirring rods adjustable in height without tools- Reliable and repeatable results from VELP stirring quality- Precise speed from an electronically controlled DC gear motor- Strong resistance to chemical and mechanical corrosion- Independently selectable speeds 10-15-30-45-60-90-120-150-200-300 rpm- Same product can be submitted to different conditions in parallel- Choice of 4- or 6-place modelsWhat is JAR TEST?Jar testing is a pilot-scale test of the treatment chemicals used in a particular water plant.It simulates the coagulation/flocculation process in a water treatment plant, helping the operator in the determination of the right amount of treatment chemicals, and, thus, in improving the plant’s performance.Jar testing entails adjusting the amount of chemicals and their sequence in which they are added. The sample requires to be stirred so that the formation, development, and settlement of floc can be watched just as it would be in the fullscale treatment plant.The operator then performs a series of tests to compare the effects of different amounts of flocculation agents at different pH values to determine the right size floc.
    atribut:
    • Construction Material: Epoxy Painted Metal Structure
  13. Hanna Instruments Conductivity Standard (Larutan Kalibrasi Konduktivitas)
    Mulai

    Rp779.900

    Hanna Instruments Conductivity Standard (Larutan Kalibrasi Konduktivitas)
    Deskripsi:
    HI70039C is a premium quality 5,000 µS/cm conductivity solution that is NIST traceable and supplied with a Certificate of Analysis. Each sachet has the lot number and expiration date stamped on it and is made of light block foil ensuring freshness each time one is opened. Hanna’s line of conductivity solutions have been specially formulated to have an expiration of 5 years from the date of manufacture for an unopened sachet. The HI70039C is for 25 sachets containing 20 mL of solution.Supplied with Certificate of AnalysisTemperature chart of the actual µS/cm value at various temperatures printed on each bottleConvenient packaging for one time use
  14. Peak Instrument Spectrofotometer
    Mulai

    Rp14.999.900

    Peak Instrument Spectrofotometer
    Deskripsi:
    Steady, modern and elegant appearance design. Adopt the newest microcomputer technology and electronic control system. Optimized optical system and structure can both extend new functions and ensure the accuracy, stability and durability.Main Features1. 7 inch color LCD screen and long life, more comfortable and sensitive silicone buttons. The instrument can show various scanning curves and charts for users to complete various tests without computers.2. Support USB storage and different data formats such as Excel, txt and image(PC software). Users can output test data to flash memory, open and edit them on computers directly without any auxiliary software.3. Advanced hardware and 32-bit Cortex_M3 processor with the clock speed 120MHz. The equipment can store 5000 pieces of data and 500 curves.4. High-efficiency holographic grating of 1200 lines/mm and low stray light.5. The equipment has long-life socket type tungsten-halogen and deuterium lamps which can work up to 2000 hours, can switch the lamps according to test needs and record its working time automatically. Socket type lamps make the replacement much easier.6. Excellent silicon photodiode can guarantee the equipment is highly sensitive and stable.7. Huge sample chamber and various accessories can meet all kinds of needs.8. Can be connected to printer directly and output test charts and data.9. Powerful PC software.10. Standard RS232, USB(A), USB(B) port for printer, data transfer and PC connection.UI Design1. PhotometryThere are three test modes: Absorbance, transmittance and energy. 2. Quantitative test.To test sample solution concentration, you can choose different methods like coefficient, standard curve, linearity, linear zero crossing and quadratic. Up to 15 standard samples can be used to build a curve. Advance arithmetic make curvilinear regression more precise and test data more accurate.3. Kinetics Measurement (Time Scanning)To test the sample chemical reaction process by fixed time scanning the sample solution with fixed wavelength. The equipment can calculate its changing rate after entering the corresponding parameters.4. Wavelength Scanning (Qualitative Test)To test sample solution absorbance peak, can scan the sample characteristic curve of any wavelength range between 190 and 1100nm. You can look up the peak value on the device standalone. 5. Multi wavelength testingIt is much more convenient for users to test the absorbance of several wavelengths for the same sample solution, which is much simpler than single wavelength testing.6. DNA/Protein MeasurementIt is a special function for specific users to make the operation easier. There are two test modes.
Daftar Harga Timbangan Protein Terbaru November 2026
Termic Timbangan DigitalRp85.900
Master Flex Silicone Tube (Selang Silikon)Rp1.199.900
Ultra Milk Susu UHT Full CreamRp5.900
M.I.T Cleaning Agent CleanerRp2.099.900
TESTO Ph MeterRp12.999.900
Shimadzu Spectrophotometer Ultraviolet-Visible (Alat Uji Absorbansi Cahaya)Rp209.999.900
TESTO Ph/Temperature Measuring InstrumentRp4.799.900
Ultra Milk Susu UHT CoklatRp5.900
Lipton Teh Celup Sir ThomasRp69.900
Merck Millipore QCM Chemotaxis Cell Migration AssayRp11.999.900

Data diperbarui pada 13/11/2026 (Harga belum termasuk PPN)