Beli Alat Pengukur Kelembaban Tanah di monotaro.id
Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
- TESTO Moisture Meter (Alat Ukur Kelembaban)Deskripsi:The testo 616 professional moisture meter provides you with a precise and non-destructive means of measuring the moisture content of wood and building materials and of monitoring the drying process after water damage. Simply select the characteristic curve and place the meter’s measuring claw against the surface of the material you would like to measure. The meter shows you the moisture content as a weight percentage compared to the dry weight. Press the relevant key to save the reading to your meter.Although the measuring claw only comes into contact with the surface, wall or flooring that is being measured, it is able to determine the moisture content of the wood or other material down to a depth of 5 cm.Ideal areas of use for the testo 616 moisture meterThe testo 616 moisture meter is a professional measuring device that can be used in areas as diverse as water damage restoration or carpentry or joinery.Moisture damage detection: the non-destructive method for finding moisture in walls and floorsMonitoring drying processes: from carrying out moisture inspections to meeting building schedules to controlled drying after water damage - the non-destructive method for determining the moisture content in wood and building materialsMoisture in wood: for checking the moisture content of wood that has been stored prior to processingtesto 616 moisture meter with 10 characteristic curvesSoft woodHard woodPressboardAnhydrite screedCement screedLime sand brickGas concreteConcreteHigh insulation bricksBrickwork Product Includes: testo 616 moisture meter for wood and building materials, calibration protocol, batteries.Determining moisture in wood Moisture content is a decisive factor in the further processing and use of timber products. If wood is installed with the wrong moisture content this may result in mechanical deformations (contracting and swelling) at the site where the material is subsequently used, and therefore damage to pieces of furniture or entire supporting structures in buildings. Therefore, before being made into furniture or supporting material by a joiner/carpenter, the suitability of the wood has to be assessed by measuring the moisture content. The testo 616 enables the quick and non-destructive examination of the material moisture characteristics in timber. Characteristic curves are available for measuring wood moisture in soft and hard woods, and chipboard. These characteristic curves were developed in cooperation with the LPI institute.The measurement results are calculated up to a depth of 5 cm and can be recorded at the touch of a button. The readings are displayed in percent by weight in comparison to the dry mass of the material. Monitoring drying processes Whether freshly laid screed, or monitored drying of moisture damage, timely determination of the required moisture level will save time and therefore money. Screeds are laid in the in interior works stage, generally after plastering. The flooring and painting and decorating then follow. The drying behaviour is therefore a significant factor in the works schedule, primarily because the laying of flooring depends on this.The moisture measurement establishes readiness for flooring; liability for the flooring is thus transferred to the respective trade installing the flooring. An important part of this work is therefore documentation and assurance in the testing for readiness for flooring. What is the extent of moisture damage? This question has to be answered in order to decide which instruments are to be used to speed up the drying process.The testo 616 can be used to quickly and non-destructively examine the material moisture in building materials. It also makes work easier when drying processes for floors, walls and surfaces have to be observed. Diagnosing building moisture Moisture may penetrate walls, floors and ceilings due to pipes bursting or water ingress. Some of this moisture damage may not be detected immediately. Rising or ingressing water, faulty rain and waste water drains, or even blocked drains and inadequate seepage capacity may be the cause. Depending on where it is getting out or in, the moisture can spread in different ways; enormous damage may be done if discovered too late. Therefore, measurement of the material moisture in the affected places is necessary to be able to identify the source of the damage. The testo 616 can be used to quickly and non-destructively examine the material moisture in building materials. The measuring clamp is laid on the surface; the value can be read immediately. The measurement results are calculated up to a depth of 5 cm and can be recorded at the touch of a button. The readings are displayed in percent by weight in comparison to the dry mass of the material. For easy, quick handling, characteristics are already stored in testo 616 for the following construction materials: anhydrite screed, cement screed, lime sand brick, aerated concrete, concrete, vertically perforated brick and solid brick; these aid detection of wet places in the construction materials.
- SHINWA pH Meter (Pengukur pH Tanah)Deskripsi:Batteryless, easy to operate. Measurement is completed, if the tip is inserted into the soil only for one minute.atribut:
- Accuracy (pH): ±0.5
- Resolution (pH): 0.2
- Range (pH): 4 to 7
- WxDxH (mm): 47x47x160
- TESTO Material Moisture Meter (Alat Ukur Kelembaban)atribut:
- AS ONE Part Number: 1-6453-01
- TGK Part Number: 540-68-08-01
- Measurement Accuracy: (Material moisture) +/- 1% (with respect to measured electric conductivity)
- Battery: 2xAAA alkaline batteries
- Measurement Range: (Material moisture) 0-54.8 mass%
- Resolution: (Material moisture) 0.1%
- Accessories: Shipping inspection, strap, belt holder, protective cap, dry cell
- Battery Life (hour): 200 (when backlight is off)
- External Dimensions (mm): 119x46x25 (excluding protective cap device)
- TRUSCO Number: 333-7481
- Weight (g): 45 (excluding battery)
- KRISBOW Hot Wire Anemometer (Pengukur Kecepatan Angin)atribut:
- Air Temperature (°C): 0 to 50 Deg.C / 32 to 122 Deg. F (0.1 Deg. C / 0.1 Deg. F;1 Deg.C / 1. 8 Deg.F)
- Dimensions (mm): 198x78x51
- monotaro Digital Moisture Analyzer (Analisa Kelembaban Digital)Deskripsi:A compact, lightweight size, convenient style for carrying mobile phones. Data hold function with fixed measurement value. With maximum value/minimum value/average value display function.With auto power off function to prevent battery drain due to forgetting (cancellation possible).Convenient backlight function when working in the dark. To check moisture of timber, cement and other building materials.Dokumentasi Produk:WARRANTY MonotaRO Private Brandatribut:
- Measurement Pricision: ± 1%
- Operating Temperature and Humidity Range: 0 to + 50 ° C, 70% RH or less (with no condensation)
- Sampling: 1 time / s
- Storage Temperature/Humidity Range: -20 to + 60 ° C, 80% RH or less (with no condensation)
- Accessories: Instruction manual, strap, protective cover
- Measuring Range: 8.8 to 54.8% (beech, spruce, larch, birch, cherry, walnut),. 7.0 - 47.9% (oak, pine, maple, ash tree, rice bran, melan tea),. 0.9 to 22.1% (cement, concrete, plaster),. 0.0 to 11.0% (gypsum),. 0.7 to 8.6% (cement mortar),. 0.6 to 9.9% (lime mortar),. 0.1 to 16.5% (brick)
- Measurement Item: Moisture percentage
- Batteries: Two AAA (1.5 V) batteries
- Resolution Capability: 0.10%
- Weight (g): Approximately 119 (with protective cover installed, batteries included)
- Battery Life (continuous use): About 150 (when using alkaline dry batteries)
- Dimensions (mm): 50.9x132.9x24.7
- OneMed Digital Hygrometer (Pengukur Suhu Ruangan)Deskripsi:Thermometer Digital, Thermometer Hygrometer merk OneMed untuk mengukur suhu dan kelembapan udara secara digital. Basic Functions:- Temperature/Humidity- C/F temperature switch display- The maximum/minimum temperature and humidity memory function 12/24 hour clock- The Whole point timekeeping function- Daily alarm- Calendar Displayatribut:
- Marketing Authorization Number of KEMENKES RI: AKL 20901906493
- Temperature Measurement Accuracy (°C): ± 1 (1.8F)
- KRISBOW Environment Meter 5in1 Pro (Alat Ukur Multifungsi)atribut:
- Power: 1x9V NEDA 1604 battery
- Resolution: 0.1
- Dimensions (mm): 248x65x45
- HTC-1 Digital Hygrometer (Pengukur Suhu Ruangan)Deskripsi:- Large character LCD display, easy to read- Temperature, Humidity and Clock display simultaneously- Hourly chime, Daily alarm function- Max/Min temperature and humidity memory function- Calendar display function (Month and date)- Temperature display modesatribut:
- Humidity Range (% RH): 10 to 99
- Temperature Range (°C): -50 to +70
- Dimensions (mm): 93x21x101
- Material: ABS
- Power Supply: AAA 1.5V Battery - 1pc
- TRUSCO Digital Thermometer & Hygrometer (Pengukur Suhu Ruangan)atribut:
- Measured Humidity Range (% RH): 30 to 95
- Dimensions (Width x Depth x Height) (mm): 102x18x103
- Material: ABS Resin
- Humidity Minimum Indication: 1% RH
- Measurement Item: Temperature, Humidity
- Measurement Temperature Range (°C): -5 to 49
- Minimum Temperature Display (°C): 0.1
- Power Supply: AAA battery x 1 (attached for testing)
- Extech Moisture MeterDeskripsi:MO260 is a Combination Pin/Pinless Moisture Meter which measures Relative Moisture in wood and other building materials using pinless technology plus % of Moisture in sheetrock and other materials using the direct pin method. Measurements are displayed on a digital LCD with backlighting and a tri-color LED bargraph. Pinless non-invasive measurement depth to 0.75 Inch (22mm) below the surface. Complete with 9V battery, replacement pins, protective cap, and pouch case.
- Lutron pH Meter (Pengukur pH)Deskripsi:- Economical type.- pocket size.
- Extech pH MeterDeskripsi:- Flat Surface Electrode measures pH in liquids, semi-solids,and solids. No more electrode breakage or clogged junctions.- RENEWindicator tells you when it's time to replace your electrode which eliminates guesswork CAL alert tells you its time to recalibrate.- Ensures accuracy.- Memory records and recalls 15 sequentially tagged readings allowing detection of changes over time- Analog bargraph displayed on LCD 1, 2 or 3 point calibration automatically recognizes buffer solutions.- Order pH buffers separately.- Automatic Temperature Compensation Simultaneous display of pH and Temperature Display indicates when the reading is stabilized.- Data Hold, Auto power off and low battery indication - Waterproofdesign (IP57) floats in water and protects the meter in wet environment- Interchangeable probes available for Chlorine & ORP- Optional weighted base (EX006) holds plastic cup and ExStik meter - Complete with flat surface pH electrode, protective sensorcap, sample cup with cap, four 3V CR-2032 button batteries, and 48INC(1.2m) neckstrap.- Order pH buffers separatelyatribut:
- Resolution (pH): 0.01
- Range (pH): 0 to 14
- Accuracy (pH): ± 0.01
- Dimension Unit (cm): 3.56x17.2x4.1
- Item: PH Meter
- Manufacturing Number: PH100
- Netto Weight (kg): 0.1
- Power Source: Baterai CR2032 (optional/exclude)
- Temperature (°C): -5 to 90
- Type: PH Meter
- KRISBOW pH & Temperature Tester (Pengukur pH dan Suhu)atribut:
- Temperature Range (°C): -5 to 50
- Temperature Accuracy (°C): ± 0.8
- Index Protection: IP65
- Temperature Resolution: 0.1
- pH Accuracy: ± 0.03
- pH Range: 0 to 14
- pH Resolution: 0.01
- Shinwa Rules Digital pH Meteratribut:
- Operating Temperature Range: 5-35°C
- Measuring Range: 1.0 to 14.0pH
- Minimum: (Resolution) pH0.1
- Precision: ± pH0.1
- Body Material: ABS resin
- Material (measuring section): Glass
- Power: Three silver oxide batteries LR44
- Shinwa Rules Soil Acidity Meter Aatribut:
- 1 Scale: pH 0.2
- Measuring Range: 3 to 7pH
- Main Part Dimension: 106x47x47mm
- Precision: ± 0.5pH
- Body Material: ABS resin
- TRUSCO Number: 405-5870
- KDS Measuring Tape Long Tufmic-12R (Meteran)Deskripsi:Rulenya berbahan fiber, tidak mudah merenggang maupun menyusut, anti terhadap air, kelembaban, suhu dan zat kimia lainnya, mudah dibersihkan dari kotoran dan lumpur. Sangat disarankan untuk pengukur tanah dan mereka yang membutuhkan peralatan dengan kualitas tinggi.Tegangan standar :20degree C 20N (2kgf).atribut:
- Specification: 50mX12mm
- Non Brand Polyurethane InjectionDeskripsi:KOMOBLOCK UWBM-310 merupakan material water-blocking poliurethane 1 komponen bertipe Hydrophilic (anti air), dan jika terjadi kebocoran akibat kerusakan pada struktur beton, maka akan terbentuk sebuah foam (busa) yang memiliki elastisitas, daya rekat, dan fleksibilitas tinggi seperti karet karena bereaksi kimia dengan air yang bertemu di dalam retak atau celah jika material injeksi dimasukkan. Oleh karena itu, material ini adalah produk unggulan yang mengatasi kebocoran dan dapat menanggapi secara cukup pergerakan akibat getaran atau pemuaian/penyusutan sebuah struktur bangunan. - Tujuan Penggunaan: 1) Bagian retak atau sambungan (joint) sebuah struktur bangunan beton. 2) Bagian dengan retakan fluktual akibat mendapatkan beban bangunan berlebih. - Lingkup Pengaplikasian: 1) Bagian bocor pada joint sambungan beton, bagian retak bocor yang memiliki getaran dan fluktuasi, serta bagian retak bocor dari struktur baru. 2) Bagian bocor yang memiliki banyak bagian lembab di struktur betonnya.
- TESTO Infrared ThermometerDeskripsi:-With laser point function.-Consumer products safety act PSC marked item.-Equipped with auto power off and automatic hold functions.-With backlight.
- PUREAIR Oxygen TankDeskripsi:- Kapasitas oksigen silinder 1m3 - Sudah termasuk isi oksigen - Regulator oksigen dengan manometer dan alat pelembab udara - Dilengkapi dengan nasal canula - Troli oksigen terbuat dari pipa baja - Dilengkapi dengan kastor (jaring pada tabung oksigen)atribut:
- Diameter (mm): 140
- Height (cm): 65
- Capacity (m³): 1
- Makita Angle Grinder (Mesin Gerinda Tangan)Deskripsi:Produk Gerinda Tangan dari Makita ini memiliki kecepatan mesin mulai dari 6,600 - 11,000 RPM, cocok untuk industri manufaktur, bengkel konstruksi, dan juga pemakaian sehari-hari
Daftar Harga Alat Pengukur Kelembaban Tanah Terbaru November 2026
| TESTO Moisture Meter (Alat Ukur Kelembaban) | Rp3.399.900 |
| SHINWA pH Meter (Pengukur pH Tanah) | Rp999.900 |
| TESTO Material Moisture Meter (Alat Ukur Kelembaban) | Rp6.299.900 |
| KRISBOW Hot Wire Anemometer (Pengukur Kecepatan Angin) | Rp3.699.900 |
| monotaro Digital Moisture Analyzer (Analisa Kelembaban Digital) | Rp2.599.900 |
| OneMed Digital Hygrometer (Pengukur Suhu Ruangan) | Rp129.900 |
| KRISBOW Environment Meter 5in1 Pro (Alat Ukur Multifungsi) | Rp3.599.900 |
| HTC-1 Digital Hygrometer (Pengukur Suhu Ruangan) | Rp149.900 |
| TRUSCO Digital Thermometer & Hygrometer (Pengukur Suhu Ruangan) | Rp489.900 |
| Extech Moisture Meter | Rp1.699.900 |
Data diperbarui pada 13/11/2026 (Harga belum termasuk PPN)



















































































































































/6oP105736240-1.jpg)
/quP105263966-1.jpg)
/hqP103658638-1.jpg)
/h3P101516615-2.jpg)
/45P102229149-3.jpg)
/djP105708487-2.jpg)
/8tP103209317-2.jpg)
/pvP103205931-1.jpg)
/7jP101503271-3.jpg)

/lbP105145767-3.jpg)

/1rP101517063-3.jpg)


/P102084908-1.jpg)
%20%26%20Pengelasan/Lem%2C%20Bahan%20Perbaikan/Lem%20Industri/Non%20Brand%20Polyurethane%20Injection/ebP105469515-1.jpg)

%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Kesehatan/Pertolongan%20Pertama%2C%20Kebutuhan%20Higienis/P3K/PUREAIR%20Oxygen%20Tank/0sP103794028-2.jpg)
/P101578446-1.jpg)
%20Alkaline%20Battery%20AA%20(Baterai%20AA)/ABC%20(Battery)%20Alkaline%20Battery%20AA%20(Baterai%20AA)%20LR6%20Millenium%20Power%204B%2B2B%201pack(4%2B2pcs)/iqS000001674-4.jpg)
/WD-40%20Multi-Use%20Product%20(Pelumas%20Serbaguna)%20333ml%201pc/60S000055216-2.jpg)
/Mama%20Lemon%20Sabun%20Cuci%20Piring%20Cair%20Pouch%20(Dishwashing%20Liquid)%20Extra%20Pouch%20680ml%201pc/j1S000001685-5.jpg)
/PaperOne%20Copy%20Paper%20A4%2075gsm%20(Kertas%20HVS%20%2F%20Fotocopy)%201box(5reams)/9uS010737354-7.jpg)
/Sinarline%20Copy%20Paper%20A4%2070gsm%20(Kertas%20HVS%20%2F%20Fotocopy)%20White%201box(5reams)/meS056175806-2.jpg)
/monotaro_id%20Kantong%20Plastik%20Sampah%20Hitam%20HDPE%2070micron%20(Trash%20Bag%20%2F%20Kresek)%201kg%2090x120cm%201pack(%C2%B17pcs)/bnS034771419-7.jpg)
/monotaro_id%20Kain%20Lap%20Mikrofiber%2040x40cm%20320gsm%20(Cleaning%20Cloth)%20Biru%20Muda%201pc/ntS034715857-3.jpg)

/Sunlight%20Sabun%20Cuci%20Piring%20Pouch%20(Dishwashing%20Liquid)%20Lime%20370ml%201pc/j8S032839692-2.jpg)
%20Alkaline%20Battery%20AAA%20(Baterai%20AAA)/ABC%20(Battery)%20Alkaline%20Battery%20AAA%20(Baterai%20AAA)%20LR03%20Milenium%20Power%204B%2B2B%201pack(4%2B2pcs)/4kS028113164-2.jpg)

/Max%20Stapler%20Needle%20(Isi%20Staples)%20No_10-1M%205%2F16x3%2F16Inch%201pack(20pcs)/S000005230-4.jpg)
/Kenko%20Cutter%20Refill%20Blade%20(Isi%20Mata%20Pisau)%20L-150%20100x18mm%201pack(5pcs)/2gS000021088-3.jpg)
/monotaro_id%201%20inch%20Clear%20Tape%20(Solasi%20%2F%20Selotip)%2064m%20Transparent%2024mmx72yard%201roll/96S042206330-1.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Sarung%20Tangan/Sarung%20Tangan%20Sekali%20Pakai/Sarung%20Tangan%20PVC%20Sekali%20Pakai/Bagus%20Plastic%20Gloves%20(Sarung%20Tangan)/Bagus%20Plastic%20Gloves%20(Sarung%20Tangan)%20W-22599%2010%C2%B5%201pack(50pcs)/jsS039716712-1.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Masker/Masker%20Sekali%20Pakai/Masker%20Daily/Suojella%203ply%20Earloop%20Rubber%20Mask/Suojella%203ply%20Earloop%20Rubber%20Mask%20White%201box(50pcs)/9pS031693349-2.jpg)
/Sinarline%20Copy%20Paper%20A4%2070gsm%20(Kertas%20HVS%20%2F%20Fotocopy)%20White%201ream/lyS056175790-3.jpg)
/Sinarline%20Copy%20Paper%20A4%2075gsm%20(Kertas%20HVS%20%2F%20Fotocopy)%20White%201ream/msS056175820-3.jpg)
/monotaro_id%20Lakban%20OPP%202inch%20(Solasi%20%2F%20Selotip)%20Transparent%2048mmx64m%201roll/h7S036166619-4.jpg)
/monotaro_id%20Plas%20Chamois%20(Lap%20Kanebo)%20with%20tube%20Yellow%2032x21cm%201pc/4uS037754174-2.jpg)
/monotaro_id%20Kain%20Lap%20Mikrofiber%2035x35cm%20300gsm%20(Cleaning%20Cloth)%20Biru%20Tua%201pc/65S039548221-2.jpg)
/Paperline%20Envelope%20(Amplop)%20PPL%20EV%2090%20PPS%20Buklet%20Putih%20110x230mm%201box(100pcs)/66S000008222-6.jpg)
/3M%20Red%20Buffer%20Pad%205100%20(Pad%20Buffer%20Lantai)%2016inch%201pc/3cS033966120-1.jpg)
/Standard%20Pen%20AE-7%20(Pulpen%20%2F%20Bolpoin)%20ATK02092%20Alfa%20Tip%20Black%200_5mm%201pc/dzS034610503-1.jpg)