Beli vacuum cleaner with hepa filter di monotaro.id
Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
- NILFISK Vacuum Dry Backpack with Hepa EuDeskripsi:There are many things that should be present in a good backpack vacuum cleaner. It should be light in weight, with even weight distribution, and the noise level must be as low as possible. At the same time, the power needs to be sufficient for fast, effective cleaning, and the dust bag must be large enough to avoid constant changing. Without these basics, a backpack vacuum cleaner is uncomfortable and impractical to operate. The GD5 backpack vacuum cleaner meets these criteria and more. There are many things that should be present in a good backpack vacuum cleaner. It should be light in weight, with even weight distribution, and the noise level must be as low as possible.The Nilfisk GD 5 backpack vacuums surpass all criteria, making fast productive cleaning at a price that won’t bust your budget.atribut:
- Rated Power (W): 1300
- Dimensions (mm): 380x260x570
- Cable Lengt (m): 15
- Vacuum at Nozzle (kPa): 24
- Air Flow (L/s): 41
- Dust Bag Capacity (L): 5
- Frequency (Hz): 50-60
- Main Filter Area (cm²): 1400
- Sound Pressure Level (dBA): 59
- Suction Motor Power (W): 255
- Suction Power End of Tube (W): 240
- Voltage (V): 240
- NILFISK Vacuum DryDeskripsi:Lightweight and portable, the Nilfisk GM 80P is the symbol of Nilfisk quality and provides durability, high performance and efficient cleaning - required by dust control professionals. The sturdy aluminium container means that the vacuum cleaner is almost indestructable and therefore especially suitable for rough and heavy duty cleaning. Mounted on a strong steel trolley with large rubber wheels, the machine is easy to manoeuvre. Ideal for e.g. production lines, chemi/pharma industries, hospitals and offices. GM 80P is a versatile machine with high suction power and can be used for both industry cleaning and integrated into production facilities. The unique multi-stage filtration system allows for adaption to special applications where high filtration level and low emission is required. Choose between two types of dust bags (fleece or paper), four different washable sack filters (Polyester, Cotton, PTFE or Nomex) and special exhaust filters with HEPA or ULPA classication. GM 80P can handle every heavy duty cleaning task and has become a vacuum cleaner icon in variety of industries
- NILFISK High Pressure Cold Home UseDeskripsi:Penyemprot air bertekanan tinggi air Nilfisk E130.3-8 hadir dengan pompa aluminium yang awet & dapat digunakan berulang kali serta hadir dengan fitur Click&Clean; yang memudahkan Anda. Kompresor ini hadir dengan tombol on/off yang mudah dinyalakan serta tempat penyimpanan untuk selang dan kabel. Dilengkapi fitur Noise reduction dengan suspensi karet dari motor pump unit.
- NILFISK Vacuum Wet and DryDeskripsi:The VHO 200 is a powerful vacuum for liquids with a diverting valve for convenient and fast container emptying. A metal basket for the metal chips recovery is also available as well as different kinds of nylon filters, letting the user select the required level of filtration for the application and then re-use the collected materials (both liquids and solids). The container emptying is performed manually by a ball valve or by differential pressure with discharge accessories kit. The VHO200 cleverly uses its twin vacuum motors to both collect and then to discharge the collected liquid without the need for an integral electric discharge pump. 2,4 kW power rating using two single-phase by-pass motors placed within a protective polypropylene cover connected to the container by a self-centering metal band. Once the metal band is released the motor-head is free to be tilted open. To protect the motors the VHO200 safety measures are comprehensive: both a visual cut off system and a float shut-off system are fitted as well as a double filter pad and an absorbent pad. A metal basket for metal chips recovery with integrated float shut-off is also available as well as different kinds of nylon filters, letting the user choose appropriate levels of filtration for the task and then to re-use the collected material (both liquids and solids). Oil mist can be filtered as well by a dedicated filter positioned under the motorhead. The drain point on the bottom of the container allows complete draining of the liquid collected. The container is easily removable for cleaning. With all these features this machine is suitable for many different sectors: ideal for the oil recovery and recycling from tooling machines, in its stainless steel version (with the exception of the motor-head and the trolley) it’s also suitable for chemical & pharmaceutical use as well as in food companies whenever there is the need to collect liquid. Dedicated accessory kits for different sectors are also available.
- KARCHER HOME & GARDEN Multi Purpose Vacuum CleanersDeskripsi:KARCHER Multi Purpose Vacuum Cleaners is A vacuum cleaner for diverse usage. A match for any type of dirt: the Kärcher multi-purpose vacuum cleaners are ideal for car interior cleaning, workshops, garages, cellars, outside areas and renovation.
- Innotechs Backpack Dry Vacuum Cleaneratribut:
- Power (W): 1000
- Voltage (V): 220-240
- Air Flow Rate (L/s): 48
- Vacuum Suction (Mbar): 190
- Cable Length (m): 18
- Hose Diameter (mm): Ø 36
- Functions: Dry
- Tank Capacity (L) : 3
- NILFISK Vacuum Cleaner DryDeskripsi:A famous and well-known workhorse-efficient and durable for large area cleaning.atribut:
- IP Protection Class: 55
- ABN Pipette TipsDeskripsi:- Pipet Tips untuk pipet berukuran 100-1000 ul (microliter) berwarna kuning- Harga diatas untuk 1 pack : 1000 pipet tips- Cocok untuk pipet merk Socorex volume 100-1000 ul (microliter) dan cocok dengan sebagian besar merek pipet- Autoclavable- Pipette Tips ABN tahan terhadap bahan kimia dan tahan panasatribut:
- Color: Blue
- KARCHER Professional Dry Vacuum CleanersDeskripsi:Standard equiped with a high effective fleece filter bag which allows an up to three times higher filter bag volume in contrast to a paper filter bag. This is a benefit that pays for itself since the operating periods between filter bag changes are longer. The T 12/1 eco!efficiency motor performance, air flow and the 6-stage filter system (incl. microfilter as special option) have been designed in such a way that there is hardly any loss of suction power. Its low centre of gravity provides stability. The power cable can be wind up in between the cable storage or onto a pull-out cable hook as a fast storage when often changing the location, e.g. cleaning objects in hotels, ect. Special feature: the floor tool plugs into the accessory holder (on the back of the unit) and can be used as a complete accessory fixation at the machine after work. The suction hose on the unit has a simple but effective plug-in clip system. You push the hose on to the unit's intake stub, a resilient ring engages – that's all. This system ensures that the suction hose does not become detached when the unit is pulled along behind the user. The new clip system (change without tools) on the bend allows an easy extension of the suction hose of additional 2,5 m (extra extension suction hose - part number 6.906-237.0) for e.g. cleaning steps, stairways, etc. With the power brush ESB 28 (additional accessory) the T 12/1 eco!efficiency converts into a brush-type vacuum cleaner. In cases where the hygienic standards are particularly stringent, a HEPA filter which retains very fine particles (99.95% retention rate) can be fitted (instead the standard air exhaust filter) in addition to the paper filter bag. Equipment - Suction hose, 2.5 m - Suction Tube, 2 piece(s), 0.5 m - Filter bag, fleece - Container material, plastic - Clip system for hose extension - Safety class, II - Permanent filter basket, fleece
- NILFISK High Pressure CleanerDeskripsi:Hadirkan pembersih bertekanan berkualitas dari Nilfisk untuk membantu kebutuhan Anda saat membersihkan dinding, lantai, atau barang-barang yang sangat kotor. Dengan performa tinggi, alat ini dapat menghasilkan tekanan sebesar 140 bar, sangat mudah dioperasikan, dan hadir dengan panjang selang 9 meter untuk daya jangkau yang lebih baik. Cocok untuk frekuensi pemakaian sedang hingga tinggi untuk kebutuhan rumah tangga Anda. Saat tidak digunakan, selang dapat disimpan dengan rapi pada gulungan selang yang terletak pada alat. Noozle juga dapat disimpan di dalam mesin ketika tidak digunakan untuk menjaga semua aksesorisnya tetap tersimpan dengan rapi.
- BLANCETT Turbine Flowmeter & TotalizerDeskripsi:Inline turbine flowmeters for oils and water measure the flow rate of water and water-based liquids traveling through a system. Inline meters and sensors are installed level with the system's piping, where media travels directly through the instrument. They're used in applications with limited space, minimize the impact on system line pressure, and require minimal plumbing alterations.
- Vertex 3-Way Angle Milling ViseDeskripsi:Angles can be set in 3 dimensions. Swivels 360 Degree around base. The vise can be elevated through 90atribut:
- Angle (°): 0-90
- NAKANISHI Ultra-Precision Brushless Micro Grinder Espert500Deskripsi:- Collet chuck: 6mmatribut:
- Dimensions (mm): 22.4x75
- No-load Speed (minute): 40000 or less
- TENAX Silt FenceDeskripsi:These silt fences are supported by wooden stakes and designed to control erosion along the perimeter of a project. They feature a lightweight, woven, polypropylene fabric that lets fluids pass through while trapping soil and preventing soil loss. Fences help to prevent silt and sediment run-off from land development sites along streams, slopes, drainage and waterways, embankments, ditches, medians, and more.atribut:
- UNSPSC: 30152002
- Color: Black
- Length (ft): 100
- Material: Polypropylene
- Number of Stakes: 11
- NILFISK Vacuum BackpackDeskripsi:There are many things that should be present in a good backpack vacuum cleaner. It should be light in weight, with even weight distribution, and the noise level must be as low as possible. At the same time, the power needs to be sufficient for fast, effective cleaning, and the dust bag must be large enough to avoid constant changing. Without these basics, a backpack vacuum cleaner is uncomfortable and impractical to operate. The GD5 backpack vacuum cleaner meets these criteria and more. There are many things that should be present in a good backpack vacuum cleaner. It should be light in weight, with even weight distribution, and the noise level must be as low as possible.The Nilfisk GD 5 backpack vacuums surpass all criteria, making fast productive cleaning at a price that won’t bust your budget.atribut:
- Rated Power (W): 650
- Dust Bag Capacity (L): 5
- Battery Capacity (Ah/5): 7.8/280.8
- Battery Running Time (minute): 60/30
- Dimensions (mm): 240x330x755
- Grounded: Class II
- IP Protection Class: IP20
- Main Filter Area (m²): 35
- Minimum Battery Charging Time (minute): ≤ 40
- Number of Battery: 1
- Number of Filter: 2
- Plug Type: EU
- Sack Filter Area (cm²): 1397
- Sound Pressure Level (dBA): 60/65 (at 1.5m, with nozzle ISO 11203)
- Voltage (V): 36
- MILWAUKEE Fuel Backpack Vacuum Cleaneratribut:
- Air Volume (L/minute): 1557
- Capacity Liquids (L): 3.8
- Hose Length (cm): 270
- Battery Platform: M18™ REDLITHIUM™-ION
- Voltage (V): 18
- LED Light: No
- Fuel Gauge: Yes
- Maximum Vacuum (mbar): 189
- NILFISK Vacuum Cleaner Wet and DryDeskripsi:The Nilfisk wet and dry range of vacuum cleaners includes durable machines from 20 to 75 liters that can take on any application, big or small. With outstanding performance and features like easy emptying and corrosion resistance, our range of wet and dry
Daftar Harga vacuum cleaner with hepa filter Terbaru March 2026
| NILFISK Vacuum Dry Backpack with Hepa Eu | Rp10.999.900 |
| NILFISK Vacuum Dry | Rp10.999.900 |
| NILFISK High Pressure Cold Home Use | Rp2.999.900 |
| NILFISK Vacuum Wet and Dry | Rp2.499.900 |
| NILFISK Vacuum Cleaner Wet & Dry Type for Industrial Use | Rp4.499.900 |
| KARCHER HOME & GARDEN Multi Purpose Vacuum Cleaners | Rp1.699.900 |
| NILFISK Dry Vacuum Cleaner | Rp8.499.900 |
| Innotechs Backpack Dry Vacuum Cleaner | Rp2.299.900 |
| Kartell Pipette Tips | Rp62.900 |
| NILFISK Vacuum Cleaner Dry | Rp99.999.900 |
Data diperbarui pada 10/03/2026 (Harga belum termasuk PPN)