Beli data logger di monotaro.id

Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
  1. Elitech Temperature Data Logger
    Mulai

    Rp429.900

    Elitech Temperature Data Logger
    Deskripsi:
    Elitech RC-5 USB Temperature Data Logger terutama digunakan untuk pencatatan suhu selama penyimpanan dan transportasi laut / udara / jalan raya bahan makanan, obat-obatan, bahan kimia dan produk lainnya, terutama banyak digunakan di semua jenis pergudangan, logistik dan rantai dingin, seperti wadah berpendingin, berpendingin truk paket berpendingin, penyimpanan dingin, laboratorium, dll. atau dalam bisnis rantai pasokan global berskala besar.Pencatat Data Suhu mini ini memiliki rentang pengukuran yang luas -30 ° C ~ + 70 ° C, akurasi tinggi, interval pencatatan yang dapat disesuaikan & masa pakai baterai yang lama untuk perekaman, pemantauan, dan analisis data suhu yang nyaman dan andal.Memiliki memori data permanen besar 32000 poin dan dilengkapi dengan perangkat lunak manajemen data untuk mengunduh data dengan mudah ke komputer melalui antarmuka USB. Dengan software ini, Anda dapat menganalisis data dalam bentuk tabel dan grafik dan mengekspornya dalam format gambar. Data dapat dipertanyakan, disimpan, dicetak dan diekspor dalam format Word / Excel / TXT / PDF.
    atribut:
    • Temperature Resolution (°C/°F): 0.1
  2. Hioki Temperature Logger
    Mulai

    Rp3.099.900

    Hioki Temperature Logger
    Deskripsi:
    A compact logger that can record temperature depending on the measurement target using an external sensor (sensor sold separately).It is small, lightweight, and pocket-sized so you don't have to worry about installation space.Two-item display that is easy to understand at a glance.Equipped with large capacity internal memory (60,000 data per channel).Data can be transferred to a PC without stopping recording.You can replace the battery while recording (recording continues for about 30 seconds even if the battery is removed).Since the previous recorded data is backed up, there is no need to worry even in the unlikely event of an incorrect operation.Purpose:For temperature measurement.For temperature control during transportation of pharmaceuticals, specimens, and chemicals.For temperature measurement and management in cold storage, storage, and showcases.For temperature control in inspection rooms, analysis/test rooms, factories, and kitchens.For temperature control of food, vegetables, fruits, and sweets.For fermentation and aging temperature control of foods such as alcohol, soy sauce, miso, and bread.
  3. TESTO Data Logger
    Mulai

    Rp4.899.900

    TESTO Data Logger
    Deskripsi:
    -Software is not required to produce PDF report automatically.-Ultra low temperature type.-Direct USB connection.-NFC wireless communication possible. -Temperature for pharmaceutical drugs/food/precision devices and while transporting work of art.
    atribut:
    • Temperature Min Display: 0.1degree C
    • W x D x H: 44x12x97mm
  4. TESTO Mini Data Logger
    Mulai

    Rp4.799.900

    TESTO Mini Data Logger
    Deskripsi:
    Does your work involve the warehousing or storage of climate-sensitive items (food, drugs, archive media, museum exhibits, metal parts susceptible to rust film, etc.)? Or would you like to keep a check on the building climate, for example monitoring how your tenants use ventilation? Then continuous recording of temperature and humidity readings can be very useful for you. The testo 174H mini data logger for temperature and humidity provides you with competent support for this kind of measurement task. It may be small, but it achieves great (measurement) results.This is what the mini data logger for temperature and humidity offersThe current measuring values and any possible violations of limit values can be read on the mini data logger’s display. Its measurement data memory can reliably record up to 16¿000 measuring values. Saved measurement data will not be lost even when the battery is empty or being replaced.The testo 174H mini data logger has internal sensors which measure temperature and humidity. The humidity sensor is a capacitive Testo humidity sensor with long-term stability which has an accuracy of up to ±3 % RH when measuring humidity. With an accuracy of ±0.5 °C, the internal NTC temperature sensor is particularly high-precision and covers a measuring range from -20 to +70 °C.Particularly practical: the mini data logger runs on standard batteries (2x CR 2032) which you can replace yourself at any time.Programming and analysis with the data logger for temperature and humiditySoftware is used to programme and read your mini data logger as well as to analyze measurement data on the PC. You have a choice of three software versions: ComSoft Basic software - available as a free download - for fast programming of the mini data logger and easy analysis of measurement data ComSoft Professional software - can also be ordered as an option - offers a variety of possibilities for detailed analysis of temperature and humidity readings ComSoft CFR 21 Part 11 software - can also be ordered as an option - the best solution for special requirements according to CFR 21 Part 11 in the pharmaceutical sectorAdvantage of the set: the mini data logger is ready to use straight awayA USB interface is needed to programme and read your mini data logger for temperature and humidity. If you decide on this set, it includes a USB interface which means a speedy start for your measuring tasks.Attention: Please download the newest software version before using the USB interface for the first time. The software can be found in the download area. Product Includes: testo 174H mini data logger set for temperature and humidity, including USB interface for programming and reading the mini data logger, wall bracket, batteries (2 x CR 2032 lithium) and calibration protocol.Monitoring and documentation of building climate Temperature and relative humidity are crucial factors when it comes to assessing air quality and comfort levels in indoor areas, e.g. in workplaces. Both values can be monitored and documented over the long term using data loggers.They are also very well suited for checking ventilation systems or for assessing any building moisture which occurs.The use of special software means measurement configurations can be carried out individually and recorded measurement data can be both analysed and archived. Monitoring and documentation of storage temperature and humidity Correct compliance with storage temperature and humidity is an important prerequisite for the quality assurance of many products, e.g. in the area of food and pharmaceutical products.As a general rule, data loggers are used to do this. They automatically check and document the profile of the ambient conditions and thus make a crucial contribution to verifiable preservation of product quality.Viewing breaches of limit values directly on the display means you can respond quickly to temperature and humidity deviations. In addition, with the help of the configuration and read-out software, customer-specific measurement configurations can be carried out and recorded measurement data can be both analysed and archived. Monitoring and documentation of transport temperature and humidity For all goods which react sensitively to temperature and humidity fluctuations or have to be stored within a predefined range, uninterrupted measurement data recording and documentation play a major role.Incorrect conditions during transport can lead to major losses of quality, including the total loss of value of the products that require monitoring.Using a data logger, shipments can be checked for compliance with the specified temperature and humidity ranges and the data can then be read, analysed and archived by means of special software.
    atribut:
    • Measuring Rate: 1 min - 24 h
    • Memory: 16,000 Measuring values
    • Battery Type: 2x3V button cell (CR 2032)
    • Dimensions (mm): 60x38x18.5
    • Product/Housing Material: Plastic
    • Storage Temperature: -40 to +70 °C
  5. AND Temperature Data Logger
    Mulai

    Rp1.199.900

    AND Temperature Data Logger
    Deskripsi:
    Include Monitor battery, instruction manual, dedicated USB communication cable AX-KO4141
  6. AS ONE Data Logger
    Mulai

    Rp33.999.900

    AS ONE Data Logger
    atribut:
    • Supported OS: Windows(R)Vista(TM)/7/8/8.1
    • Size (mm): Approx 188x117x42
    • Display Contents: Analog waveform,history data display during the measurement, digital value
    • Humidity: 0-100%
    • Measurement Range Voltage (mV): 20, 50, 100, 200, 500
    • Temperature/Thermocouple: K, J
    • Analog Input Terminal: Screw type terminal
    • Incorporated Memory (GB): 4
    • Package Size (mm): 300x200x150
    • Power Supply: AC adapter AC100 - 240V, 50/60Hz or DC input (DC8.5 24V)
    • Sampling Cycle (ms-hour): 10ms - 1h (10 - 50ms is only for voltage, ch restriction applies depending on the sampling period)
  7. TESTO Nonelectrical Properties Data Logger
    Mulai

    Rp3.099.900

    TESTO Nonelectrical Properties Data Logger
    atribut:
    • UNSPSC: 20122903
    • AC Adapter: No
    • Alarm: Yes
    • Brand: TESTO
    • Compatible With: 0572 0500 - USB Interface
    • Depth (inch): 3.25
    • Digital Readout: Yes
    • Frequency of Transmissions (minute-hour): 1 to 24
    • Height (inch): 1.25
    • Includes: Batteries; Data Logger,Locking Wall Holder
    • Interface: 0572 0500 - USB Interface Cradle
    • Product Type: Mini Data Logger
    • Sample Point Storage (minute): 15 Measuring Cycle
    • Sample Point Storage (°F): 77
    • Software Required: Yes
    • Temperature Range (°F): -22 to 158
    • Time Intervals: Variable
    • Type: NTC
    • Waterproof: IP65
  8. ROTRONIC Humidity Datalogger
    Mulai

    Rp2.599.900

    ROTRONIC Humidity Datalogger
    Deskripsi:
    The Rotronic compact Data Loggers cover the most important measurement parameters and can measure climatic parameters such as humidity, temperature and ambient pressure. Small in size but accurate and fully compatible with the free evaluation and configuration Software HygroSoft.BL-1D Ambient Pressure and Dew Point Humidity Data LoggerIn addition to humidity and temperature, the BL-1D also logs ambient pressure and dew point.
  9. Socomec Webview - Datalogger
    Mulai

    Rp14.999.900

    Socomec Webview - Datalogger
    Deskripsi:
    Monitoring software for energy measurement and analysis.WEBVIEW is a web bassed software embedded in DIRIS A-40 meters and in communication gateways (DIRIS G, DIRIS DIGIWARE D-70, DATALOG H80/H81) delivering real time monitoring of all measurements from up to 200 devices and displaying the breakdown of energy consumptions.Uncover the causes of electrical disturbances and anticipate maintenance requirements thanks to historical records of multiple electrical parameters.Pre-set alarms defined by the user can be sent by e-mail. Users can access WEBVIEW via a web browser on a PC or a tablet.
  10. TESTO WiFi Data Logger
    Mulai

    Rp5.999.900

    TESTO WiFi Data Logger
    Deskripsi:
    testo Saveris 2-T1; WiFi data logger (wirelessLAN) with display and internal NTC temperaturesensor, incl. USB cable, wall bracket, batteries andcalibration protocolWiFi (wireless LAN)Signal transmission: wireless; frequency band: 2.4 GHz; supported wireless LAN standards: IEEE 802.11 b/g/n and IEEE 802.1X Possible encryption methods: without encryption, WEP, WPA, WPA2, WPA2 Enterprise The data loggers communicate via the standard protocol MQTT and are SNTP time synchronization-capable
    atribut:
    • Communication Rate: Dependent on Cloud licence; Basic: 15 min to 24 h / Advanced: 1 min to 24 h
    • Measuring Rate: Dependent on Cloud licence; Basic: 15 min to 24 h / Advanced: 1 min to 24 h
  11. Hioki Instrumentation Logger
    Mulai

    Rp3.099.900

    Hioki Instrumentation Logger
    Deskripsi:
    For 4-20 mA Instrumentation Measurement Data LoggerHioki compact 1 or 2-channel data loggers feature a 60,000 data set/channel memory to measure temperature, humidity, voltage or instrumentation signals. The LR5031 logs instrumentation signals such as 4-20mA signals over 1 channel in as fast as 1 second intervals.
    atribut:
    • Storage Capacity: Instantaneous value mode: 60,000 data, Statistical value mode: 15,000 data
    • Waterproof and Dust-proof: IP54 (EN60529) (with connection cable connected, but not including cable tip)
    • Interfaces: Infrared optical communications with LR5091, LR5092-20
  12. TESTO Mini Temperature Data Logger
    Mulai

    Rp2.199.900

    TESTO Mini Temperature Data Logger
    Deskripsi:
    If your professional work involves food or pharmaceutical products, you know that the storage temperature of your goods should not exceed specific limit values under any circumstances. The testo 174T mini temperature data logger helps you comply with the specified temperature ranges. It records the temperature values reliably and thus ensures uninterrupted measurement data recording and documentation. This is what the testo 174T mini temperature data logger offers You can save up to 16 000 readings with the testo 174T temperature data logger securely. Because measurement data you have saved will not be lost even when the battery is empty or being replaced. This means a high level of data security is guaranteed. You can easily and quickly read the current temperature measuring value on its large display, along with any possible violations of limit values. The integrated NTC sensor stands for a high level of accuracy. Its large measuring range, from -30 to +70 °C, and its compact design make the testo 174T temperature data logger a competent support for virtually every kind of temperature recording.The testo 174T mini temperature data logger meets the requirements of EN 12830 and is HACCP-compliant, as well as having international HACCP certification, which means it is ideally suited for measurements in the food industry (e.g. for storage temperature measurement). Particularly practical: the data logger has water spray and jet protection according to IP 65. This enables it to be left in the measuring location even when warehouses are being cleaned. The temperature data logger is also suitable for temperature control in refrigerators or cold stores, because it can be used at temperatures down to -30 °C. Programming and analysis with the mini temperature data logger You can choose between three software versions for programming and reading your data logger and for analyzing the measurement data on the PC: ComSoft Basic software - available as a free download - for fast programming of the temperature data logger and easy data analysis ComSoft Professional software - can also be ordered as an option - offers a variety of possibilities for detailed analysis of temperature readings ComSoft CFR 21 Part 11 software - can also be ordered as an option - the best solution for special requirements according to CFR 21 Part 11 in the pharmaceutical sector You need a USB interface for programming and reading the mini temperature data logger.Attention: Please download the newest software version before using the USB interface for the first time. The software can be found in the download area. Product Includes: testo 174T mini temperature data logger, including wall bracket, batteries (2 x CR 2032 lithium) and calibration protocol.Monitoring and documentation of the temperature in cold rooms Many foods and drugs have to be stored within a specific cold temperature range. This can be done in individual cooled store rooms, but also in specialised cold stores or cold warehouses with high-rack facilities. The temperature must be continuously documented in all these cold storage facilities, because strict rules apply to quality management in both the food and drugs industries.Data loggers are usually installed at the so-called critical control points (CCPs) of the cold room, in order to identify any possible temperature deviations and to introduce appropriate countermeasures. Critical points are for instance doors or passages through to other temperature areas within a warehouse. Monitoring and documentation of transport temperature For all goods which react sensitively to temperature fluctuations or have to be stored within a predefined temperature range, uninterrupted measurement data recording and documentation play a major role.Incorrect temperature conditions during transport can lead to major losses of quality, including the total loss of value of the products that require monitoring.Using a data logger, shipments can be checked for compliance with the specified temperature ranges and the data can then be read, analysed and archived by means of special software. Monitoring the temperature in deep-freeze rooms for food There are many facilities where (deep) frozen foods need to be stored. These range from individual deep-freeze rooms at small food producers (e.g. butcher's shops), restaurants and supermarkets, via deep-freeze rooms in the food processing industry, right through to specialized refrigerated warehouses/high-bay deep-freeze warehouses. In all of these facilities, the temperature has to be documented continuously. Only temperature recording devices that comply with EN 12830 are allowed to be used in Europe.  Data loggers are typically used to measure the air temperature in storage facilities of this kind. The measuring instrument is positioned in the deep-freeze room, where possible at critical locations, such as doors or refrigeration units, where it records temperature data at specified intervals (typically: every 15 minutes). The recorded data can subsequently be analyzed and archived using special software.
    atribut:
    • Measuring Rate: 1 min - 24 h
    • Memory: 16,000 Measuring values
    • Operating Temperature: -30 to 70 °C
    • Protection Class: IP65
    • Battery Life: 500 days (15 min Measuring cycle, +25 °C)
    • Battery Type: 2x3V button cell (CR 2032)
    • Channels: 1 internal
    • Dimensions (mm): 60x38x18.5
    • Product Color : White
    • Product/Housing Material: Plastic
    • Standards: EU-guideline 2014/30/EU; 2011/65/EU
    • Storage Temperature: -40 to +70 °C
    • Weight (g): 35
  13. ebro Temperature Data Logger
    Mulai

    Rp3.699.900

    ebro Temperature Data Logger
    Deskripsi:
    With internal temperature sensorApplication samples• For process monitoring during convenience food production• For routine control in bedpan washers• For temperature mappings• To measure in raw material storage
  14. TZONE Data Logger Suhu
    Mulai

    Rp629.900

    TZONE Data Logger Suhu
    Deskripsi:
    - Original TZONE- Mendapatkan Sertifikat Kalibrasi berstandar NIST USA, dan CNAS- Plug and play, tanpa software: Otomatis memberikan laporan PDF/CSV- Temperature Data Logger yang ideal digunakan untuk pergudangan, logistik, ekspedisi, transportasi bahan makanan, obat-obatan, bahan kimia, cold storage , laboratorium, dll.
    atribut:
    • Accuracy: +/- 0.5 C (-20 top 40 C), +/- 1 C (other range)
    • Alarm Delay: Programmable (0 to 960 minutes), default: 10 minutes
    • Alarm Range: Programmable high or low alarm limit for each channel
    • Communication Interface: USB 2.0
    • Default Temperature Alarm Range (°C): less than 2 or greater than 8
    • Dimensions (mm): 89x36x16
    • Interval: Programmable (10s to 18 h), default: 10 minutes
    • Memory Capacity: 32000
    • Recording Option: Push-to-start or Start Delay
    • Resolution: 0.1
    • Shelf Life/Battery: Typically 1 year, CR2032 3.0V Lithium battery
    • Start Delay: Programmable (0 to 254 minutes), default: 30 minute
    • Temperature Operating Range (°C): -30 to 60
    • Temperature Scale: °C or °F
    • Time Zone: UTC +0:00 (default)
    • Waterproof Level: IP65 (with waterproof O-ring)
  15. Elitech Digital Temperature and Humidity Data Logger
    Rating:
    100% of 100
    (1)
    Mulai

    Rp1.099.900

    Elitech Digital Temperature and Humidity Data Logger
    atribut:
    • Temperature Range (°C/°F): -40 to +85/-40 to 185
    • Humidity Range (%RH): 0 to 100
    • Resolution (°C/°F/RH): 0.1; 0.1
    • Record Capacity Temperature (points): 16000
    • Logging interval: 10 seconds to 24 hours
    • Data Interface: Micro USB
    • Alarm Configuration: Buzzer; LCD Display
    • Certification: EN12830, CE, RoHS
    • Dimensions (mm): 118x61.5x19
    • Logging Mode: Stop when full; Circular logging
    • Power Supply: Single-use 3.6V ER14505H lithium battery; Or powered via USB
  16. Benetech Data Logger Kelembaban dan Suhu
    Mulai

    Rp1.199.900

    Benetech Data Logger Kelembaban dan Suhu
    Deskripsi:
    Pengukur Data Kelembaban & Suhu Benetech GM1365Data-Logger konsumsi daya rendah ini menggabungkan fungsi pengambilan sampel sinyal, tampilan, penyimpanan dan analisis, diterapkan secara luas di industri obat-obatan, pengolahan makanan, penelitian pertanian, laboratorium, elektronik, AC, layanan cuaca, manajemen arsip, dll.
    atribut:
    • Temperature (°C): -30 to 80
    • Humidity (%RH): 0-100
    • Recording Capacity: 32256
    • Power: 3.6V 1/2AA Lithium Battery (not included)
    • Accuracy Error: (+/-)0.3°C (Typical); (+/-) 2% RH (Usual)
    • Item Size (mm): 126x28x22
  17. TESTO Temperature Data Logger for Transport Monitoring
    Mulai

    Rp2.299.900

    TESTO Temperature Data Logger for Transport Monitoring
    Deskripsi:
    Under normal conditions, the sublimation of dry ice takes place at -78.48 °C. With the temperature data loggers testo 184 t4, you can monitor the transport of pharmaceuticals with dry ice over an unlimited period of time and up to -80 °C. More info on applications (link to tab Applications)At their destination, a glance at the LEDs tells you whether the configured limit values have been adhered to. In order to obtain detailed information, it is sufficient to connect the logger to a PC - a PDF report is immediately generated with all relevant data. In order for you to be able to work even more efficiently and conveniently with the data loggers, all required files and information are stored directly and securely in the testo 184 T4: Configuration file, acceptance test certificate 3.1 according to DIN ISO 10204, instruction manual and PDF report of your recorded data.The measurement value store of the temperature data logger testo 184 T4 has a capacity of 40000 measurement values. The measurement rate is freely selectable from 1 min to 24 h. The battery has a life of 100 days (at -80 °C and 15 mins measurement rate). The temperature data logger testo 184 T4 is supplied by a standard battery which can be exchanged by the user.testo 184 T4 is compliant with GxP, 21 CFR Part 11, HACCP and EN 12830. Testo is an ISO 9001-certified company, and ensures the adherence to the norms through internal audits as well as accredited external audits.All advantages at a glance:1. Clear alarm indicationA glance at the the LEDs is enough to know whether limit values have been violated during transport. 2. Easiest operationtesto 184 T4 is intuitively operated, and can be used without special training or previous knowledge: The "Start" button begins data recording. "Stop" ends it. 3. Easiest configurationIn each testo 184 T4, a configuration file is stored, with which the configuration of the testo 184 T4 is childsplay - no download, no installation, no user interface and no additional costs. 4. Convenient readoutA PDF report with the transport data is created immediately on connection of the testo 184 T4 data logger to the USB interface of a computer. This is suitable for long-term archiving according to PDF/A standard. 5. Mobile readout/printout on siteData transfer from the data logger to a compatible Testo fast printer (option) also functions wirelessly via NFC. 6. IT-safeThe testo 184 T4 data loggers work securely without software installation or download, so that IT problems are triggered neither by the firewall nor the virus scanner. Product Includes: Temperature data logger testo 184 T4, including acceptance test certificate 3.1 according to DIN ISO 10204 (stored in testo 184 T4 ), battery and 1 piece double-sided adhesive tape for easy attachment of the data logger.Monitoring and documentation of temperature, humidity and shock in food logistics Handling foods involves danger to human health at all levels. In order to be able to eliminate them as far as possible, food companies must comply with an HACCP concept which guarantees food safety along the entire production chain – "from farm to fork". The adherence to product-specific limit values and the uninterrupted monitoring of the cold chain are crucial. In many cases, the monitoring of humidity and shock, in addition to temperature, are relevant for the maintenance of food quality.With the testo 184, quality managers in food logistics have six HACCP International-certified data loggers available to them, which monitor and document all critical parameters during the transport of foods. The data loggers testo 184 T1,T2, T3 and T4 have been additionally tested and certified according to EN 12830 by the TÜV Süd, and are therefore ideally suitable for the transport of refrigerated and deep-frozen foods. Monitoring and documentation of temperature, humidity and shock in logistic services of all kinds Providers of logistic service often take on the responsibility for expensive and sensitive products from the fields of pharmaceuticals, food, electronics or art. The wrong conditions during transport can lead to considerable losses of quality, right up to the complete devaluation of the monitored products.With the help of the testo 184 data logger, the prescribed temperature and humidity limit values as well as the shock tolerance levels can be monitored during transport, and thanks to the automatic report creation, very easily analyzed and documented. This allows all doubts regarding the correct transport conditions to be eliminated.Shock-sensitive products such as electronics, delicate machinery or certain bio-pharmaceuticals can be additionally monitored for the violation of previously defined shock limits with the help of the testo 184 G1. Monitoring and documentation of temperature, humidity and shock in pharmaceutical logistics Most pharmaceuticals must be continuously transported and stored at defined upper and lower temperature and humidity limit values, along the entire supply chain. A violation of these predefined upper and lower limit values can lead to irreversible alterations of the active ingredients or the composition of the medicaments. However, not only medicaments and their active ingredients are endangered. Minus temperatures or extreme temperature fluctuations can also cause damage to containers or medical instruments. The consequence is the threat of spoilage of the entire goods, financial losses and damage to reputation.In GxP-compliant quality management, the control of the entire cold chain, from production to delivery, is therefore a prerequisite, in order not only to ensure product quality, but also to prevent financial losses and damage to your reputation in the pharmaceutical industry.With the testo 184 data loggers, your products can be protected from unnoticed gaps in the cold chain, and the entire distribution path monitored and documented simply, securely and compliantly with all common standards, guidelines and regulations.
    atribut:
    • Protection Class: IP67
    • Certificate Type: Certified by HACCP International
    • Channels: 1 internal
    • Interface: USB; NFC
    • Product Color : White
    • Product/Housing Material: ABS
    • System Requirements: Adobe Acrobat Reader
  18. Extech Volt/Current AC Datalogger TRMS
    Mulai

    Rp7.199.900

    Extech Volt/Current AC Datalogger TRMS
    atribut:
    • Item: Voltage Detector
    • Netto Weight (kg): 0.25
    • Manufacturing Number: DL150
    • Dimension Unit (mm): 114x63x34
    • Type: Voltage Detector
  19. Elitech Data Logger Suhu dan Kelembaban
    Mulai

    Rp929.900

    Elitech Data Logger Suhu dan Kelembaban
    Deskripsi:
    Elitech GSP-6 Temperature & Humidity Data Logger ini terutama digunakan untuk mencatat suhu dan kelembaban makanan, obat-obatan dan bahan kimia, dll. Dalam penyimpanan dan transportasi. Ini secara luas berlaku untuk setiap tautan dalam penyimpanan dan logistik rantai dingin, seperti wadah berpendingin, truk kulkas, tas pendingin, lemari coo, lemari obat, cold storage, laboratorium, dll.Elitech GSP-6 sesuai dengan standar GSP edisi baru. Ini memiliki satu layar LCD besar, tombol, sensor suhu eksternal dan sensor kelembaban eksternal. Dengan dua mode untuk menyimpan data: rekaman berhenti penuh dan rekaman siklik, pencatat data memiliki fungsi melebihi batas alarm suara-cahaya. Ini juga dapat secara otomatis mempersingkat rekaman, interval jika suhu berlebih dan batas kelembaban. Dua buah magnet built-in nyaman untuk memperbaiki pencatat data ke permukaan bahan logam.Elitech GSP-6 data suhu dan kelembaban logger terutama digunakan untuk mencatat suhu dan kelembaban makanan, obat-obatan dan bahan kimia, dll. Hal ini secara luas berlaku untuk setiap link dalam penyimpanan dan logistik rantai dingin, seperti wadah berpendingin, truk kulkas, tas pendingin, lemari pendingin, lemari obat, penyimpanan dingin, laboratorium, dll. Data logger ini sesuai dengan standar GSP edisi baru sangat sesuai dengan harga.
  20. ebro Multi-Use PDF Data Logger
    Mulai

    Rp3.899.900

    ebro Multi-Use PDF Data Logger
    Deskripsi:
    Standard versionFor transport and storage monitoring.Applications: Logistics, Laboratory, Pharma – Vaccine –Drugs, Food and Storage control• Tamper proof• PDF reports created at the destination with no additional software required• USB interface eliminates need for additional interface
Daftar Harga data logger Terbaru March 2026
Elitech Temperature Data LoggerRp429.900
Hioki Temperature LoggerRp3.099.900
TESTO Data LoggerRp4.899.900
TESTO Mini Data LoggerRp4.799.900
AND Temperature Data LoggerRp1.199.900
AS ONE Data LoggerRp33.999.900
TESTO Nonelectrical Properties Data LoggerRp3.099.900
ROTRONIC Humidity DataloggerRp2.599.900
Socomec Webview - DataloggerRp14.999.900
TESTO WiFi Data LoggerRp5.999.900

Data diperbarui pada 07/03/2026 (Harga belum termasuk PPN)