Beli vacuum cleaner backpack di monotaro.id

Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
  1. Innotechs Backpack Dry Vacuum Cleaner
    Mulai

    Rp2.299.900

    Innotechs Backpack Dry Vacuum Cleaner
    atribut:
    • Power (W): 1000
    • Voltage (V): 220-240
    • Air Flow Rate (L/s): 48
    • Vacuum Suction (Mbar): 190
    • Cable Length (m): 18
    • Hose Diameter (mm): Ø 36
    • Functions: Dry
    • Tank Capacity (L) : 3
  2. KARCHER Professional Backpack Vacuum Cleaner
    Mulai

    Rp9.199.900

    KARCHER Professional Backpack Vacuum Cleaner
    Deskripsi:
    KARCHER Back Pack Vacuum Cleaner is The new backpack vacuum cleaner BV 5/1 can be carried comfortably on the back like a rucksack above all because of its low weight of just 5.3 kg. The BV 5/1 is particularly used where it is too thight for conventional vacuum cleaners: Between seat rows of cinemas and theatres, in buses, trains and airplane cabs, in stairways of hotels and offices as well as in strongly transferred areas.
    atribut:
    • Air Flow Rate (L/s): 53
    • Cable Length (m): 15
    • Turbine Power (W): 800
    • Vacuum (mbar/kPa): 240/24
    • Voltage (V): 220-240
    • Part Number: 1.394.200.0
    • Container Capacity (L): 5
    • Dimensions (mm): 400x320x540
    • Frequency (Hz): 50-60
    • Maximum Rated Input Power (W): Max. 800
    • Sound Pressure Level (dBA): 62
    • Standard Nominal Width: ID/35
  3. NILFISK Vacuum Dry Backpack with Hepa Eu
    Mulai

    Rp10.999.900

    NILFISK Vacuum Dry Backpack with Hepa Eu
    Deskripsi:
    There are many things that should be present in a good backpack vacuum cleaner. It should be light in weight, with even weight distribution, and the noise level must be as low as possible. At the same time, the power needs to be sufficient for fast, effective cleaning, and the dust bag must be large enough to avoid constant changing. Without these basics, a backpack vacuum cleaner is uncomfortable and impractical to operate. The GD5 backpack vacuum cleaner meets these criteria and more. There are many things that should be present in a good backpack vacuum cleaner. It should be light in weight, with even weight distribution, and the noise level must be as low as possible.The Nilfisk GD 5 backpack vacuums surpass all criteria, making fast productive cleaning at a price that won’t bust your budget.
    atribut:
    • Rated Power (W): 1300
    • Dimensions (mm): 380x260x570
    • Cable Lengt (m): 15
    • Vacuum at Nozzle (kPa): 24
    • Air Flow (L/s): 41
    • Dust Bag Capacity (L): 5
    • Frequency (Hz): 50-60
    • Main Filter Area (cm²): 1400
    • Sound Pressure Level (dBA): 59
    • Suction Motor Power (W): 255
    • Suction Power End of Tube (W): 240
    • Voltage (V): 240
  4. KARCHER Professional Battery Vacuum Cleaner
    Mulai

    Rp17.999.900

    KARCHER Professional Battery Vacuum Cleaner
    Deskripsi:
    The new powerful and battery-operated backpack vacuum BV 5/1 Bp is the first choice wherever a lack of space makes cleaning work difficult – whether in the cinema, aeroplane, buses, trains or also on stairs. The powerful Kärcher Battery Power+ battery ensures maximum suction power with very long runtimes. The clever, ergonomic and patented carrying frame with Air Stream Comfort system enables simple handling, reduces the build-up of heat on the back and at the same time prevents annoying vibrations. It can be easily adjusted to various users, thus ensuring a high level of comfort. The machine is also easy to operate because all important operating and additional functions, such as eco!efficiency mode or the charge status display, are controlled directly via the control panel on the hip strap
    atribut:
    • Container Volume (L): 5
  5. INABA DENKO Duct Tape Non Lem
    Mulai

    Rp40.900

    INABA DENKO Duct Tape Non Lem
    Deskripsi:
    Best Choice to Cover The Exposed Insulation. Tight Fitting and Very Strong Against Sunshine. Specially Formulated Non-Adhesive Tape Will Not Unroll by Itself Even If Dropped During Application.
    atribut:
    • Thickness: 0.12mm
    • Material: PVC
  6. KLAZ Cordless Vacuum Cleaner
    Mulai

    Rp3.599.900

    KLAZ Cordless Vacuum Cleaner
    atribut:
    • Water Tank Capacity (ml): 400
    • Maximum Suction Power (KPa): Up to 20
    • Battery Capacity (mAh): 2600
    • Charging Time (hour): 4
    • Dimensions (cm): 35x35x10
    • Dust Tank Capacity (ml): 600
    • Filter: HEPA H13
    • Maximum Power (W): 200
    • Packaging Dimensions (cm): 103.1x16.5x35.3
    • Suction Power (Pa): 8000 (Low), 20000 (High)
    • Type: Cordless
    • Working Time (minute): Up to 50
  7. Makita Cordless Backpack Vacuums
    Mulai

    Rp12.999.900

    Makita Cordless Backpack Vacuums
    Deskripsi:
    Bagged, cordless backpack vacuums rest on your back and operate without the limitations of a power cord to trap dirt, dust, and allergens in reusable bags or replaceable bags that are discarded when full. They keep debris contained for disposal to help prevent recirculation of dust and allergens, making them a common choice for vacuuming in healthcare and educational settings.
    atribut:
    • Voltage (V): 16
  8. Makita Cordless Backpack Vacuum Cleaner
    Mulai

    Rp6.599.900

    Makita Cordless Backpack Vacuum Cleaner
    atribut:
    • Voltage (V): 18
  9. HEIKO Kantong Plastik Bening OPP
    Mulai

    Rp43.900

    HEIKO Kantong Plastik Bening OPP
    atribut:
    • Thickness (mm): 0.03
    • Color: Transparent
  10. KARCHER Professional Wet & Dry Cleaners
    Rating:
    100% of 100
    (2)
    Mulai

    Rp3.099.900

    KARCHER Professional Wet & Dry Cleaners
    Deskripsi:
    KARCHER Wet & Dry Cleaners NT Indispensable: wet and dry vacuum cleaners effortlessly pick up all kinds of dirt. Whether dry, wet or liquid: Kärcher machines pick up everything. This means that you can use the vacuum cleaner purely as a wet vacuum cleaner or just as a dry vacuum cleaner.
  11. KARCHER Professional Dry Vacuum Cleaners
    Mulai

    Rp5.999.900

    KARCHER Professional Dry Vacuum Cleaners
    Deskripsi:
    Standard equiped with a high effective fleece filter bag which allows an up to three times higher filter bag volume in contrast to a paper filter bag. This is a benefit that pays for itself since the operating periods between filter bag changes are longer. The T 12/1 eco!efficiency motor performance, air flow and the 6-stage filter system (incl. microfilter as special option) have been designed in such a way that there is hardly any loss of suction power. Its low centre of gravity provides stability. The power cable can be wind up in between the cable storage or onto a pull-out cable hook as a fast storage when often changing the location, e.g. cleaning objects in hotels, ect. Special feature: the floor tool plugs into the accessory holder (on the back of the unit) and can be used as a complete accessory fixation at the machine after work. The suction hose on the unit has a simple but effective plug-in clip system. You push the hose on to the unit's intake stub, a resilient ring engages – that's all. This system ensures that the suction hose does not become detached when the unit is pulled along behind the user. The new clip system (change without tools) on the bend allows an easy extension of the suction hose of additional 2,5 m (extra extension suction hose - part number 6.906-237.0) for e.g. cleaning steps, stairways, etc. With the power brush ESB 28 (additional accessory) the T 12/1 eco!efficiency converts into a brush-type vacuum cleaner. In cases where the hygienic standards are particularly stringent, a HEPA filter which retains very fine particles (99.95% retention rate) can be fitted (instead the standard air exhaust filter) in addition to the paper filter bag. Equipment - Suction hose, 2.5 m - Suction Tube, 2 piece(s), 0.5 m - Filter bag, fleece - Container material, plastic - Clip system for hose extension - Safety class, II - Permanent filter basket, fleece
  12. KARCHER HOME & GARDEN Multi Purpose Vacuum Cleaners
    Rating:
    100% of 100
    (3)
    Mulai

    Rp1.699.900

    KARCHER HOME & GARDEN Multi Purpose Vacuum Cleaners
    Deskripsi:
    KARCHER Multi Purpose Vacuum Cleaners is A vacuum cleaner for diverse usage. A match for any type of dirt: the Kärcher multi-purpose vacuum cleaners are ideal for car interior cleaning, workshops, garages, cellars, outside areas and renovation.
  13. KARCHER Professional High Pressure Cleaners-Cold Water
    Rating:
    100% of 100
    (1)
    Mulai

    Rp15.999.900

    KARCHER Professional High Pressure Cleaners-Cold Water
    Deskripsi:
    KARCHER High Pressure Cleaners-Cold Water is a cold shower for stubborn dirt. Clean machines, vehicles and buildings daily: with high pressure and a high flow rate. Cold water high-pressure cleaners remove even stubborn dirt and are Ideal for large areas.
  14. INABA DENKO Duct Tape Lem
    Mulai

    Rp68.900

    INABA DENKO Duct Tape Lem
    Deskripsi:
    Best Choice to Cover The Exposed Insulation. Tight Fitting and Very Strong Tape Against Sunshine. Thinner Than The Older HF Series, Improved Flexibility Allows Ease of Application.
    atribut:
    • Thickness: 0.18mm
    • Material: PVC
  15. KRISBOW Vacuum Cleaner Basah dan Kering
    Rating:
    100% of 100
    (4)
    Mulai

    Rp899.900

    KRISBOW Vacuum Cleaner Basah dan Kering
    Deskripsi:
    Jaga rumah Anda agar senantiasa bersih dengan menggunakan Penghisap Debu Kering & Basah Krisbow yang terbuat dari baja tahan karat dengan kualitas terbaik. Filter dapat dicuci setelah dipakai dan mempunyai 2 fungsi, untuk debu basah dan kering. Penghisap debu ini sangat efisien jika digunakan karena dapat menghisap debu maupun cairan yang tumpah dan cocok untuk digunakan baik untuk kebutuhan rumah tangga maupun kantor.
    atribut:
    • Frequency (Hz): 50
  16. Innotechs Wet & Dry Vacuum Cleaners
    Mulai

    Rp1.899.900

    Innotechs Wet & Dry Vacuum Cleaners
    atribut:
    • Voltage (V): 220-240
    • Functions: Wet and Dry
  17. Bellstar Abrasive Mfg. Abrasive Paper Waterproof MATADOR (Kertas Amplas)
    Mulai

    Rp1.299.900

    Bellstar Abrasive Mfg. Abrasive Paper Waterproof MATADOR (Kertas Amplas)
    Deskripsi:
    -Waterproof paper manufactured by STARCKE, a German long-established abrasive cloth paper manufacturer founded in 1829.
    atribut:
    • Grain Size: #3000
    • WidthxLength: 230x280mm
    • Purpose of Use: Polishing of metal, wood, plastic, and ceramics, etc. Polishing of metal and wood painted surfaces.
  18. KARCHER Professional Vacuum Cleaner Basah & Kering
    Rating:
    100% of 100
    (1)
    Mulai

    Rp3.999.900

  19. BELLSTAR Abrasive Paper Waterproof MATADOR (Kertas Amplas)
    Mulai

    Rp869.900

    BELLSTAR Abrasive Paper Waterproof MATADOR (Kertas Amplas)
    atribut:
    • Material: Grindstone material: Silicon carbide (C)
    • Width (mm): 230
    • Length (mm): 280
Daftar Harga vacuum cleaner backpack Terbaru March 2026
Innotechs Backpack Dry Vacuum CleanerRp2.299.900
KARCHER Professional Backpack Vacuum CleanerRp9.199.900
NILFISK Vacuum Dry Backpack with Hepa EuRp10.999.900
KARCHER Professional Battery Vacuum CleanerRp17.999.900
INABA DENKO Duct Tape Non LemRp40.900
KLAZ Cordless Vacuum CleanerRp3.599.900
Makita Cordless Backpack VacuumsRp12.999.900
Makita Cordless Backpack Vacuum CleanerRp6.599.900
HEIKO Kantong Plastik Bening OPPRp43.900
KARCHER Professional Wet & Dry CleanersRp3.099.900

Data diperbarui pada 06/03/2026 (Harga belum termasuk PPN)

Halaman Terkait