Hanna Instruments Photometer Portable Total Chlorine ULR HI97761 1unit

#Nomor SKU S034715611
Wishlist
Rp16.999.900
Persediaan

Spesifikasi Produk

Model Number HI97761
Unit 1unit
Display 128x64 pixel B/W LCD with backlight
Logging Memory 50 measurement
GLP Date, time of last calibration
Environment Temperature (°C) 0 to 50 (32 to 122°F); relative humidity: 100% (IP 67, floating case)
Range (mg/L) 0.000 to 0.500 (ppm) (as Cl2
Method Adaptation of the USEPA method 330.5
Dimensions (mm) 142.5x102.5x50.5
Automatic Shut-off After 15 minutes of inactivity (30 minutes before a READ measurement)
Resolution (mg/L) 0.001 (ppm)
Cuvette Type Round, 24.6 mm diameter (22 mm inside)
Bandpass Filter Wavelength Accuracy (nm) ±1.0
Bandpass Filter Bandwidth (nm) 8
Photometer/Colorimeter Light Source LED
Photometer/Colorimeter Light Detector Silicon photocell with narrow band interference filter @ 525 nm
Accuracy (mg/L) ±0.020 ±3% of reading
Battery Type/Life 1.5V AA battery (3 pcs.) / > 800 measurements (without backlight)
Berat (Kg) 0.3
Tanggal Produk Terdaftar 08 December 2022
Terakhir Diperbaharui 04 September 2026
ask-button

Apakah produk dengan spesifikasi yang Anda inginkan belum tersedia? Hubungi tim Layanan Pelanggan kami di sini

Informasi Produk

Description
This meter offers a superior optical system that utilises a reference detector and narrow band interference filters for extremely fast and repeatable measurements.

No warm up time before taking a measurement
Tutorial mode for step-by-step instructions
Uses either powder or cost saving liquid reagents


Each photometer is delivered in a cardboard box and is supplied with:

Sample cuvette (2 pcs.)
Sample cuvette cap (2 pcs.)
Plastic stopper (2 pcs.)
1.5V AA Alkaline batteries
Instrument quality certificate
Instruction manual

The photometer has an innovative optical system that offers superior performance in accuracy, repeatability and the short amount of time it takes to perform a measurement. This compact, waterproof meter is extremely user friendly with a tutorial mode that walks the user graphically, step by step, in performing a measurement. The use of a backlit dot matrix LED allows the use of virtual keys which makes the operation of the meter very intuitive including selecting different methods, reviewing GLP data, recalling the last 50 measurements, and customising the meter to user preferences.
The photometer is waterproof including the cuvette holder that is designed with ridges to protect the optical path from getting scratched by the cuvette and a protected battery compartment that holds three AA batteries. The compact design fits comfortable in the hand for use in the field or on a table for benchtop use. The LCD is 71 mm (2.75") by 37 mm (1.6") and is backlit for easy viewing under all conditions.

Advanced optical system
LED that generates very little heat.
8 nm narrowband interference filter that is accurate to +/- 1 nm and offers 25% increase in light efficiency.
Reference detector that modulates the voltage to LED for consistent light output.
A concave focusing lens that reduces errors from imperfections in the cuvette.
Stable Light Source:
The internal reference system of the photometer compensates for any drifts due to power fluctuations or ambient temperature changes. With a stable source of light the readings are fast and stable between your blank (zero) measurement and sample measurement.

High Efficiency Light Source:
LED light sources offer superior performance compared to tungsten lamps. LEDs have a much higher luminous efficiency, providing more light while using less power. They also produce little heat, which could otherwise affect electronic stability.

High Quality Filters:
Improved optical filters ensure greater wavelength accuracy and allow a brighter, stronger signal to be received. The end result is higher measurement stability and less wavelength error.

Greater Light Yield:
A focusing lens collects all of the light that exits the cuvette, eliminating errors from imperfections and scratches that may be present in the glass. The use of the convex lens reduces the need for indexing cuvettes.

CAL Check Functionality:
Hanna's exclusive CAL Check feature allows for performance verification and calibration of the meter using NIST traceable standards. Our CAL Check standard vials are developed to simulate a specific absorbance value at each wavelength to verify the accuracy of subsequent readings.

Multiple Measurement Methods:
Users can select the use of powder reagents supplied in packets or the use of low cost liquid reagents supplied in a dropper bottle.

Built-in Reaction Timer:
Waiting the proper reaction time is of key importance when performing colorimetric measurements. The countdown timer displays the time remaining until a measurement will be taken, ensuring consistent results between sample measurements and users.

Large Cuvette Size:
The sample cell of the photometer fits a round, glass cuvette with a 25 mm path length. The relatively long path length of the sample cuvette allows the light to pass through more of the sample solution, ensuring accurate measurements even in low absorbance samples.

Intuitive Dot Matrix Display:
The photometer is designed with a backlit, graphic LCD. With virtual keys, a battery status indicator, and error messages. Users will find the meter interface intuitive and easy to read. A dedicated help key provides information relating to the current meter operation, and can be used at any stage in the setup or measurement process to show contextual help.

Auto-off Protection:
The meter uses three common AA batteries that allow for about 800 measurements to be taken. The auto-off feature automatically shuts off the meter after 15 minutes of inactivity in order conserve battery life.

Significance of use
As one of the most common forms of disinfectants used, chlorine improves water quality by destroying disease-producing microorganisms, and by reacting with other organic and inorganic substances. Chlorine levels must be actively monitored to ensure sufficient chlorine is present for disinfection, as well as to control adverse effects such as taste, odour, and potential reactions with organic matter to form harmful disinfection by-products.




Ketentuan dan Kondisi Barang

Pengembalian Barang 14 hari
Berubah pikiran tidak dapat diterima. Lihat selengkapnya
Ketersediaan Barang
Subtotal
GRATIS ONGKIR* ke Jabodetabek, Banten,
Jabar & Jatim dengan minimum total pesanan Rp200.000 saat checkout. Lihat selengkapnya

Pilih jenis produk yang diinginkan

Nomor SKU Model Number Masa Persiapan Barang Harga Jumlah
Loading...

Ulasan Produk

Tidak ada ulasan