ALTECO Epoxy Adhesive (Lem Epoksi Dua Komponen) F30C 1pc
Rp2.199.900
Persediaan
Spesifikasi Produk
| Model Number | F30C |
|---|---|
| Unit | 1pc |
| Retention period (year) | 1 |
| Characteristic | Durability, heat resistance, water resistance, weather resistance, chemical resistance, electrical insulation |
| Formaldehyde grade | F☆☆☆☆ |
| Adhesive Materials | Metal |
| Hardness (Shore D) | 80 |
| suitable usage | Waterproof/water resistant/outdoor |
| Name of The Hazardous | Synthetic resins and others |
| Main Works | Panel frame, Parts, 3D shape |
| Classification of the Hazardous | Designated combustibles |
| Time Can be Used (minute) | 20 |
| Tensile Shear Strength (N/mm²) | 13 |
| Appearance | (Main agent) colorless and transparent, (curing agent) yellow transparent |
| Main application | Metal, glass, pottery, trees, Plastic, if necessary: Metal, glass, pottery, tree, Plastic |
| Curing Time (minute) | 30 |
| Specific Gravity | (Main agent) 1.17, (curing agent) 1.14 |
| Main Component | (Maintaining agent) Modified epoxy, (curing agent) modified polythiol |
| Viscosity (mPa s) | (Main agent) 15000, (curing agent) 16000 |
| M Code | 24364847 |
| Berat (Kg) | 1.1 |
| Tanggal Produk Terdaftar | 17 December 2021 |
| Terakhir Diperbaharui | 02 October 2026 |
Informasi Produk
Description
How to use :
(1) Remove dirt, moisture, rust and oil on the adhesive surface.
(2) Remove the main agent and the curing agent at a specified blending ratio.
- Weigh the curing agent with an error of ± 5 to 10% for the main agent. In particular, if it is required to be strict characteristics, the error is smaller as much as possible.
- Basically, do not remove the main agent and the curing agent with the same sp. If you use the same spin, please wipe off and use it.
(3) Mix the main agent and the curing agent uniform.
- When using containers such as paper cups, make sure that unevenness does not appear on the surrounding area and bottom.
- When using plates such as PE, please reliably and mix until the surface of the plate is reached by the splash.
- The corners of the cup or plate may be insufficient. If you are using a small amount, do not use it because it will affect hardening.
(4) Apply to the surface to be bonded, bond it immediately and fix it so that it does not move.
- Curing starts with powerful time. Click within the time and complete the bonding.
(5) Do not move up to the curing time after bonding.
(1) Remove dirt, moisture, rust and oil on the adhesive surface.
(2) Remove the main agent and the curing agent at a specified blending ratio.
- Weigh the curing agent with an error of ± 5 to 10% for the main agent. In particular, if it is required to be strict characteristics, the error is smaller as much as possible.
- Basically, do not remove the main agent and the curing agent with the same sp. If you use the same spin, please wipe off and use it.
(3) Mix the main agent and the curing agent uniform.
- When using containers such as paper cups, make sure that unevenness does not appear on the surrounding area and bottom.
- When using plates such as PE, please reliably and mix until the surface of the plate is reached by the splash.
- The corners of the cup or plate may be insufficient. If you are using a small amount, do not use it because it will affect hardening.
(4) Apply to the surface to be bonded, bond it immediately and fix it so that it does not move.
- Curing starts with powerful time. Click within the time and complete the bonding.
(5) Do not move up to the curing time after bonding.
Warning
- Wipe off the main agent and hardener that have adhered to the container lid, nozzle, used equipment, etc. (If you make a mistake in the main agent and hardener lid, you may not be able to remove it). - After work, wash your hands and gargle thoroughly.
- Seal the container and store it in a dry, cool and dark place.
- Keep out of reach of children and be careful not to mischief.
- Incinerate waste based on the Waste Disposal and Cleaning Law and prefectural ordinances, or entrust a licensed disposal company to dispose of it.
- Do the same for containers and waste cloths.
- If it gets on your skin, wipe it off immediately and wash it off with soap and water or hot water. If you experience itching or inflammation, seek medical advice immediately.
- If inhaled, inhale the main agent, curing agent, and vapor due to the temperature rise during mixing, and if any abnormality such as itching occurs, consult a doctor immediately.
- If it spills, wipe it off with a piece of paper or cloth. If the amount is large, collect it in a container with a lid.
- If it gets in your eyes, immediately rinse with plenty of water and see an ophthalmologist immediately.
- If swallowed, do not force vomiting and seek medical advice immediately.
- Install a local exhaust system in the workplace such as mixing, injection, coating, and bonding processes.
- If a fire breaks out, turn off the incinerator to the source of the fire and extinguish it from the windward side with a powder or carbon dioxide (ABC type) fire extinguisher.
- Wear impervious gloves, long-sleeved work clothes, etc. so that you do not touch the human body directly, and avoid working methods that you handle directly by hand.
Feature
Demonstrates excellent performance such as strong adhesive strength, heat resistance & chemical resistance.Strong adhesive strength. Many materials can be bonded. In particular, it has excellent adhesion to metals, concrete & porous materials.
Excellent durability. It has excellent heat resistance, water resistance, weather resistance & chemical resistance.
Low curing shrinkage. Since it does not contain volatile solvents, there is almost no shrinkage due to curing.
Electrical insulation. Does not conduct electricity. It is an excellent insulator.
Environmentally friendly. A low formalin adhesive.
Ketentuan dan Kondisi Barang
Pengembalian Barang 14 hari
Berubah pikiran tidak dapat diterima. Lihat selengkapnya
GRATIS ONGKIR* ke Jabodetabek, Banten,
Jabar & Jatim dengan minimum total pesanan Rp200.000 saat checkout. Lihat selengkapnya
Jabar & Jatim dengan minimum total pesanan Rp200.000 saat checkout. Lihat selengkapnya
Pilih jenis produk yang diinginkan
| Nomor SKU | Model Number | Masa Persiapan Barang | Harga | Jumlah |
|---|---|---|---|---|
| Loading... | ||||
Produk Terpopuler
Ulasan Produk
Tidak ada ulasan



















































































































































%20%26%20Pengelasan/Lem%2C%20Bahan%20Perbaikan/Lem%20Industri/Tipe%20Dua%20Komponen/ALTECO%20Epoxy%20Adhesive%20(Lem%20Epoksi%20Dua%20Komponen)/ALTECO%20Epoxy%20Adhesive%20(Lem%20Epoksi%20Dua%20Komponen)%20F30C%201pc/c9S030248441-1.jpg)
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
/WD-40%20Multi-Purpose%20Lubricant%20(Pelumas%20Serbaguna)%20333ml%201pc/60S000055216-2.jpg)
/OLFA%20Cutter%20Knife%20Safety%20(Pisau%20Cutter)%20149B%201pc/S009054721-2.jpg)
/Joyko%20Gel%20Ink%20Pen%20Q%20(Pulpen%20G2%20%2F%20Pulpen%20Gel)%20GP-265%20Black%200_5mm%201box(12pcs)/qmS009904958-2.jpg)
/REXCO%20Multi-Purpose%20Lubricant%20(Pelumas%20Serbaguna)%20RX-SP0009%20500ml%2F415g%201pc/2bS000076083-4.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Sarung%20Tangan/Sarung%20Tangan%20Tahan%20Minyak/Sarung%20Tangan%20Tahan%20Minyak%20Karet%20Nitril/ANSELL%20Gloves%20Solvex%20Nitrile%20(37-176)%20(Sarung%20Tangan%20Nitrile%20Anti%20Kimia)/ANSELL%20Gloves%20Solvex%20Nitrile%20(37-176)%20(Sarung%20Tangan%20Nitrile%20Anti%20Kimia)%2037-176%20Size%209%201pair/S000074366-1.jpg)

%20Copy%20Paper%20A4%2070gsm%20(Kertas%20HVS%20%2F%20Fotocopy)/IKA%20(Copy%20Paper)%20Copy%20Paper%20A4%2070gsm%20(Kertas%20HVS%20%2F%20Fotocopy)%20IKF%20PC%2070%20A4G%201ream/8pS035166313-2.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Kesehatan/Pertolongan%20Pertama%2C%20Kebutuhan%20Higienis/Perban%2C%20Kain%20Kasa/OneMed%20Alkohol%20Swab%20(Tisu%20Alkohol)/OneMed%20Alkohol%20Swab%20(Tisu%20Alkohol)%201box(100pcs)/h6S039287618-2.jpg)
/3M%20Post-it%20654%20Sticky%20Notes%20(Kertas%20Memo)%20654-5CY%201pack(5pads)/5iS030245198-4.jpg)
/monotaro_id%20Lakban%20OPP%202inch%20(Solasi%20%2F%20Selotip)%20Transparent%2048mmx64m%201roll/h7S036166619-4.jpg)

/monotaro_id%20Cable%20Ties%204_8x250mm%20(Pengikat%20%2F%20Kabel%20Tis)%20White%201pack(100pcs)/2xS039549105-2.jpg)
/Max%20Stapler%20Needle%20(Isi%20Staples)%20No_10-1M%205%2F16x3%2F16Inch%201pack(20pcs)/S000005230-4.jpg)
/monotaro_id%20Plas%20Chamois%20(Lap%20Kanebo)%20with%20tube%20Yellow%2032x21cm%201pc/4uS037754174-2.jpg)