A&D Multi-Channel Wireless Environmental Thermo-Hygrometer AX-KO4449 (AD5664 slave unit temperature probe) 1pc
Rp289.900
Persediaan
Spesifikasi Produk
| Model Number | AX-KO4449 (AD5664 slave unit temperature probe) |
|---|---|
| Unit | 1pc |
| Suitable Model | AD-5663,AD-5664SET,AD-5665SET |
| Cable Length (m) | About 2.5 |
| Accuracy | ± 1 degree (10 to 39.9 degrees), ± 2 degrees (-10 to 9.9 degrees, 40 to 49.9 degrees), ± 3 degrees (-40 to -10 degrees, 50 to 70 degrees) |
| M Code | 49831976 |
| Berat (Kg) | 0.1 |
| Tanggal Produk Terdaftar | 26 December 2025 |
| Terakhir Diperbaharui | 29 December 2025 |
Informasi Produk
Description
Wirelessly displays temperature and humidity, heat stroke index (WBGT), and absolute humidity (VH) at remote locations.
It can be used to know the danger of heat stroke and the epidemic of seasonal influenza.
Up to 5 slave units can be connected to one master unit.
The maximum communication distance is 100m (line-of-sight distance, height 1.2m).
Built-in sensor to measure environmental temperature and humidity.
A temperature probe (sold separately) can be connected, and up to two can be connected to one slave unit.
Soil temperature and liquid temperature can be measured (cable length of temperature probe is about 2.5 m).
Since the handset also has a liquid crystal display, it is possible to check the measured value at the measurement site.
Specified low power equipment, radio frequency used is 429.2MHz.
In an agricultural house. For measuring temperature and humidity and soil temperature (soil temperature) in the house such as raising rice seedlings, in a warehouse for vegetables, fruits, and liquor. For fermentation of crops such as vegetables and fruits, sake brewery / wine, temperature and humidity control of brewing, temperature and humidity of factories, offices, gymnasiums, facilities, houses, risk of heat stroke and influenza pandemic control ..
*If the product comes with general calibration documents, the relevant documents will be attached when shipped. *If you require the name and address of the person requesting the certificate, please be sure to inform us of the name and address of the person requesting the certificate in the options settings when ordering. *If you do not inform us of this together, the name and address of the person requesting the certificate will be left blank. *It will take approximately two weeks for a product with a calibration certificate to be delivered, as the calibration will be carried out after the order is confirmed. (However, please note that additional days will be required during the New Year holidays and long vacations.) *We cannot accept cancellations or returns after an order has been placed. *For other information, please check the instruction manual.
It can be used to know the danger of heat stroke and the epidemic of seasonal influenza.
Up to 5 slave units can be connected to one master unit.
The maximum communication distance is 100m (line-of-sight distance, height 1.2m).
Built-in sensor to measure environmental temperature and humidity.
A temperature probe (sold separately) can be connected, and up to two can be connected to one slave unit.
Soil temperature and liquid temperature can be measured (cable length of temperature probe is about 2.5 m).
Since the handset also has a liquid crystal display, it is possible to check the measured value at the measurement site.
Specified low power equipment, radio frequency used is 429.2MHz.
In an agricultural house. For measuring temperature and humidity and soil temperature (soil temperature) in the house such as raising rice seedlings, in a warehouse for vegetables, fruits, and liquor. For fermentation of crops such as vegetables and fruits, sake brewery / wine, temperature and humidity control of brewing, temperature and humidity of factories, offices, gymnasiums, facilities, houses, risk of heat stroke and influenza pandemic control ..
*If the product comes with general calibration documents, the relevant documents will be attached when shipped. *If you require the name and address of the person requesting the certificate, please be sure to inform us of the name and address of the person requesting the certificate in the options settings when ordering. *If you do not inform us of this together, the name and address of the person requesting the certificate will be left blank. *It will take approximately two weeks for a product with a calibration certificate to be delivered, as the calibration will be carried out after the order is confirmed. (However, please note that additional days will be required during the New Year holidays and long vacations.) *We cannot accept cancellations or returns after an order has been placed. *For other information, please check the instruction manual.
Ketentuan dan Kondisi Barang
COD Tidak Berlaku
Pembayaran COD tidak tersedia untuk produk ini. Lihat selengkapnya
Pengembalian Barang 14 hari
Berubah pikiran tidak dapat diterima. Lihat selengkapnya
GRATIS ONGKIR* ke Jabodetabek, Banten,
Jabar & Jatim dengan minimum total pesanan Rp200.000 saat checkout. Lihat selengkapnya
Jabar & Jatim dengan minimum total pesanan Rp200.000 saat checkout. Lihat selengkapnya
Pilih jenis produk yang diinginkan
| Nomor SKU | Model Number | Masa Persiapan Barang | Harga | Jumlah |
|---|---|---|---|---|
| Loading... | ||||
Ulasan Produk
Tidak ada ulasan



















































































































































%201pc/c5S052861437-2.jpg)