OMRON Uninterruptible Power System R6921Q12 1pc
Rp5.599.900
Persediaan
Spesifikasi Produk
| Model Number | R6921Q12 |
|---|---|
| Unit | 1pc |
| Included Accessories | 1 x Instruction Manual, 1 x Supplementary Manual, 4 x Product Number Labels, 19-inch Rack (JIS/EIA Rack) Mounting Brackets (Cage Nut M5, Pan Head Screw M5-12mm, Tapping Screw M5-12mm, Truss Screw M4-12mm, Pan Head Screw M5-35mm, Knurled Nut) |
| Cable Length (m) | Power cable: Approx. 3 |
| Rated Input Voltage (V) | 125 |
| Rated Output Current (A) | 15 |
| Rated Input Current (A) | 15 |
| Number of Phases | Single-phase 2-wire (with ground) |
| Operation Environment | [Temperature] -5°C to 40°C (24-hour average temperature must not exceed 35°C. No freezing or condensation allowed) [Humidity] 85% RH or less |
| Type of Terminal Fitting | Rack: Rack (1U) |
| Safety Standard | Electrical and Electronic Equipment Act |
| Standard to Conform | Power cable: Electrical Safety Act |
| Rated Output Voltage (V) | 125 |
| Overcurrent Protection | None |
| Plug Shape | Input: NEMA 5-15P |
| M Code | 65457929 |
| Berat (Kg) | 2.5 |
| Tanggal Produk Terdaftar | 13 November 2025 |
| Terakhir Diperbaharui | 02 April 2026 |
Informasi Produk
Warning
* The number of mounting brackets included varies depending on the Basic PDU model.Feature
<Verification of connection with Omron UPS used in the set>We have tested the connection with an OMRON UPS and confirmed that the following combinations work without any problems, so you can use them with confidence.
When used in combination with an Omron UPS with verified connection, Omron will provide a 3-year warranty.
If the product is used in any other way than as a set, it will not be covered by the warranty. Please check the set combination in the table above and be sure to use it in combination with an OMRON UPS.
<19-inch rack (JIS/EIA rack) mounting brackets included>
Various types of mounting brackets are included(※) so that the Basic PDU can be installed in 19-inch racks (JIS/EIA racks) from various rack manufacturers both in Japan and abroad, so there is no need to check how to install the Basic PDU in a rack or select or arrange the mounting brackets.
*Installation instructions using the included mounting brackets will be posted on the Omron website.
Since there are cases where installation is not possible due to influences such as the environment inside the rack, we cannot guarantee that the product can be installed in all 19-inch racks (JIS/EIA racks).
<Free warranty extension/on-site maintenance service contents also apply to Basic PDU>
If you have purchased a free warranty extension/on-site maintenance service for an OMRON UPS that you use in a set, please enter the product number of the Basic PDU you purchased along with the OMRON UPS when applying for each service. We will provide the same service for the Basic PDU as the service you purchased.
The applicable UPS is only the OMRON UPS that has been verified for connection as described on the previous page. If the product is used in any other way than in combination with the applicable OMRON UPS, the service will not be available.
<We offer an "advance replacement service" to registered customers>
If you register as a user of an Omron UPS, you will be able to take advantage of our advance replacement service, whereby a replacement will be sent to you the next business day after your application if the product breaks down within the warranty period.
<Sliding mounting bracket included>
The mounting pitch can be freely set by inserting the included mounting bracket into the slide rail on the side of the aluminum body and sliding it (0U type only).
Use
It receives power from an Omron rack-mounted UPS installed in a 19-inch rack (JIS/EIA rack) and supplies power to IT equipment (servers, storage, routers, etc.) connected to the output outlets of the Basic PDU.Ketentuan dan Kondisi Barang
COD Tidak Berlaku
Pembayaran COD tidak tersedia untuk produk ini. Lihat selengkapnya
Pengembalian Barang 14 hari
Berubah pikiran tidak dapat diterima. Lihat selengkapnya
GRATIS ONGKIR* ke Jabodetabek, Banten,
Jabar & Jatim dengan minimum total pesanan Rp200.000 saat checkout. Lihat selengkapnya
Jabar & Jatim dengan minimum total pesanan Rp200.000 saat checkout. Lihat selengkapnya
Pilih jenis produk yang diinginkan
| Nomor SKU | Model Number | Masa Persiapan Barang | Harga | Jumlah |
|---|---|---|---|---|
| Loading... | ||||
Ulasan Produk
Tidak ada ulasan



















































































































































/OMRON%20Uninterruptible%20Power%20System/OMRON%20Uninterruptible%20Power%20System%20R6921Q12%201pc/a1S048853361-1.jpg)