Daytona Golden Pad X 97128 1pc

#Nomor SKU S007467602
Wishlist
Rp769.900
Persediaan

Spesifikasi Produk

Model Number 97128
Unit 1pc
Compatible XJR1300 (98-99) <R>, XJR1300 (00) <R>, FJ1200 (86-88) <WF>, FJ1200 (86-88) <R>, FJ1200 (89-93) <R>, V- MAX (85-92) <WF>, V-MAX (85-92) <R>, V-MAX (93-07) <R>, XJR1200 (94) <R>, XJR1200 (95-96) <R >, XJR1200R (96) <R>, XJR1200SP (97) <R>, F
Third-Party Reference Number (DAYTONA) 68238
M Code 89497625
Berat (Kg) 0.2
Tanggal Produk Terdaftar 25 October 2018
Terakhir Diperbaharui 01 December 2025
ask-button

Apakah produk dengan spesifikasi yang Anda inginkan belum tersedia? Hubungi tim Layanan Pelanggan kami di sini

Informasi Produk

Warning
Please do not use absolute cast iron rotor. In conformity statement, notation for the front disc of , will be for the rear disk. Notation because of the front double-disk car, you will need two sets. year is not the year model of the manufacturer's declaration, it is represented in sales started the year. also genuine pad is a shape is the same, the thickness of the friction material is a wide variety. Also similar in materially wear resistance, the life of the pad varies in thickness of the friction material. Also, please understand that life is different depending on the frequency of use of the brake. caliper (movement of the piston condition, etc.) and disc rotor (wear, mirror surface, oil, such as the coated by the previous pad that was used) might not be sufficiently exhibited original performance in the cause. Maintenance of the parts involved will also be important. Golden pad is a registered trademark of the (stock) Daytona.
Feature

Sintered renewal! Concept the Golden pad, which has been supported for many years by the honest control potentially overturn the common sense of the metal pad for the first time in 10 years as it is, we further enhance the control and efficacy. Push the brake pads as custom parts, please come and experience the pleasure that has been freed from the fear of the brake.
Ketersediaan Barang
Subtotal
GRATIS ONGKIR* ke Jabodetabek, Banten,
Jabar & Jatim dengan minimum total pesanan Rp200.000 saat checkout. Lihat selengkapnya

Pilih jenis produk yang diinginkan

Nomor SKU Model Number Masa Persiapan Barang Harga Jumlah
Loading...

Ulasan Produk

Tidak ada ulasan